Power & Energy
  • Technologies
  • More
Power & Energy
Blog Solar Energy Harvesting with Epishine Flexible Solar Cell - Pt 2: Circuit Analysis
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
  • Author Author: Jan Cumps
  • Date Created: 31 Jul 2020 4:27 PM Date Created
  • Views 4890 views
  • Likes 10 likes
  • Comments 12 comments
  • epishine
  • energy_harvesting
Related
Recommended

Solar Energy Harvesting with Epishine Flexible Solar Cell - Pt 2: Circuit Analysis

Jan Cumps
Jan Cumps
31 Jul 2020

I got a preview of a light harvesting kit from Epishine and element14. Check my intro here.

In this post, I try to analyse the ways of working. I don't have a schematic.It's based on google-research.

 

image

 

 

 

There are 3 main modules:

  • the photovoltaic cell to turn light into electric energy
  • energy harvesting IC with a super cap to collect and store the energy
  • a variable buck regulator for the output voltage

image

 

Solar Cell: Epishine LEH3_50x50_6

 

The largest part of the kit is covered by the flexible photovoltaic cell.

This is Epishine's core business: organic solar cells printed on plastic sheet. The company says it uses biopolymers.

For a manufacturer independent view on printed cell technology, I found the explanation of Sadok Ben Dkhil a good read.

image

You can clearly see the 6 printed elements, and the - also printed - wiring between them.

Epishine suggests on the website that these are for ambient and artificial light conditions.

A soft suggestion. It's not explicitely stated. But all proposed use cases are for those conditions.

Jon has commented that UV light in particular may age them.

 

The flex design can be interesting. First of all, it allows the manufacturer to produce and ship these on rolls.

That's a way easier process than producing big flat surfaces. Handling in the logistics chain and storage are easier for products "on roll".

It's new technology though. And as of now, it's still difficult to master the production print process, and get stability over time.

 

Another possible advantage is that these are thin. Very thin. They take up surface, but almost no depth.The

The flex also allows to put them in a design that has a curved outline.

The material isn't hardened and can't be flexed beyond a reasonable point. Designs will have to take that into account.

 

In the evaluation kit, the cell is fixed on a flexible PCB. The PCB adds protection against over-bending - it is less compliant than the cell.

This combination is a good example of a very thin design that protects the cell against physical force.

The cell surface is exposed. It isn't protected in this kit.  Proper care is needed when handling and storing.

 

Harvesting Circuit: e-Peas AEM10941 and CAP-xx Super Capacitor

 

image

 

The harvest circuit is an e-Peas solar energy harvesting IC. It's an IC that is specifically designed for this kund of application:

  • input from a solar cell
  • additional battery sourcing option - it switches to that to extend the on-time when the super cap is discharging.

 

image

image source: AEM10941 PRODUCT BRIEF: Functional block diagram

 

You can find some of this device's parameters back in the kit's spec:

 

  • Cold start from 380 mV
  • Automatically switches to the primary battery when the secondary battery is exhausted

 

On the kit from Epishine, the PV Cell is the fex solar cell. The Primary battery is the optional one that can be connected in.

The Energy Storage is the super CAP.

The CFG [0..2] can be found back on the board too: 0 and 2 pulled down. 1 pulled up. May want to look up what that config means...

 

The super capacitor is a GA230F CAP-XX 0.40 F, 5 V component. The datasheet is available.

It's made out of two separate capacitors, with a tap in the middle called BAL. The e-Peas IC uses that middle tap.

Like all components in this kit, it's a master of miniaturisation. 400 miliFarads in a component the size of a CR-2032.

image

The circuit loads the capacitor at 4.5 V. Who remembers the formula to calculate the energy contained by  a 0.4 F capacitor at 4.5 V?

 

Output Circuit: Buck Converter with Selectable Voltage

 

image

 

The output is controlled by a Texas Instruments TPS62740.

The functionality of this step down converter, again, matches the details of the Epishine kit.

 

  • Up to 300mA Output Current
  • 16 Selectable Output Voltages in 100mV Steps between 1.8V to 3.3V

They even mention in the application: The input voltage range up to 5.5V allows also operation from a USB port and thin-film solar modules.

 

 

The three blocks above result in a nice combination.

When I first looked at the kit, I couldn't imagine that there would be a wealth of electronics to investigate.

 

 

 

Off to the next blog. First measurements ...

 

Related blog
Pt 1: intro
Pt 2: Circuit Analysis
Pt 3: Charge and Discharge
Pt 4: Battery Backup
Pt 5: test points
  • Sign in to reply

Top Comments

  • jc2048
    jc2048 over 6 years ago +4
    I leave it to the coulomb experts to calculate the charge. That's easy. Even I can do sums like that! Q = C x V so 0.4F x 4.5V = 1.8 coulombs of charge The charge is directly proportional to voltage so…
  • Jan Cumps
    Jan Cumps over 6 years ago +3
    Note to self: excellent application note from e-Peas about provisioning the right cell and capacitor for a given load - with calculations and guiderails: https://e-peas.com/wp-content/uploads/2020/06/AppNote_EH_Photovoltaic_AEM10941…
  • DAB
    DAB over 6 years ago +2
    Good update Jan. UV would be very bad for the Bio-polymers they use, so if you want to put them outside, pick up a UV filter. The circuit looks very similar to one I picked up from Texas Instruments five…
Parents
  • DAB
    DAB over 6 years ago

    Good update Jan.

     

    UV would be very bad for the Bio-polymers they use, so if you want to put them outside, pick up a UV filter.

     

    The circuit looks very similar to one I picked up from Texas Instruments five or six years ago. They had the same idea, solar cell to super cap, but it never did work well when I tested it.

     

    The supercap looks huge, what is the energy storage specs on it?

     

    DAB

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • Jan Cumps
    Jan Cumps over 6 years ago in reply to DAB

    DAB  wrote:

    ...

    The supercap looks huge, what is the energy storage specs on it?

    ...

    datasheet: https://www.cap-xx.com/wp-content/uploads/2018/07/CAP-XX-GA130-GA230-Datasheet-v4-3-Copy.pdf

    Spectacular. The capacity is 400mF (not µF), up to  5V.

    The Epishine design charges them with a little over 4.5 V. I leave it to the coulomb experts to calculate the charge.

     

    I's not huge though. Similar footprint size to a coin cell.

     

    The circuit looks very similar to one I picked up from Texas Instruments five or six years ago. They had the same idea, solar cell to super cap, but it never did work well when I tested it.

    Do you have a pointer to that test? That kind of circuit has no magic, so it should work as specified - if you respect that it delivers the power it's specced for - not some magical extra energy ...

    Asking because I may have tested that one too. The one I tested was up to their specs.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • Jan Cumps
    Jan Cumps over 6 years ago in reply to DAB

    DAB  wrote:

    ...

    The supercap looks huge, what is the energy storage specs on it?

    ...

    datasheet: https://www.cap-xx.com/wp-content/uploads/2018/07/CAP-XX-GA130-GA230-Datasheet-v4-3-Copy.pdf

    Spectacular. The capacity is 400mF (not µF), up to  5V.

    The Epishine design charges them with a little over 4.5 V. I leave it to the coulomb experts to calculate the charge.

     

    I's not huge though. Similar footprint size to a coin cell.

     

    The circuit looks very similar to one I picked up from Texas Instruments five or six years ago. They had the same idea, solar cell to super cap, but it never did work well when I tested it.

    Do you have a pointer to that test? That kind of circuit has no magic, so it should work as specified - if you respect that it delivers the power it's specced for - not some magical extra energy ...

    Asking because I may have tested that one too. The one I tested was up to their specs.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
Children
  • DAB
    DAB over 6 years ago in reply to Jan Cumps

    Thanks Jan.

     

    It was a home project, so I did not publish anything on the results.

     

    I will have to do a search through my parts bin to see if I can find it.  Maybe it is worth another look.

     

    DAB