Test & Tools
  • Technologies
  • More
Test & Tools
Blog Keithley DMM6500: Verify a µCurrent Manually
  • Blog
  • Forum
  • Documents
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Test & Tools to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: Jan Cumps
  • Date Created: 17 Jan 2019 6:05 PM Date Created
  • Views 2884 views
  • Likes 7 likes
  • Comments 2 comments
  • RoadTest
  • dmm6500
  • rt
  • keithley
  • 121gw
  • µcurrent
  • eevblog
Related
Recommended

Keithley DMM6500: Verify a µCurrent Manually

Jan Cumps
Jan Cumps
17 Jan 2019

I'm road testing the  Keithley Bench Digital Multimeter DMM6500.

In this blog, I verify the performance of an EEVBlog µCurrent; from the DMM6500 frontpanel controls..

image

 

 

The µCurrent is a test instrument that translates current to volt. You can think of it as a shunt resistor with an amplifier.

It's specifically designed to be used for low current measurements.

In this blog, I want to compare its measurements with the DMM6500, in mA range.

Not for a specific reason. Just to have a valid test setup that I can automate in the next post.

 

The Test Setup

 

  • a 2 V power supply, loaded by a dc load.in the 2 to 90 mA range
  • µCurrent and DMM6500 in series to measure the current
  • 121GW DMM to measure the output of the µCurrent. 1mA measured results in 1 mV output.
  • pen and paper

 

image

 

Test Procedure

 

The 121GW DMM, set to mV range, measures the out put of the µCurrent.

Because the 1 mV = 1 mA factor, I just have to write down the measured value and give it the mA unit.

 

The DMM3500 set to DCI, in slow with high precision mode. I don't need the precision for this example, but the slow reading helps me get a stabler screen.

  • Set to DCI
  • Press Menu -> Measure -> Quickset -> Activate Control.
  • Slide the control to the very left, for high resolution at low speed.

image

  • Press Home

 

The DC load (I'm using my homegrown one) is set to sink current from the supply. I'm not asking it for a precise current because I'm not speccing the load.

As long as the same current runs through the µCurrent and the DMM6500 it's OK. And they are in series, so that requirement is fulfilled.

The load current is controlled by a DAC. I'm stepping it from 120 to 960, roughly 2 to 90 mA.

At each increment, I write down the readings of both meters.

 

Results

 

In my setup, the µCurrent measures just a tad higher than the DMM6500.

The measurements can be influenced by the 121GW's precision in the mV range. No worries here, its virtually in sync with the DMM6500 in this range.

image

The graph isn't very revealing. The lines fully overlap. That's actually a good thing.

image

 

The purpose of this post wasn't to make a very precise specification of the µCurrent. I want to set the scene for the automation in the next blog.

This exercise allows to look back and have a comparison point.

 

I'll have to find a way in the automated setup to switch the DMM3500 between current and volt measurement.

Switching the instrument's mode is easy, but I'll have to alter the circuit, because the ground input is shared between volt and current mode, and the µCurrent input ground is connected to its output ground.

If you look at the test setup, you can see that I can't get away with simply wiring the DMM6500 in for current and measure the µCurrent output in the same circuit.

Maybe I'll use an oscilloscope to measure the µCurrent output ...

 

Related Blog
Software Control Options Pt 1 - TSP Script Builder, LabVIEW, Web Interface
TSP Script Example - Measure Power
How to Create a Bitmap for a Custom App
Verify a µCurrent Manually
Verify a µCurrent in an Automated Setup
Measure Amp-Hours of a microcontroller with a µCurrent
Trigger from External Trigger Input
Trigger from External Trigger Input in LabVIEW
Software Control Options Pt 2 - Test Commands with Communicator
App to Hold Measurements
Store Multiple Measurements Manually
Keithley DMM6500: Script Example - Externally Triggered Measurements

 Keithley DMM6500: Software Control Options Pt 3 - VSCode TSP Toolkit 

  • Sign in to reply
Parents
  • DAB
    DAB over 7 years ago

    Nice post on your test set up and methodology.

     

    DAB

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • DAB
    DAB over 7 years ago

    Nice post on your test set up and methodology.

     

    DAB