Test & Tools
  • Technologies
  • More
Test & Tools
Blog The Modular Bench Power Supply ++, The Essential DIY Build for Every EE Student and Old Timer alike...
  • Blog
  • Forum
  • Documents
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Test & Tools to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: Robert Peter Oakes
  • Date Created: 15 Sep 2014 4:56 AM Date Created
  • Views 16391 views
  • Likes 20 likes
  • Comments 54 comments
  • tutorial
  • bench
  • meter
  • supply
  • load
  • dc
  • power
Related
Recommended

The Modular Bench Power Supply ++, The Essential DIY Build for Every EE Student and Old Timer alike...

Robert Peter Oakes
Robert Peter Oakes
15 Sep 2014

For every student of Electrical / Electronic Engineering and also the more mature Hobbyist, there is one thing you MUST build for your self at one time or another in your career, preferably earlier on

 

That's a Bench Power Supply and if you don't know how to start or are interested in having a second go at it then welcome to the show, it is going to be a fun and educational ride for all of us.

 

Blog #2 - Voltage References http://www.element14.com/community/groups/test-and-measurement/blog/2014/09/29/voltage-references--the-modular-bench-power-supply

Blog #3 - OP Amps and the Power Stage : http://www.element14.com/community/groups/test-and-measurement/blog/2014/10/04/op-amps-1--intro--the-modular-bench-power-supply

Blog #4 - Displays - Digital and Simple http://www.element14.com/community/groups/test-and-measurement/blog/2014/11/13/the-modular-bench-power-supply--simple-display-setup

BLOG #5 - Power Output Stage (BJT/MOSFET) http://www.element14.com/community/groups/test-and-measurement/blog/2014/11/16/the-modular-bench-power-supply--power-output-stages

BLOG #6 - Basic Unit The Modular Bench Power Supply ++, Putting it all together, the bare bones

Blog #7 - The Modular Bench Power Supply ++ The Input Stage... I want the POWER!!!

Blog #8 - The Modular Bench Power Supply ++, Getting the higher voltages for high side MOSFETS

Blog #9 - The Modular Bench Power Supply ++, More on Displays and using an Arduino to measure Volts and Amps

Blog #10 - The Modular Bench Power Supply ++, Arduino UNO and precision ADC, DAC + MDO3000 I2C debugging

Blog #11 - The Modular Bench Power Supply ++, Differential Sensing and summing junctions

Blog #12 - The Modular Bench Power Supply ++, Integration theory and practical

Blog #13 - The Modular Bench Power Supply ++, testing it all on the bench with the BreadBoard

Blog #14 - Electronic DC Load - Design and Build to test PSU Project

Blog #15 - Electronic DC Load - Performance Improvements

 

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

So firstly why should every EE build one of these, well for starters it is a very useful tool for any EE to use for prototyping, testing and many other things from Battery Charging to help test the power limits of a new control system

the second and an equally important reason is it provides numerous opportunities to learn some great skills regarding controlling power, feedback loops used for current limits and voltage stability, you can learn the difference between Accuracy and Stability (Which do you think is more important for a voltage reference in a power supply, well you will find out).

 

So who am I to show you how. Well I'm a certified electronics engineer who went through an apprenticeship in the north of England with a great company called Welwyn Electric (Now I believe part of the Vishay group). Anyway I learned my trade there and also had the awesome opportunity to work in a second level Calibration LAB where I got to play with all sorts of electronics equipment to numerous to list, learning how to calibrate them way beyond the manufacturers standard cal procedures but I also learned the value of having certain good equipment to help with project design, testing and maintenance. A good Meter, Scope and Power Supply, the first two are out of reach as a tutorial but the supply is not. I built my first one when I was 17, there were no micro-controllers, no LCD Displays, it was all analogue and Moving Coil Meters... Ah those where the days.

 

Anyway, the whole process from designing it, figuring out why things worked the way they did and also how to improve on the design over time to make it more accurate, more stable and provide more power was always a great learning opportunity

 

Now I wish to share this with everyone on a new and improved Modular Bench Power System, and when I say modular I mean modular. I have seen so many designs claiming to be modular but in reality it is one design and one fixed result. Some good and some bad.

 

Element 14 has been kind enough to sponsor me for this project and I will be providing links to all the components used in he project so you can also use the same if you so desire.

 

What I am planning is a power system that can be as upgradeable as most desktop computers (Need a new video card, great, swap out the old for new, need a better CPU, Same thing). In our case each significant module of this power supply will go through two or more versions as we ride the project to its destination. My Target destination anyway, you will be welcome to ride all the way with me or get off part way through depending on your budget and time. Oh and of course you can also stay on the train and take it beyond my design and make it yours. and you don't have to do everything, there is plenty of opportunity to mix and match as we go.

 

by now yo may be wondering, why do I keep calling it the Bench power System and not Supply, well this is why:-

 

My ideal target specifications

There will be three significant parts that can be built as separate projects or included into the Power System

Dual Channel Power Supply each outputting 30V @ 4A or 15V @ 8A, user selectable, independently adjustable

DC Load 60V /10A (But not 600W image ) controlling  Volts and Current

Power Meter showing Watts, Watt Hour, Volts, Current

Battery Charging Profiles

Logging on all modules above

Network and USB support for LXI and VISA protocols (SCPI)

All modules controlled by micro-controller/s with a master control unit based on embedded Linux

4" touch screen display / control

Speech Output

 

Not all of the above features are needed or essential, and there is no need to build yours to the same specification, I will tell you where the opportunities are to put in parts to meet your budget and requirements

 

The main power supply is broken down in to several sub modules as follows

 

Voltage Reference circuit, providing feeding the other modules

DC Power, this module converts the mains supply to a safe and smooth voltage for the rest of the supply

Output Driver. This module will be  power transistors providing the actual limiting of the output to supply channels

Output and Sense, this is the actual output and also the voltage sense circuit needed for control

Voltage Control module set and vary the desired output voltage of the supply

Current control module will allow the user to pre-set the current limits of the power supply outputs

Displays and Controls, how else will you see and adjust things image

 

We will start with the basics, a backgrounder on the modules purpose and basic functionality, the simpler analogue design and accurate enough for basic projects, this will help you understand Voltage references, OP-AMPS, feedback loops, Curent shunts both high side and low side and the benefits of each

 

Later, once we have the basic PSU working, we will upgrade modules to improve the regulation, accuracy and then some form of digital control in the form of a micro-controller, at this point we will discuss ADC, DAC resolution, over sampling etc.

 

This is a block diagram of the first modules we will tackle:

image

Oh and don worry if your unsure of handling mains voltages , there will be an option to cover that off too, I don't want to put anyone in harms way or take them out of their comfort zone (If your new to electronics and don't have experienced help, take the simpler approach I will present)

 

Oh, just so were clear. not all the designs are complete, only the concepts and target specifications are known at this point, I have many parts selected based on experience but what we end up with is unknown at this time and like I said at the beginning, its going to be a fun ride. So buckle up and get the soldering irons tuned

 

So what do you think, I'm open to ideas and nothing too crazy will be rejected from the considerations pile, if there is something you would specifically like covered, let me know

 

I look forward to your input and support

 

First lesson coming soon all about Voltage References.

  • Sign in to reply

Top Comments

  • 4ringfan
    4ringfan over 11 years ago +1
    I'm interested in this as well. I'm looking forward to watching the videos.
  • jw0752
    jw0752 over 11 years ago in reply to 4ringfan +1
    Hi Mike, This is a great series of videos by Peter. Peter is also an expert on Arduino in case you have any questions. John
  • DAB
    DAB over 11 years ago +1
    Hi Peter, Count me in, I have been following your progress with great interest. DAB
Parents
  • omnacron
    omnacron over 9 years ago

    Hello Sir i know this forum post is rather old and i hope someone still views it that may be able to help me. i have the circuit mocked up on my bread board and for the most part it is working except it seems that i don't have the proper current control and on both my pots it seems that all my control is in the very first 1/4 of the pots. my input power is from a 12v atx supply so my max output is only around 8.4 volts. the pots are very sensitive in that first 1/4 of the turn except for the current pot which dosn't seem to work correctly i was hoping some one could look at my diagram and see if I have something incorrect. don't pay attention to the bridge rectifier. part of the diagram its not implemented yet. image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • jw0752
    jw0752 over 9 years ago in reply to omnacron

    Hi Timothy,

     

    You might want to move the reference voltage connection from the anode of D1 to the Cathode of D1. As it is drawn your reference voltage sits one diode drop above ground. I think you want it to be at one diode drop plus 5.1 volts. Your limiting factor is of course the rather low 12 volt supply that you are working with. R7 and R5 would indicate an approximate 10 to 1 ratio between output voltage and reference voltage. Your current control is likely not working for the same reason. The reference voltage is tied to the wrong side of the Zener.

     

    John

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • omnacron
    omnacron over 9 years ago in reply to jw0752

    Thank you for the very quick reply. as to the Zener i didnt catch the mistake in the diagram on the breadboard the connection is on the other side of the zener. For the low voltage im working with im using the ATX supply to make sure the cicut works before running it through the full 32 volts, I started the project doing just that and melted a bread board and fried most of my circuit lol. so decided to start with a lower voltage this time. I do have a 19 volt 4 amp brick i could swap out and see how it responds. I do have a question about the shunt that im using, In Peters original diagram he is using a current shut resistor i do not have one of those will the current shunt that i have which is a 50amp 75mv shunt used with my YB27A volt and ammeter can i hook it up to the current feed back to the op amp?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • omnacron
    omnacron over 9 years ago in reply to jw0752

    Thank you for the very quick reply. as to the Zener i didnt catch the mistake in the diagram on the breadboard the connection is on the other side of the zener. For the low voltage im working with im using the ATX supply to make sure the cicut works before running it through the full 32 volts, I started the project doing just that and melted a bread board and fried most of my circuit lol. so decided to start with a lower voltage this time. I do have a 19 volt 4 amp brick i could swap out and see how it responds. I do have a question about the shunt that im using, In Peters original diagram he is using a current shut resistor i do not have one of those will the current shunt that i have which is a 50amp 75mv shunt used with my YB27A volt and ammeter can i hook it up to the current feed back to the op amp?