Test & Tools
  • Technologies
  • More
Test & Tools
Documents Programmable Electronic Load - ADC and DAC BoosterPack test
  • Blog
  • Forum
  • Documents
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Test & Tools to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Engagement
  • Author Author: Jan Cumps
  • Date Created: 24 Nov 2017 11:12 AM Date Created
  • Last Updated Last Updated: 2 Dec 2017 10:04 AM
  • Views 5355 views
  • Likes 7 likes
  • Comments 35 comments
Related
Recommended

Programmable Electronic Load - ADC and DAC BoosterPack test

WIP

 

This blog documents the characteristics of the DAC/ADC BoosterPack of the electronic load that Robert Peter Oakes, jc2048 and Jan Cumps are designing.

We have the same DAC/ADC BoosterPacks so we can compare the measurements of each ADC and DAC channel. Check the main document for anything related to hardware and firmware.image

 

Test Setup

 

Peter has created a GUI that we can use to shoot SCPI commands. We can control the DACs and read the ADCs.

Measurements are performed with and without the power driver BoosterPack installed. We'll use 5V to power the DACs and ADCs in both situations.

 

image P1 and P2 on the bottom of the DAC/ADC BoosterPack have to be open. Else you'll inject 5V onto the LaunchPad 3V3 rail and you'll damage components.

 

It's not critical if you switch on the power supply before or after you connect the LaunchPad to your computer. The circuits are isolated.

All measurements use P3.10 as GND reference and P3.1 as reference voltage.

 

image

 

Setup without the power driver BoosterPack:

Mount the DAC/ADC BoosterPack on the LaunchPad.

Use a +5V power supply. It should be a decent one, current is approximately 5 mA.

Connect image with DAC/ADC BoosterPack P4.2  and image with P4.1.

 

Setup with the power driver BoosterPack:

Mount the DAC/ADC BoosterPack on the LaunchPad and the Power Driver BoosterPack on top of that.

On the Power Driver BoosterPack, bridge pins P2.4, P2.5 and P2.6 to tie both opamp inputs of opamp 3D to ground.

Use a +12V power supply. It should be a decent one, current is approximately 50 mA.

Connect image  with Power Driver BoosterPack P1.1 image  and with P1.2.

 

image

 

Measurements

 

In the table, the first column shows what we're measuring, the second column the SCPI command to execute with Peter's GUI.

The next columns are the measurements for Peter, Jon or Jan with and without the Power Driver BoosterPack.

The last column is for comments. We can indicate odds, errors, learnings.

 

JonPeterJan
Data PointSCPIWithoutWithWithoutWithWithoutWithMeasurement method
SupplyN/A4.989 V11.88 VDMM
DAC/ADC V+N/A4.989 V5.035 VDMM
VREFN/A2.046 V2.046 VDMM
ADC A GNDDEVE:ADC1?2SCPI output
ADC A VREFDEVE:ADC1?10918SCPI output
ADC ADEVE:ADC1?1138SCPI output
ADC B GNDDEVE:ADC2?12SCPI output
ADC B VREFDEVE:ADC2?10920SCPI output
ADC BDEVE:ADC2?1
SCPI output
ADC C GNDDEVE:ADC3?22SCPI output
ADC C VREFDEVE:ADC3?1092010919SCPI output
ADC CDEVE:ADC3?26868SCPI output
ADC D GNDDEVE:ADC4?83SCPI output
ADC D VREFDEVE:ADC4?1091910919SCPI output
DAC A 0DEVE:DAC1 00.000 V0.001 VDMM
DAC A maxDEVE:DAC1 655352.040 V2.040 VDMM
DAC B 0DEVE:DAC2 00.005 V0.005 VDMM
DAC B maxDEVE:DAC2 655352.046 V2.046 VDMM
DAC C 0DEVE:DAC3 00.000 V0.000 VDMM
DAC C maxDEVE:DAC3 655352.039 V V2.039 VDMM
DAC D 0DEVE:DAC4 00.000 V0.000 VDMM
DAC D maxDEVE:DAC4 655352.039 V2.039 VDMM

 

 

To resolve

With the power driver installed, ADC C and D act strange (probably also A and B, but I didn't inject a voltage in them because they are connected to opamp pins).

In particular strange for ADC D, because that one isn't routed. Strange.

I will try to decrease the frequency of the sample speed and the i²c speed to see if it's related to that ...

 

Follow up: the cause is that OPAMP 3C injects -0.8V into ADC A. All measurements are off when that happens. As soon as I force ADC A positive (by tying it to ground or a positive voltage) all measurements are correct.

 

image

 

We have a separate document to analyse the summing node at zero.

  • metrology
  • boosterpack
  • msp432
  • ti-rtos
  • launchpad
  • laboratory
  • instrument
  • Share
  • History
  • More
  • Cancel
  • Sign in to reply

Top Comments

  • shabaz
    shabaz over 8 years ago +3
    Hi Jan, I was wondering, what are the expected values, is it reading a value representing 1.602V when it should read a value representing 2.048V? I'm wondering if it could be due to conversion time (i…
  • Jan Cumps
    Jan Cumps over 8 years ago in reply to shabaz +3
    yes, Shabaz, I have a controlled value of 2.040 V. Once I mount my additional driver board (self-designed so many things can be wrong ) the ADC says it’s 1.6 V. I checked signals with my scope to see if…
  • jc2048
    jc2048 over 6 years ago in reply to Andrew J +3
    Andrew J , have you read the blog I did when building Jan and Peter's load? That has some material on the low end of the DAC. Long story short, I adapted the analogue stuff after the DAC so the output…
  • Jan Cumps
    Jan Cumps over 6 years ago in reply to Andrew J
    I was expecting that I'd need to keep a look up table, which, again, seems to be the approach you have taken.

    I haven't. I just store the offset and the correction factor. 2 values. But I haven't been able to turn this in a precise result.

     

     

     

    My DAC has a 0 offset of +7mV and a max offset of -2.5mV so it can't get a full range through a simple software adjustment - I think, I was hoping to get an insight from the work you have done here.

     

     

    I have tried to use an external additional OpAmp to deal with that offset. On the output of my DAC, I wired up  that opamp as analog adder, and provided the offset error as input.

    So that if the DAC outputs 0.0001 V at 0, I would feed - 0.0001 into the opamp, and the offset would be erased.

    It didn't work in my case. I blogged about it, but couldn't find it back right now. I'll search for it ...

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • Andrew J
    Andrew J over 6 years ago in reply to Jan Cumps

    Perhaps I missed it when I read through the calibration steps - but I understand what you are doing above and I am trying to do the same, coincidentally!  It's effectively compensating for the gain (multiplier) and offset (addition).   I can see with my DAC that it isn't linear so I was expecting that I'd need to keep a look up table, which, again, seems to be the approach you have taken.  What I was hoping to understand is how you drove the DAC output to 0 when it has an offset of 5mV or to 2.040 when it has an offset of -1mV.  My DAC has a 0 offset of +7mV and a max offset of -2.5mV so it can't get a full range through a simple software adjustment - I think, I was hoping to get an insight from the work you have done here.

     

    Thanks

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • Jan Cumps
    Jan Cumps over 6 years ago in reply to Andrew J

    Use with caution, because I haven' been able to define a stable and linear solution yet.

    I'll include links to the source code in gitub....

     

     

    I use two calibration functions. One that deals with offset, one with scale (I use a corrective multiplier):

    My calibration functions are in this API: https://github.com/jancumps/msp432/tree/master/MSP432_SCPI_ElectronicLoad/calibration_impl

    The function that uses the calibration corrections: https://github.com/jancumps/msp432/blob/master/MSP432_SCPI_ElectronicLoad/control_impl/control_strategy_constantcurrent.…

     

     

    I have several of those offset + multiplier correction pairs. I'll focus on the DAC:

     

     

    // current write calibration
    
    
    bool calibrationSetCurrentWriteMultiplier(float value) {
        if(_bCalibrationActive) {
            _CalibrationData.current_write_multiplier = value;
        }
        return _bCalibrationActive;
    }
    
    
    float calibrationGetCurrentWriteMultiplier() {
        // The DAC drives the FET todo in my case the DAC setting multiplied by 0.000116 gives current
        float fRetval = 0.0;
        fRetval = _CalibrationData.current_write_multiplier;
        return fRetval;
    }
    
    
    bool calibrationSetCurrentWriteOffset(float value) {
        if(_bCalibrationActive) {
            _CalibrationData.current_write_offset = value;
        }
        return _bCalibrationActive;
    }
    
    
    float calibrationGetCurrentWriteOffset() {
        // The DAC drives the FET todo in my case the DAC runs 0.008 A when not driven
        float fRetval = 0.0;
        fRetval = _CalibrationData.current_write_offset;
        return fRetval;
    }

     

     

    Then in the current set function, I use these (stored in EEPROM) values to correct the DAC seting:

     

    void ConstantCurrentStrategyControlFunction () {
        if (bConstantCurrentChanged) {
            uint32_t value = 0U;
            value = ((fConstantCurrent/calibrationGetCurrentWriteMultiplier())-calibrationGetCurrentWriteOffset()); // todo: double check if it is - or plus offset
            eloadRawSetDac(0, value);
            bConstantCurrentChanged = false;
        }
        return;
    }

     

     

    I've tried to explain the calibration approach:

     

     

    Programmable Electronic Load - Calibration Steps (focus on Configure the Input Current Set Correction)

    Programmable Electronic Load - Calibration Data in Flash

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • Andrew J
    Andrew J over 6 years ago

    Hi Jan,

     

    I notice on your table of measurements for the DAC, that channel B was outputting +5mV for an input of 0; max for this channel was +6mV; channels C and D were -1mV at max.  I was reading through your calibration post to see how you dealt with this but it didn't cover DAC calibration.  Are you able to share how you calibrated this output: in particular, I'd be interested in understanding how (if) you dealt with the +5mV offset error.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • Robert Peter Oakes
    Robert Peter Oakes over 8 years ago in reply to Jan Cumps

    As soon as I get the parts and build mine up, I will be in testing things out

     

    from a summing junction perspective, think of it as simply a pair of resistors where one end is the input and the other is the feedback, the middle should always return to zero, pretty simple when thought of that way

     

    of course we have added op amps etc in the feedback loops etc just to make it more interesting image

     

     

     

    Peter

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • Jan Cumps
    Jan Cumps over 8 years ago in reply to Robert Peter Oakes

    Robert Peter Oakes, I've made a document to investigate the summing node of the design: Programmable Electronic Load - Analyse the Summing Node Zero Point

    Let's check what drives this away from 0V and if we can compensate that ...

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • Jan Cumps
    Jan Cumps over 8 years ago

    I've completed the measurements on my boards and updated the table.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • Jan Cumps
    Jan Cumps over 8 years ago in reply to Jan Cumps

    Some test points:

    The 5.036 V on the ADC3 (measured with a DMM) is sampled as 5.0364

     

    With all inputs of opamp C tied to ground and the DAC A set to 0 V, the voltage at the summing node (measured with a DMM between R3 and R4) is 0.018 V

    This results in a voltage going out of opamp B into ADC A of -0.212V (also measured with a DMM on the pin of ADC A). The ADC reads -0.2130 V.

     

    I've been running the device for many hours now. Things aren't drifting

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • Robert Peter Oakes
    Robert Peter Oakes over 8 years ago in reply to Jan Cumps

    Good, I was hoping it was not my design image, once I saw you mention the - voltage it seemed to indicate a floating current sense input, glad it was something simple

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • Jan Cumps
    Jan Cumps over 8 years ago in reply to jc2048

    There's good news. If I tie both inputs of the current sampling opamp 3C (the one that feeds back into the summing node) to ground, the negative voltage disappears.

    I now get a fairly stable reading on all four ADCs.

    It's very likely that this turns out to be a non-issue.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
<>