1 Meter of Pi
  • Challenges & Projects
  • Design Challenges
  • 1 Meter of Pi
  • More
  • Cancel
1 Meter of Pi
Blog Gr0G - 06 - Building the box
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
  • Author Author: amgalbu
  • Date Created: 2 Nov 2020 9:59 AM Date Created
  • Views 1824 views
  • Likes 6 likes
  • Comments 6 comments
  • 1meterofpi
  • gr0g
  • 1meter of pi
Related
Recommended

Gr0G - 06 - Building the box

amgalbu
amgalbu
2 Nov 2020

Here is a list of the posts in this challenge

Gr0G - 01 - Introduction

Gr0G - 02 - Why aeroponics?

Gr0G - 03 - High-pressure system design

Gr0G - 04 - Mechanical design

Gr0G - 05 - Electrical design

Gr0G - 06 - Building the box

Gr0G - 07 - Playing with the Gertbot

Gr0G - 08 - Installing LEDs

Gr0G - 09 - The control board

Gr0G - 10 - Software design

Gr0G - 11 - Building the box (2)

Gr0G - 12 - Building the high-pressure system

Gr0G - 13 - Building the high-pressure system (2)

Gr0G - 14 - Piping

Gr0G - 15 - Improvements

Gr0G - 16 - Remote UI

Gr0G - 17 - Remote UI (2)

Gr0G - 18 - Conclusions

 

Source code available at https://github.com/ambrogio-galbusera/gr0g, https://github.com/ambrogio-galbusera/gr0g-ble-android and https://github.com/ambrogio-galbusera/gr0g-ble

 

In this post we will finally start building the frame of Gr0G box

 

Building the top and bottom panels

 

Parts list

To build the top and bottom panels, you need

  • 8 pieces of bar with LED housing 46 cm in length with 45 degrees cut on both sides (when cutting, keep the LED housing facing upside)
  • 8 clamps. I got my clamps from an L-shaped 40 mm x 40 mm x 1.5 mm aluminum bar. I cut 8 pieces of 20 mm in height
  • Rivets (16, at least). I used 3 mm rivets, so I drilled the parts with a 3.3 mm bit
  • a 46 cm x 46 cm plexiglass
  • 8 M4 x 20 mm screws with bolts

 

How to proceed

  • Drill two holes for each side of the clamps (4 holes per clamp, in total). Try to stay on the middle of the clamp (see picture) because the section of the bar with the LED housing is irregular and you will get a better result if stay 10 mm from the border

image

  • Mate the clamp with the aluminum bars and fix the parts with 2 rivets per side

image

imageimage

image

  • With a 4 mm bit, drill 2 holes for each edge of the frame, close to the corner in order not to interfer with the LED strip we will install later. Drill the holes close the inner edge of the aluminum bar or you will not have enough room for the bolt
  • Screw the screws and bolts

imageimage

 

Building the four lateral panel

 

Parts list

To build the four lateral panels, you need

  • 4 pieces of bar with LED housing 50 cm in length
  • 4 pieces of L-shaped 30 mm x 20 mm x 1 mm aluminum bar 50 cm in length (referred as bar "A")

image

  • 4 pieces of L-shaped 20 mm x 20 mm x 1 mm aluminum bar 50 cm in length (referred as bar "B")

image

  • 4 pieces of 30 mm x 1 mm aluminum bar 50 cm in length (referred as bar "C")
  • Rivets. I used 3mm rivets, so I drilled the parts with a 3.3 mm bit
  • 4 50 cm x 50 cm plexiglass
  • 16 M4 x 20 mm screws with bolts

 

How to proceed

  1. Drill holes in bar "A" as shown in picture
  2. Mate the bar "A" with the LED aluminum bars and fix the parts with 2 rivets
  3. Drill holes in bar "B" as shown in picture
  4. Mate the bar "B" with the LED aluminum bars and fix the parts with 1 rivet
  5. Mate bar "C" with bar "A" leaving 20 mm from the edge of bar "A"
  6. Mate bar "C" with bar "B" leaving 20 mm from the edge of bar "B"
  7. Put the plexiglass in place and, with a 4 mm bit, drill 2 holes in bar "A" and two holes in bar "B"
  8. Screw the screws and bolts

image

 

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

Joining panels

Parts list

To join the panels, you need

  • 10 joints with a maximum height of 20 mm
  • 30 countersunk head screws and bolts

How to proceed

  • Take the bottom panel
  • Place the joint on the bar with LED housing, drill an hole for the screw and fix
  • Place one of the side panels with the plexiglass facing upside. Place the joint as shown, drill two holes for the screws and fix

imageimage

Refer to the assembly plan below for the location of the joints

image

 

Final result

This the Gr0G assembled and unfolded

image

 

UPDATE

while building the Gr0G box, I realized that a front door make access and inspection much easier. So I changed the layout as follow

image

Attachments:
Assembly.skp.zip
BarA.skp.zip
Clamp.skp.zip
Top.skp.zip
BarB.skp.zip
  • Sign in to reply

Top Comments

  • dubbie
    dubbie over 5 years ago +2
    Looks to be a clever assembly process. I picked up some good tips. I must get my hand riveter out and try this sometime. Dubbie
  • aspork42
    aspork42 over 5 years ago +1
    Nice build!
  • balearicdynamics
    balearicdynamics over 5 years ago +1
    Great!!! What a neat build Enrico
Parents
  • DAB
    DAB over 5 years ago

    Good job and nice design.

     

    DAB

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • DAB
    DAB over 5 years ago

    Good job and nice design.

     

    DAB