Path to Programmable
  • Challenges & Projects
  • Design Challenges
  • Path to Programmable
  • More
  • Cancel
Path to Programmable
Blog Path to Programmable: Final Projects and Graduation Awards
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
  • Author Author: rscasny
  • Date Created: 18 Feb 2019 5:27 PM Date Created
  • Views 4885 views
  • Likes 20 likes
  • Comments 17 comments
Related
Recommended

Path to Programmable: Final Projects and Graduation Awards

rscasny
rscasny
18 Feb 2019

In 2018, we had our first Path to Programmable class. I described how the class was conceived by the element14 team, and why we are committed to providing element14 members training on programmable logic devices in a previous blog, Final Words and Future Opportunities on the Path to Programmable: Summary, Projects, Conclusions and Thank Yous. Path to Programmable provide some of our member-engineers who had limited experience designing with programmable devices a training program. The trainees received a Development Board for MiniZed Single-core Zynq 7Z007S and we gave them access to the MiniZed Speedway Design training. Then we had them complete the training and labs while we monitored, read, and enjoyed their blogs.

 

Now we are ready to graduate our first class, with more classes to come. To graduate, a trainee had to complete all lessons and labs and create a project of their choice that included the MiniZed. I'll give you a brief of the projects below, but each trainee that accomplished these requirements will receive:

 

Designing with XilinxRegistered FPGAs: Using VivadoFLUKE 3000 FC -  Wireless Digital MultimeterPro's Kit Electronic Tool Kit
imageimageimage

 

So, without further adieu, here is a brief summary of the graduation projects:

 

image

A MiniZed WS2812 Controller

While this project could easily have been done with a microcontroller, and often is, avnrdf decided to build one with the Minized, using both its PS and PL. Here's how it works: "The WS2812 RGB LED uses a single wire serial protocol that infers '1's and '0's by varying the width of a pulse. The project moves the serial output generation & refresh to the PL. The idea is that software in the PL simply writes 'data' to an 'address' in the BRAM (which corresponds to the RGB data of a LED of a given index), and the logic in the PL independently iterates through all the data in the BRAM using the other port, refreshing the LEDs. the main parts are the application that runs in the PS, the AXI4-Lite interface, a custom AXI to BRAM interface, dual port BRAM, a custom BRAM to RGB interface and a RGB to WS2812 generator. I could have used memory mapped BRAM using the Xilinx AXI-BRAM IP, but decided to build a custom interface that uses registers."

 

Timer Interrupt Library

Designed by aspork42  and based in the FPGA fabric, "it generates an interrupt every "N" clock cycles; and I mapped it to the 48 MHz clock. This interrupt then feeds into the interrupt concatenator as interrupt #0. I used the IP Library to find new IP and import into my hardware design."

image

 

Continuing, "I then exported the hardware and made a new workspace & BSP in the SDK utility. I started with some base code in the SDK and got it working with my new hardware to run things. So I'm using both the PS + PL. I had to re-map the interrupt which was used in the base program to the one generated from Vivado."image

 

Video Gimbal Project with PMOD TDM114 Camera Module

This project started out as something interesting using the PMOD TDM114 camera module. To control the camera module, "I'm going to use a X-Y gimbal made from RC servos. I will run the servos from the MiniZed. To do this, I have modified the code from the IP training to run two RC servos instead (and addition to) the PL LEDs." (Designed by rsc)

 

Gamma Radiation Measurement with the Avnet MiniZed

This project was quite a surprise to me. But kk99  stated that "I have a really nice sensor module called GDK101 which measures gamma radiation in range up to 200 usV/h. This sensor has really simple communication interfaces: I2C or UART. There is also analog output which could be used for verifying the energy spectrum analysis of gamma photons." [His] plan [was] to use this module to measure gamma radiation and the energy spectrum analysis of gamma photons. The first step was to setup an I2C controller in PS of the MiniZed and communicate with sensor module. The second stop was to use the ADC sensor and create in PL a multichannel analyzer to see the spectrum. See the video below.

image

 

The Microphone Sub System

The microphones included on the Minized board are surface mount ST MP45DT02MP45DT02 MEMS (Micro-Electro-Mechanical Systems) connected directly to Zync - 7000 AP SoC on the MiniZed board. It can take the PDM (pulse density modulation) from the microphone and convert it to 16 bit PCM (pulse code modulation) in two's complement format at a decimated sampling rate suitable for audio. mconners found an example project that would help him. He already had a version of MATLAB, which was necessary to conduct this experiment. That, along with System Generator utility of the Vivado design suite allow him to model circuits in MATLAB, using Xilinx IP blocks, and then export that design out to Vivado to program the FPGA.image

 

 

 

 

Project - Minized as Web Server with Video Hosting on USB Pen drive

I built this project mainly out of my need to watch videos on multiple devices. I use it to see them on my laptop, tablet, mobile device, so I maintain a copy of videos on all these devices and believe me it is a hectic. So I had the Minized Board run a webserver using a Linux Image with Python Integration so that I can do server side programing using Python. The Python Server handles those Requests regarding Setting the Led Color and Interacting with Sensors, so all these can be done from our web browser Iself. For Implementing a Webserver on minized i needed to run an Application which handles TCP/IP and Application Layer in OSI model, moreover,  i need to connect to the Network through on board Murata 1DX WiFi module. (Designed by mu.udhay )

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

 

What's Next: Path To Programmable 2

I'd like to thank everyone who participated in the first Path to Programmable program. I'd also like to thank Xilinx and Avnet  for sponsoring the program. Finally, I'd like to thank our Web Designer Pauline Chan ( pchan ) for all the hard work in posting the program on element14.

 

We are already planning our next Path to Programmable program, open to all element14 members. The training is being developed right now for the Ultra96-V2  which will be the focus of Path 2. So, stay tuned. I will be making an announcement sometime in Spring 2019.

  • Sign in to reply

Top Comments

  • Fred27
    Fred27 over 7 years ago +8
    Some very nice projects there. Well done. Path to Programmable 2 sounds interesting but once again focuses on a very powerful programmable device. I wonder if a lot of members would also benefit from the…
  • DAB
    DAB over 7 years ago +6
    Another excellent element14 challenge. DAB
  • dougw
    dougw over 7 years ago +5
    Congratulations on making it through the course and thanks for blogging about it. Those are some very nice rewards. How many courses have you ever taken that came with such awards?
Parents
  • Fred27
    Fred27 over 7 years ago

    Some very nice projects there. Well done.

     

    Path to Programmable 2 sounds interesting but once again focuses on a very powerful programmable device. I wonder if a lot of members would also benefit from the simpler end of programmable logic - i.e. getting started with a more basic and slightly less daunting FPGA?

    • Cancel
    • Vote Up +8 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • Fred27
    Fred27 over 7 years ago

    Some very nice projects there. Well done.

     

    Path to Programmable 2 sounds interesting but once again focuses on a very powerful programmable device. I wonder if a lot of members would also benefit from the simpler end of programmable logic - i.e. getting started with a more basic and slightly less daunting FPGA?

    • Cancel
    • Vote Up +8 Vote Down
    • Sign in to reply
    • More
    • Cancel
Children
  • dubbie
    dubbie over 7 years ago in reply to Fred27

    David,

     

    I agree that something much simpler would be helpful for those of us with even less knowledge than these participants must have. I don't even understand some of the projects so it is unlikely I'll understand the implementation. What about flashing an LED? I know it's simple but I always use that as my starting point with new technologies and programming languages and work my way outwards from there.

     

    Dubbie

    • Cancel
    • Vote Up +5 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • 14rhb
    14rhb over 7 years ago in reply to Fred27

    Something like the Lattice iCEstick perhaps ? Product LinkProduct Link

    image

    Rod

    • Cancel
    • Vote Up +4 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • dubbie
    dubbie over 7 years ago in reply to 14rhb

    Rod,

     

    This looks just like the sort of thing that I could cope with. It seems easy to use, not too complex but enough complexity to be worthwhile. I might buy one but they seem to be out of stock. I may have to wait until they become available again.

     

    Dubbie

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • 14rhb
    14rhb over 7 years ago in reply to dubbie

    Hi Dubbie,

     

    I've never used one but would think, being smaller devices, they should be easier to understand than a top range FPGA. I wanted to get one with my recent prize cart but as you note they are out of stock. They aren't new but perhaps Element14 could do a project/challenge/roadtest with them ?

     

    Back some 20 years ago I bought a Lattice Semiconductors Dev kit from Farnell - it was based on the In System Programmable Devices they had at the time (ispLSI range) - I think they were CPLD as once programmed they held the setup permanently. I found those really easy to understand and setup - the IDE I used was visual with drag and drop of the logic symbols and then wire them together. It kind of worked with how my brain undertook digital design image

     

    I do think this iCEstick looks cool though.

     

    Rod

    • Cancel
    • Vote Up +4 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • Fred27
    Fred27 over 7 years ago in reply to 14rhb

    I had a lot of deliberation over what manufacturer to get started with for FPGAs, as I wanted to stick to one toolchain and not jump around. I received a lot of good (but sometimes conflicting) advice here: Where to start for an easy intro to FPGAs?

     

    In the end I went with Xilinx. They have a great range of FPGAs and SoCs at the top end. They also have much simpler CPLDs (Coolrunner and XC9500XL) at the lower end - slightly old tech in some ways but simpler and no need for external flash. I feel I made a good choice, although I'm sure there are a lot of good points for other FPGA manufacturers too.

    • Cancel
    • Vote Up +4 Vote Down