PiCasso Design Challenge
  • Challenges & Projects
  • Design Challenges
  • PiCasso Design Challenge
  • More
  • Cancel
PiCasso Design Challenge
Blog Hologram Pi-ramid - 3D printed parts and initial assembly
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
  • Author Author: luislabmo
  • Date Created: 8 Apr 2019 2:44 AM Date Created
  • Views 3693 views
  • Likes 9 likes
  • Comments 16 comments
  • pla
  • picasso
  • luislab
  • 3d printed
Related
Recommended

Hologram Pi-ramid - 3D printed parts and initial assembly

luislabmo
luislabmo
8 Apr 2019

Once I was happy with all necessary the details in my project design, I started 3d-printing all the parts required to begin testing the assembly which overall is looking really good!.

image

 

3-D Print settings

Below the settings used:

  • Printer: Creality CR-10S -a big thanks to Element14 for this awesome price!
  • Material: PLA Blue-denim
  • Infill: 15%, triangles
  • Adhesion: Brim
  • Supports: No
  • Layer height: 0.2mm

image

 

Assembly and materials required

It didn't make much sense to me to incorporate snap-fit features to the general assembly since the overall structure will have to support the weight of the RPi + Touchscreen mainly. Also I would most likely be assembling/disassembling several times the project while it evolves. With all of the above in mind, it made sense to add holes for screws to the project -which require to be tapped as threads that small are hard to replicate in a 3d printed part. Below the list of screws I will be using to assemble the project:

 

  • 2 x #2 x 3/8" Slotted Round Head Screws
  • 6 x #5-40 x 3/8" Socket Head Cap Screws
  • 2 x #6-32 x 2" Socket Head Cap Screws

 

{gallery:width=960,height=768,autoplay=false} Hologram Pi-ramid - Initial assembly

image

Hologram Pi-ramid hardware: #2 x 3/8" and #6-32 x 2" screws

image

Hologram Pi-ramid hardware: #5-40 x 3/8" screws

image

Hologram Pi-ramid: Some tools needed for the 3d printed parts assembly

image

Hologram Pi-ramid: Tapping #5-40 holes with a 3d printed tap wrench

image

Hologram Pi-ramid: Tapped holes #5-40

 

 

Blogs in this series

 

  1. Hologram Pi-ramid - Intro and initial design
  2. Hologram Pi-ramid - 3D CAD/CAM design
  3. Hologram Pi-ramid - 3D printed parts and initial assembly
  4. Hologram Pi-ramid - Plexiglass Pyramid
  5. Hologram Pi-ramid - My name is Automan
  6. Hologram Pi-ramid - PCB Design
  7. Hologram Pi-ramid - Painting the 3D printed parts
  8. Hologram Pi-ramid - Electronic Parts
  9. Hologram Pi-ramid - Displaying Holograms
  10. Hologram Pi-ramid - Project complete!

 

  • My Picasso Design Challenge entries

 

 

image
3D CAD/CAM design

image
Plexiglass Pyramid

  • Sign in to reply

Top Comments

  • genebren
    genebren over 7 years ago +4
    Solid looking work there. I see that you are using 15% infill, do you have any issues when it comes to tapping the threads? Good luck on your future developments on this design challenge. Gene
  • luislabmo
    luislabmo over 7 years ago in reply to dubbie +4
    Hello Dubbie, I think 85% infill is high as a default/for average parts, usually you will need something around 15% to 20% just to give some internal volume to the parts and also to help features of the…
  • balearicdynamics
    balearicdynamics over 7 years ago in reply to luislabmo +4
    Hi, despite the fact that the shell thickness should be a multiple of the nozzle diameter - for an obvious reason - I use a higher thickness just for the parts that need some post-production like sanding…
Parents
  • dubbie
    dubbie over 7 years ago

    Luis,

     

    That is some impressive 3D printing. I may have to think about changing mine as I don't think it could do that.

     

    I'm also impressed that you are using only 15% infill. I use 85% usually and it still isn't all that good and often cracks or snaps when parts are being 'eased' together. The last time I used 100% but that didn't seem to come out correct as it was very rough.

     

    Dubbie

    l

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • balearicdynamics
    balearicdynamics over 7 years ago in reply to dubbie

    Dubbie, the problems maybe just your too high percentage of infill...

     

    Write me an email, maybe I can send you something useful, to try before changing the 3D printer image

     

    Enrico

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • balearicdynamics
    balearicdynamics over 7 years ago in reply to dubbie

    Dubbie, the problems maybe just your too high percentage of infill...

     

    Write me an email, maybe I can send you something useful, to try before changing the 3D printer image

     

    Enrico