PiCasso Design Challenge
  • Challenges & Projects
  • Design Challenges
  • PiCasso Design Challenge
  • More
  • Cancel
PiCasso Design Challenge
Blog Hologram Pi-ramid - 3D printed parts and initial assembly
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
  • Author Author: luislabmo
  • Date Created: 8 Apr 2019 2:44 AM Date Created
  • Views 3710 views
  • Likes 9 likes
  • Comments 16 comments
  • pla
  • picasso
  • luislab
  • 3d printed
Related
Recommended

Hologram Pi-ramid - 3D printed parts and initial assembly

luislabmo
luislabmo
8 Apr 2019

Once I was happy with all necessary the details in my project design, I started 3d-printing all the parts required to begin testing the assembly which overall is looking really good!.

image

 

3-D Print settings

Below the settings used:

  • Printer: Creality CR-10S -a big thanks to Element14 for this awesome price!
  • Material: PLA Blue-denim
  • Infill: 15%, triangles
  • Adhesion: Brim
  • Supports: No
  • Layer height: 0.2mm

image

 

Assembly and materials required

It didn't make much sense to me to incorporate snap-fit features to the general assembly since the overall structure will have to support the weight of the RPi + Touchscreen mainly. Also I would most likely be assembling/disassembling several times the project while it evolves. With all of the above in mind, it made sense to add holes for screws to the project -which require to be tapped as threads that small are hard to replicate in a 3d printed part. Below the list of screws I will be using to assemble the project:

 

  • 2 x #2 x 3/8" Slotted Round Head Screws
  • 6 x #5-40 x 3/8" Socket Head Cap Screws
  • 2 x #6-32 x 2" Socket Head Cap Screws

 

{gallery:width=960,height=768,autoplay=false} Hologram Pi-ramid - Initial assembly

image

Hologram Pi-ramid hardware: #2 x 3/8" and #6-32 x 2" screws

image

Hologram Pi-ramid hardware: #5-40 x 3/8" screws

image

Hologram Pi-ramid: Some tools needed for the 3d printed parts assembly

image

Hologram Pi-ramid: Tapping #5-40 holes with a 3d printed tap wrench

image

Hologram Pi-ramid: Tapped holes #5-40

 

 

Blogs in this series

 

  1. Hologram Pi-ramid - Intro and initial design
  2. Hologram Pi-ramid - 3D CAD/CAM design
  3. Hologram Pi-ramid - 3D printed parts and initial assembly
  4. Hologram Pi-ramid - Plexiglass Pyramid
  5. Hologram Pi-ramid - My name is Automan
  6. Hologram Pi-ramid - PCB Design
  7. Hologram Pi-ramid - Painting the 3D printed parts
  8. Hologram Pi-ramid - Electronic Parts
  9. Hologram Pi-ramid - Displaying Holograms
  10. Hologram Pi-ramid - Project complete!

 

  • My Picasso Design Challenge entries

 

 

image
3D CAD/CAM design

image
Plexiglass Pyramid

  • Sign in to reply

Top Comments

  • genebren
    genebren over 7 years ago +4
    Solid looking work there. I see that you are using 15% infill, do you have any issues when it comes to tapping the threads? Good luck on your future developments on this design challenge. Gene
  • luislabmo
    luislabmo over 7 years ago in reply to dubbie +4
    Hello Dubbie, I think 85% infill is high as a default/for average parts, usually you will need something around 15% to 20% just to give some internal volume to the parts and also to help features of the…
  • balearicdynamics
    balearicdynamics over 7 years ago in reply to luislabmo +4
    Hi, despite the fact that the shell thickness should be a multiple of the nozzle diameter - for an obvious reason - I use a higher thickness just for the parts that need some post-production like sanding…
Parents
  • genebren
    genebren over 7 years ago

    Solid looking work there.  I see that you are using 15% infill, do you have any issues when it comes to tapping the threads?

     

    Good luck on your future developments on this design challenge.

     

    Gene

    • Cancel
    • Vote Up +4 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • genebren
    genebren over 7 years ago

    Solid looking work there.  I see that you are using 15% infill, do you have any issues when it comes to tapping the threads?

     

    Good luck on your future developments on this design challenge.

     

    Gene

    • Cancel
    • Vote Up +4 Vote Down
    • Sign in to reply
    • More
    • Cancel
Children
  • luislabmo
    luislabmo over 7 years ago in reply to genebren

    Hello Gene, thank you for your kind comments!. I don’t have any issues when tapping the holes as I include them in the design with the right size (diameter and depth). They will have enough material to be removed when tapping -the amount of material should be the wall thickness which is 0.8mm in my current settings.

     

    if you look closely at the second picture of the assembly, the part on the left is tapped but the one on the right isn’t.

    image

     

    Hope this answers your question.

     

    Luis

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • e14phil
    e14phil over 7 years ago in reply to luislabmo

    Hey luislabmo

     

    I am loving this and will have to build one my self!

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • luislabmo
    luislabmo over 7 years ago in reply to e14phil

    Thanks Phil!. I'm planning to have a final blog post with a wrap-up summary which will include everything needed image

    • Cancel
    • Vote Up +3 Vote Down