Once I was happy with all necessary the details in my project design, I started 3d-printing all the parts required to begin testing the assembly which overall is looking really good!.
3-D Print settings
Below the settings used:
- Printer: Creality CR-10S -a big thanks to Element14 for this awesome price!
- Material: PLA Blue-denim
- Infill: 15%, triangles
- Adhesion: Brim
- Supports: No
- Layer height: 0.2mm
Assembly and materials required
It didn't make much sense to me to incorporate snap-fit features to the general assembly since the overall structure will have to support the weight of the RPi + Touchscreen mainly. Also I would most likely be assembling/disassembling several times the project while it evolves. With all of the above in mind, it made sense to add holes for screws to the project -which require to be tapped as threads that small are hard to replicate in a 3d printed part. Below the list of screws I will be using to assemble the project:
- 2 x #2 x 3/8" Slotted Round Head Screws
- 6 x #5-40 x 3/8" Socket Head Cap Screws
- 2 x #6-32 x 2" Socket Head Cap Screws
| {gallery:width=960,height=768,autoplay=false} Hologram Pi-ramid - Initial assembly |
|---|
Hologram Pi-ramid hardware: #2 x 3/8" and #6-32 x 2" screws |
Hologram Pi-ramid hardware: #5-40 x 3/8" screws |
Hologram Pi-ramid: Some tools needed for the 3d printed parts assembly |
Hologram Pi-ramid: Tapping #5-40 holes with a 3d printed tap wrench |
Hologram Pi-ramid: Tapped holes #5-40 |
Blogs in this series
- Hologram Pi-ramid - Intro and initial design
- Hologram Pi-ramid - 3D CAD/CAM design
- Hologram Pi-ramid - 3D printed parts and initial assembly
- Hologram Pi-ramid - Plexiglass Pyramid
- Hologram Pi-ramid - My name is Automan
- Hologram Pi-ramid - PCB Design
- Hologram Pi-ramid - Painting the 3D printed parts
- Hologram Pi-ramid - Electronic Parts
- Hologram Pi-ramid - Displaying Holograms
- Hologram Pi-ramid - Project complete!









Top Comments
-
kiri-ll
-
Cancel
-
Vote Up
+3
Vote Down
-
-
Sign in to reply
-
More
-
Cancel
Comment-
kiri-ll
-
Cancel
-
Vote Up
+3
Vote Down
-
-
Sign in to reply
-
More
-
Cancel
Children