Save The Bees Design Challenge
  • Challenges & Projects
  • Design Challenges
  • Save The Bees Design Challenge
  • More
  • Cancel
Save The Bees Design Challenge
Blog BeeWatch: LoRaWAN Environmental Monitoring – Blog 2: Unboxing the Kit
  • Blog
  • Forum
  • Documents
  • Leaderboard
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Save The Bees Design Challenge to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: Gough Lui
  • Date Created: 5 Mar 2023 6:46 AM Date Created
  • Views 1980 views
  • Likes 9 likes
  • Comments 5 comments
  • save the bees
  • savethebeesch
  • nicla vision
  • lorawan
  • lora
  • arduino pro
  • mkr1310
  • arduino
Related
Recommended

BeeWatch: LoRaWAN Environmental Monitoring – Blog 2: Unboxing the Kit

Gough Lui
Gough Lui
5 Mar 2023
BeeWatch: LoRaWAN Environmental Monitoring – Blog 2: Unboxing the Kit

While the challenge started a while back and some competitors have been able to race forward, I’ve been patiently awaiting the arrival of the kit before pressing much further. In the meantime, I’ve also been obtaining other parts which may be useful or necessary in-parallel, while juggling plenty of other commitments. Let’s take a look at what was provided.

Table of Contents

  • Unboxing
  • Batteries not included!
  • Conclusion

Unboxing

The kit arrived at my doorstep on Wednesday 22nd February 2023 and was a relatively small and light box. I suppose this was not unexpected as there are just two boards inside.

image

The box was packed with bubble-wrap to keep everything safe and sound.

image

Two genuine Arduino products in their boxes.

image

The MKR WAN 1310 uses an Atmel SAMD21 containing 256kB flash and 32kB RAM, clocked at 48MHz. This board has an onboard LoRa module from Murata and is a 3.3V-based board with the MKR form factor.

image image

image image

As with all official Arduino boards, it is Made in Italy and carries an authentication hologram.

image

Inside, the board is packed inside an anti-static foam. There is a label sheet and a thank-you leaflet.

image

The board itself with the MKR form factor is not dissimilar in concept to the Adafruit Feather but is incompatible. It has a set of pass-through headers offering connectivity, onboard battery charging and battery management for a lithium-polymer cell and a Quic I2C header. The microUSB-B port provides programming and charging connectivity.

image

Everything of importance is mounted on the top-side of the board, with the bottom containing helpful silkscreen.

image

Customised pin headers label the pin functions on the sides for additional convenience.

image

A closer look at the board shows the BQ24195 battery management IC, the Atmel ATSAMD21 microcontroller, clock crystal and the ATECC508A secure element.

image

This second close-up shows the Murata CMWX1ZZABZ LoRa module, a Winbond 25Q16JV1Q 16Mbit SPI NOR flash memory.

image image

image image

The Arduino Pro Nicla Vision comes in its own small board, with a black and green colour scheme that typifies the “pro” series of boards. It too, has a hologram for authentication and is Made in Italy.

image

This board is made in partnership with OpenMV.

image

Inside, the board is wrapped in a small anti-static bag with a leaflet and a flexible self-adhesive Molex antenna.

image

The board itself is more like a module, but does have a micro USB-B connection for direct connection to a computer. They’ve really packed as much as they can onto the board – having castellated pads as well as pin-header holes. The datasheet gives a comprehensive overview of the board and its components.

image
image

Components on the bottom at the top include a 6-axis IMU, a voltage level shifter and a crypto IC, but the components are not easily identified. Components towards the bottom of the rear seem concerned with power and battery, being ideal diodes, level shifter and a fuel gauge IC.

image

The other side of the board has the camera (with protective film), the main STM32H747AII6 Dual ARM Cortex M7/M4 microcontroller clocked at 480MHz/240MHz with 2MB Flash and 1MB RAM, an SMSC USB3320C USB transciever, a Murata 1DX Wi-Fi/Bluetooth module, a 25QL128A 16MiB SPI flash and a NXP MC34PF1550 PMIC. Two small MEMS oscillators provide clock references.

image

In the corner, and easily missed, are the PDM microphone and infrared time-of-flight distance sensor (ST VL53L1CB FlightSense). The latter is covered by protective tape that must be removed prior to use.

The Nicla Vision board is a lot more complex and densely packed than I could imagine. I’m surprised they were able to pack so many things onto such a tiny board!

Batteries not included!

Looking at the two boards, the MKR WAN 1310 is the logical starting point. Unfortunately, having the board on its own is not enough to get started. Hardware wise, a USB-A to USB-microB cable is needed to power and program the board, a breadboard would be good to prototype with, a compatible lithium-polymer battery would be needed if the board is expected to run without USB connection and most-crucially, an antenna is required.

I suspect the latter requirement is something not everyone can rummage around their junk box and solve easily. The board has an IPEX MHF I/u.FL connector which is similar to the ones you might find on laptop Wireless LAN cards and needs to be connected to an antenna that supports the bands you intend to use. For LoRa/LoRaWAN, this may mean EU868, US915, AU915, AS923 etc. Thus an antenna that covers the 900MHz ISM band is most desirable.

The best way is to use a pigtail that converts the MHF/u.FL to SMA (or in some cases RP-SMA) and then screw on a full-size SMA/RP-SMA whip antenna for the best range and flexibility.

image

Another option, especially for those who have a Molex Antenna Kit handy is to use some of the flexible multi-band printed self-adhesive antennas. There is a specific antenna that matches the band (105262), as well as multi-band cellular antennas (105263, 146185) which seem to have adequate coverage of the frequencies used.

image

Without this part, it would not really be possible to use the LoRaWAN radio module as there is no onboard antenna. This is somewhat understandable – antennas for such a low frequency are physically large to be efficient, and the MKR form factor is quite small by comparison. However, should people get desperate, my advice would be to remove the SMD resistor that connects the antenna trace to the MHF connector and solder down a quarter-wavelength piece of wire (8.1cm) as an antenna. This may not be optimal, but it will let you get on the air quickly. Assuming you don’t destroy the pads, you can undo the modification by soldering in the SMD resistor again.

Similarly, the Arduino Pro Nicla Vision board requires a similar USB cable for connectivity and seems to have a very specific slim battery connection which I’ve not previously used. It does have an MHF/u.FL connector for an antenna, but they’ve been nice enough to include a Molex 206994 self-adhesive 2.4/5GHz flexible antenna.

Conclusion

At last, the kit has arrived and it’s time to get started. I’ll be tackling getting the MKR WAN 1310 up and running on LoRaWAN first, before worrying about how it can be made standalone, PV-solar and battery-powered. The Nicla Vision will have to wait a bit – it’s the part I have the least experience with, so it’s probably going to take me a while to get up and running.

Thankfully, the challenge deadline has been extended – the project now ends 28th April 2023, giving us all a bit more time to get everything built. I probably won’t be winning any major prize, but the chance to get some practical experience with LoRaWAN with the MKR WAN 1310 is perhaps my main short-term goal.

[[BeeWatch Blog Index]]

  • Blog 1: README.TXT
  • Blog 2: Unboxing the Kit
  • Blog 3: LoRa vs. LoRaWAN & Getting Started with MKR WAN 1310
  • Blog 4: LoRaWAN Gateway Set-Up & MKR WAN 1310 Quirks
  • Blog 5: Power, State Saving, Using Sensors & Battery
  • Blog 6: Particulate Monitoring & Solar Power Input
  • Blog 7: Powered by the Sun & Initial Data
  • Blog 8: Getting Started with Nicla Vision
  • Blog 9: Nicla Vision IR ToF & Audio Sensing, Data Dump
  • Blog 10: Nicla Vision Power, Saving B’s & Dashboard Woes
  • Blog 11: Summary Conclusion
  • Sign in to reply
  • Gough Lui
    Gough Lui over 3 years ago in reply to embeddedguy

    There is no "big secret" - I just use a Nikon D3400 DSLR, some decent quality glass (Tamron 17-50mm f/2.8, Nikon 105mm f/2.8 Macro), take all my shots in RAW, have three flash-guns with diffusers, a white benchtop with some white paper background and process all my images in Adobe Lightroom by hand.

    It always helps when you use decent equipment and set it up properly.

    - Gough

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • embeddedguy
    embeddedguy over 3 years ago

    What is the secret behind so good image quality? Relaxed

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • ntewinkel
    ntewinkel over 3 years ago

    I'm happy to see you have some antenna choices!

    I suspect others may run into issues due to the missing antenna. It's unfortunate the organizers didn't spot this in time to drop in some kind of big antenna.

    I'm about to head for the back deck of the carriage house to see if I can get a connection with my little GPS antenna Sweat smile

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • Gough Lui
    Gough Lui over 3 years ago in reply to shabaz

    I suspect the small size made it difficult for them to squeeze an antenna into the MKR form factor, although if they could somehow "squeeze" a reasonably performing antenna into the PCB, they may offer a movable jumper resistor selection to choose an external antenna or use a connector with internal switch (there are variations where plugging an antenna in will disconnect the downstream onboard antenna).

    That being said ... you may be a little prophetic here, as the u.FL connector and pigtail does become a source of problems/confusion in later parts ... (story unfolding in future blogs ...)

    - Gough

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • shabaz
    shabaz over 3 years ago

    Hi Gough,

    Nice set of parts for a project!

    Perhaps the ideal scenario would have been for there to be two variants of the MKR board, one with antenna built-in. Personally I always think I'm going to damage the board when using small U.FL connectors, but I guess it makes sense to use them since they are so popular, and low-cost.