Safe and Sound
  • Challenges & Projects
  • Design Challenges
  • Safe and Sound
  • More
  • Cancel
Safe and Sound
Blog MSP432 and TI-RTOS: Getting Started Pt. 2 - Add an ADC Sample Task
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
  • Author Author: Jan Cumps
  • Date Created: 3 Jan 2017 11:32 AM Date Created
  • Views 3122 views
  • Likes 8 likes
  • Comments 7 comments
  • safe and sound
  • msp432
  • ti-rtos
  • launchpad
  • ti_rt
Related
Recommended

MSP432 and TI-RTOS: Getting Started Pt. 2 - Add an ADC Sample Task

Jan Cumps
Jan Cumps
3 Jan 2017

Part 2 in a series that gets you RTOS-ready for the MSP432 LaunchPad

 

image

 

When you complete this example, you have a basic RTOS setup that integrates USB, ADC and a blinky. You can use Tasks, Semaphores and a UART interrupt. And you'll know how to register Tasks in the TI-RTOS configuration editor.

 

Part 1 sets up the project, explains how to configure a task and gets the Blinky running.

Part 2 adds an ADC Sample Task.

 

What you need:

  • MSP432 LaunchPad
  • 1 micro-USB cable
  • Code Composer Studio
  • TI-RTOS for MSP43X
  • two potentiometers (say 10K or more, not critical), a little breadboard and a few wires

 

We're staring where we stopped in part 1. We'll add a task that samples two ADC pins.

The results get logged to the Code Composer Studio console.

We'll use two potentiometers to set and change the voltage on the two ADC pins.

 

Configure the ADC Driver in RTOS

First, let's set our sample strategy in the source file MSP_EXP432P401R.c.

This file standard has different settings for ADC0 and ADC1. Let's make them the same for this exercise.

 

/* ADC configuration structure */
const ADCMSP432_HWAttrs adcMSP432HWAttrs[MSP_EXP432P401R_ADCCOUNT] = {
    {
        .channel = ADC_INPUT_A0,
        .gpioPort = GPIO_PORT_P5,
        .gpioPin = GPIO_PIN5,
        .gpioMode = GPIO_TERTIARY_MODULE_FUNCTION,
        .refVoltage = REF_A_VREF2_5V,
        .resolution = ADC_14BIT
    },
    {
        .channel = ADC_INPUT_A1,
        .gpioPort = GPIO_PORT_P5,
        .gpioPin = GPIO_PIN4,
        .gpioMode = GPIO_TERTIARY_MODULE_FUNCTION,
        .refVoltage = REF_A_VREF2_5V,
        .resolution = ADC_14BIT
    }
};

 

The ADC reference voltage is 2.5V - when testing the exercise later, don't supply more than 2.5V on the pins.

They can take 3.3V, but you'll get an overflow as soon as you exceed the reference voltage.

 

In the main() function in datalogger.c, add the ADC driver initialisation.

 

int main(void)
{
    /* Call board init functions */
    Board_initGeneral();
    Board_initGPIO();
    Board_initADC();
    // ...

 

This is a good time to build and run the project. It should compile without errors and the LED should blink as it did in part 1.

 

Add the ADC Task

 

The ADC task will run every 10 seconds, sample the two ADC pins and log the results to the CCS console.

Then it gives control back to RTOS, so that it can spend time to other activities (or go idle and put the controller to a lower power mode).

But first our task configeres the two ADC pins.

 

Create a new source file adc_sample.c.

Enter this code in that file.

/* XDCtools Header files */
#include <xdc/std.h>
#include <xdc/runtime/System.h>
#include <xdc/runtime/Error.h>

/* BIOS Header files */
#include <ti/sysbios/BIOS.h>
#include <ti/sysbios/knl/Task.h>
#include <ti/sysbios/knl/Clock.h>

/* TI-RTOS Header files */
#include <ti/drivers/ADC.h>

/* Example/Board Header files */
#include "Board.h"

/*
 *  ======== taskAdcSample ========
 *  Open an ADC instance and get a sampling result from a one-shot conversion.
 */
Void taskAdcSample(UArg arg0, UArg arg1)
{
    ADC_Handle   adc0;
    ADC_Handle   adc1;
    ADC_Params   params;
    uint16_t adcValue0;
    uint16_t adcValue1;
    ADC_Params_init(&params);
    adc0 = ADC_open(Board_ADC0, &params);
    adc1 = ADC_open(Board_ADC1, &params);

    while (1) {
        Task_sleep(((UInt)arg0) / Clock_tickPeriod);
        /* Blocking mode conversion */
        ADC_convert(adc0, &adcValue0);
        ADC_convert(adc1, &adcValue1);
        System_printf("Sample %u:%u\n", adcValue0, adcValue1);
        /* SysMin will only print to the console when you call flush or exit */
        System_flush();
    }
    // theoretically close the ADC driver. This code is never reached
//    ADC_close(adc0);
//    ADC_close(adc1);
}

 

Then add the task to the RTOS configuration. Open the editor by double-clicking datalogger.cfg.

 

image

Save all files and rebuild.

You can execute the program. It will give random-ish readouts in the console because there's nothing connected to the ADC pins yet.

 

Hardware

 

Put your two potentiometers on the breadboard. Their value isn't that important. Anything between 10K and 1M is certainly ok. They don't need to have the same value. Whatever you have at home.

We'll use them to divide the 3V3 level of the launchpad, and send the value at the potentiometer's wiper to ADC0 and ADC1.

 

Wire the 3V3 of your LaunchPad to one sie of each potentiometer, GND to the other side.

The wiper of one goes to P5.4 and P5.5.

 

image

 

Set both potentiometers to the middle, plug the LaunchPad in the USB and start a debug session.

You'll see the values appear in the console.

 

Turn the potentiometers to see the values change. Once the wiper is above the reference value 2.5V, the results will not change because you've overrun the range.

 

image

 

 

Result

 

[CORTEX_M4_0] Starting the example
System provider is set to SysMin. Halt the target to view any SysMin contents in ROV.
Sample 5140: 3617
Sample 2620: 1194
Sample 1084: 426
Sample 459: 219
Sample 466: 272
Sample 380: 191
Sample 412: 205
Sample 380: 198
Sample 220: 90
Sample 220: 118
Sample 348: 303
Sample 259: 215
Sample 188: 91
Sample 211: 123
Sample 380: 223
Sample 233: 137
Sample 316: 165
Sample 252: 97
Sample 444: 209
Sample 230: 94
Sample 261: 61
Sample 380: 130
Sample 412: 211
Sample 207: 103
Sample 252: 95
Sample 252: 136

 

 

 

TI-RTOS Series
MSP432 and TI-RTOS: Getting Started Pt. 1 - Set Up and 1st RTOS Task
MSP432 and TI-RTOS: Getting Started Pt. 2 - Add an ADC Sample Task
MSP432 and TI-RTOS: Getting Started Pt. 3 - USB with Minimal CPU Use
MSP432 and TI-RTOS: PWM
MSP432 and TI-RTOS: I2C Configuration for Sensors BoosterPack
MSP432 and TI-RTOS: another I2C example - talk to a DAC
MSP432 and TI-RTOS: Sharp LCD BoosterPack
MSP432 and TI-RTOS: PID Library Part 1 - Intro
MSP432 and TI-RTOS: PID Library Part 2 - Real World Example
  • Sign in to reply

Top Comments

  • Jan Cumps
    Jan Cumps over 9 years ago +1
    Debug and real-time scheduling don't play well together. But there's more than that that can go wrong. can you upload your project somewhere? it makes it easier to replicate your situation.
  • fredws
    fredws over 8 years ago +1
    Thought while I was at it, I looked at timing in adc routine with printing and without printing. Routine takes at least 60 microseconds to process an ADC convert routine. With the print routine, it takes…
Parents
  • fredws
    fredws over 8 years ago

    In case anyone is wondering, the clock Module shows the Tick period (us).

    This is default to 1000 microseconds per tick generated, or one Tick per millisecond.

    This 1 millisecond rate is what Is used as a time source for the Task Argument 0 value in this example.

    so ADC Task Argument 0 = 10000 related to 10,000 milliseconds if used with Task_sleep((UInt)arg0);

     

    image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • fredws
    fredws over 8 years ago

    In case anyone is wondering, the clock Module shows the Tick period (us).

    This is default to 1000 microseconds per tick generated, or one Tick per millisecond.

    This 1 millisecond rate is what Is used as a time source for the Task Argument 0 value in this example.

    so ADC Task Argument 0 = 10000 related to 10,000 milliseconds if used with Task_sleep((UInt)arg0);