Upcycle It
  • Challenges & Projects
  • Design Challenges
  • Upcycle It
  • More
  • Cancel
Upcycle It
Blog [Upcycle it Design Challenge] Embedded Web SDR client on Analog Radio Receiver #7: Hardware is ready!
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
  • Author Author: konstantinoskonstas
  • Date Created: 10 May 2017 2:23 PM Date Created
  • Views 2348 views
  • Likes 4 likes
  • Comments 7 comments
  • web sdr
  • upcycled_sdr
  • hardware finished
Related
Recommended

[Upcycle it Design Challenge] Embedded Web SDR client on Analog Radio Receiver #7: Hardware is ready!

konstantinoskonstas
konstantinoskonstas
10 May 2017

Meet with Edison Hardware for the second time

 

It took a little bit more than I expected to get the components from Sparkfun to go on with the project.

Eventually they arrived yesterday afternoon, so I started work right away.

Meanwhile I had prepared the first version of the program that I had previously written for the Arduino, re-writing it in node.js to suit my needs.

I was expecting for the boards to visualize the actual size of the display and how the menu would look on such a small display. When I opened the package, everyone in the house made the comment that the display was tiny. So I had to see with my eyes.

image

I put all the pieces on the table. The two boards, the Edison core and the necessary screws to mount everything together, Good thing that I order the screws that helped to turn all the components into a firm project.

I only had to solder a two pin male header on the display board for the power, which I did first.

Then I put the pieces together as you can see in the next pictures and applied power from a 5 volt wall-wart.

image


imageimageimage

 

As there was no software loaded for the display, the only thing that I could notice was a blue led that went on on the base board.

I opened PuTTY on my computer and easily logged on my new Edison system, Obelix.localhost. From the site https://www.npmjs.com/package/edison-oled I got the instructions on how to install the OLED display under node.js .

So I run:

$ npm install edison-oled

and the display was installed again without a problem out of the box.

I looked at the sub-dir that was created “edison-oled” under root@obelix:~/node_modules# and I found the following files:

root@obelix:~/node_modules/edison-oled# ls
README.md edison_node.hpp index.js oled sparklibs.h
binding.gyp edison_node_addon.cpp makefile oled_pong.cpp spi
build gpio node_modules package.json tests

I then did

root@obelix:~/node_modules/edison-oled# cd tests
root@obelix:~/node_modules/edison-oled/tests# node test-oled-screen.js

and yes the screen demo was working as it should be, together with the joystick and buttons control.

All right. The hardware was ready.

Next test.

root@obelix:~/node_modules/edison-oled/tests# node test11.js

and here is the result.

image

This was test one anyway. It was working as it was meant to be, on screen level again.

I had used a simple font for the display that allowed me to have on the 64 x 48 matrix 5 lines of ten characters each of the same font. Not exactly what I wanted, but I could start playing now quite easily.

So I stopped at this point to prepare my post and think.

Well everyone was happy because although the screen looked tiny, the display was very bright and everyone in the house could read it.

I started thinking now of the best possible way to produce a practical UI for my WEB SDR client.

One idea that came before sleep. The sign on message could stay on for a few seconds as a greeting message and then go away. I could then keep the next 3 lines on the OLED with Mode, Step, and Band info and make the Frequency line double size, as I had initially envisioned.

Well these are the small details that I have to play with from now on until I come to the desired result that I will present to you next week.

Although a day behind schedule, everything went on as it should have been.

After all I am through with the hardware, just add the USB Soundcard with a small cable.

Goal Number One achieved. It is the smallest footprint I could imagine, slightly larger than an Edison core! It surely can fit in many Radios for Upcycling them, even what we used to call Transistor Radios!

Till the next week.

 

Published Posts
[Upcycle it Design Challenge] Embedded Web SDR client on Analog Radio Receiver #1: Introduction
[Upcycle it Design Challenge] Embedded Web SDR client on Analog Radio Receiver #2: Software Concept
[Upcycle it Design Challenge] Embedded Web SDR client on Analog Radio Receiver #3: Meeting with Edison
[Upcycle it Design Challenge] Embedded Web SDR client on Analog Radio Receiver #4: Software Challenges with Edison
[Upcycle it Design Challenge] Embedded Web SDR client on Analog Radio Receiver #5: The Software Challenge goes on
[Upcycle it Design Challenge] Embedded Web SDR client on Analog Radio Receiver #6: Changing the Display
[Upcycle it Design Challenge] Embedded Web SDR client on Analog Radio Receiver #7: Hardware is ready!
[Upcycle it Design Challenge] Embedded Web SDR client on Analog Radio Receiver #8: Problem with Audio.
[Upcycle it Design Challenge] Embedded Web SDR client on Analog Radio Receiver #9: Problem with Browser
[Upcycle it Design Challenge] Embedded Web SDR client on Analog Radio Receiver #10: Making the Web SDR Client work!
[Upcycle it Design Challenge] Embedded Web SDR client on Analog Radio Receiver #11: One of its kind!
  • Sign in to reply

Top Comments

  • konstantinoskonstas
    konstantinoskonstas over 9 years ago in reply to Workshopshed +1
    Workshopshed Hello Andy, Thanks a lot for your comment and your very valuable information about the hardware - hardware.
  • konstantinoskonstas
    konstantinoskonstas over 9 years ago in reply to DAB +1
    DAB It is surprisingly readable for the bare eyes of a 66 years person. Seeing is believing. The range of the radio board is Long Wave (153 KHz) to 30 MHz in Short Wave plus FM (87,5 to 108 MHz). But the…
  • konstantinoskonstas
    konstantinoskonstas over 9 years ago in reply to gpolder +1
    No Gerit, this one does not. Although it uses SSD1306 controller, it is 64 x 48 pixels monochrome. But it does nice inverse color. On my next post I will include some demos, a short video maybe, if I can…
Parents
  • Workshopshed
    Workshopshed over 9 years ago

    Hey konstantinoskonstas the new screen looks great!

     

    I notice that the mounting nuts are a lot bigger than the ones provided with the Intel boards. It shows that the Edison has been designed right in that you can fit the large nuts.

     

    However, it might be worth taking care not to over tighten them.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • konstantinoskonstas
    konstantinoskonstas over 9 years ago in reply to Workshopshed

    Workshopshed

    Hello Andy,

     

    Thanks a lot for your comment and your very valuable information about the hardware - hardware.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • konstantinoskonstas
    konstantinoskonstas over 9 years ago in reply to Workshopshed

    Workshopshed

    Hello Andy,

     

    Thanks a lot for your comment and your very valuable information about the hardware - hardware.