RoadTests & Reviews
  • Products & Partners
  • More
RoadTests & Reviews
Review Blogs Arduino Giga R1 Display and Camera
  • Blogs
  • Forum
  • Documents
  • RoadTests
  • Reviews
  • Polls
  • Files
  • Members
  • Sub-Groups
  • More
  • Cancel
  • New
Join RoadTests & Reviews to participate - click to join for free!
  • Share
  • More
  • Cancel
  • Author Author: dougw
  • Date Created: 20 Oct 2025 5:39 PM Date Created
  • Views 2701 views
  • Likes 10 likes
  • Comments 3 comments
Related
Recommended
  • Giga Display
  • dougw
  • Arducam B0462
  • GC2145
  • arduino giga r1

Arduino Giga R1 Display and Camera

dougw
dougw
20 Oct 2025

Intro

The Arduino Giga R1 has a camera connector, so of course I want check it out, so I purchased the highest resolution color camera I could find that had the correct connector. This is the Arducam B0462 which uses a 2 megapixel GC2145 camera sensor (1616V x 1232H). There is an example sketch that captures Arducam camera images and displays them on the Giga Display, although it is not well suited to this camera.

imageGiga displaying an Arducam image of the camera taking this picture

Giga R1 Demo of the Giga Display with an Arducam B0462 Camera

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

The example sketch displays the camera image upside down and backwards. Because the camera is connected to the display, it doesn't matter if you turn the camera upside down, the image on the display is always upside down. So I had to modify the code to transpose the image.

Here is the modified code:

Camera Display Sketch

//Arduino GIGA R1 displaying an Arducam B0462 (GC2145) on the GIGA Display
// Doug Wong 2025
// The GC2145 image has been transposed properly so it dsplays right side up

#include "arducam_dvp.h"
#include "Arduino_H7_Video.h"
#include "dsi.h"
#include "SDRAM.h"

// This example only works with Greyscale cameras (due to the palette + resize&rotate algo)
#define ARDUCAM_CAMERA_GC2145

#ifdef ARDUCAM_CAMERA_HM01B0
#include "Himax_HM01B0/himax.h"
HM01B0 himax;
Camera cam(himax);
#define IMAGE_MODE CAMERA_GRAYSCALE
#elif defined(ARDUCAM_CAMERA_HM0360)
#include "Himax_HM0360/hm0360.h"
HM0360 himax;
Camera cam(himax);
#define IMAGE_MODE CAMERA_GRAYSCALE
#elif defined(ARDUCAM_CAMERA_OV767X)
#include "OV7670/ov767x.h"
// OV7670 ov767x;
OV7675 ov767x;
Camera cam(ov767x);
#define IMAGE_MODE CAMERA_RGB565
#elif defined(ARDUCAM_CAMERA_GC2145)
#include "GC2145/gc2145.h"
GC2145 galaxyCore;
Camera cam(galaxyCore);
#define IMAGE_MODE CAMERA_RGB565
#endif

// The buffer used to capture the frame
FrameBuffer fb;
// The buffer used to rotate and resize the frame
FrameBuffer outfb;
// The buffer used to rotate and resize the frame
Arduino_H7_Video Display(800, 480, GigaDisplayShield);

void blinkLED(uint32_t count = 0xFFFFFFFF)
{
  pinMode(LED_BUILTIN, OUTPUT);
  while (count--) {
    digitalWrite(LED_BUILTIN, LOW);  // turn the LED on (HIGH is the voltage level)
    delay(50);                       // wait for a second
    digitalWrite(LED_BUILTIN, HIGH); // turn the LED off by making the voltage LOW
    delay(50);                       // wait for a second
  }
}

uint32_t palette[256];

void setup() {
  // Init the cam QVGA, 30FPS
  if (!cam.begin(CAMERA_R320x240, IMAGE_MODE, 30)) {
    blinkLED();
  }

  // Setup the palette to convert 8 bit greyscale to 32bit greyscale
  for (int i = 0; i < 256; i++) {
    palette[i] = 0xFF000000 | (i << 16) | (i << 8) | i;
  }

  Display.begin();

  if (IMAGE_MODE == CAMERA_GRAYSCALE) {
    dsi_configueCLUT((uint32_t*)palette);
  }
  outfb.setBuffer((uint8_t*)SDRAM.malloc(1024 * 1024));

  // clear the display (gives a nice black background)
  dsi_lcdClear(0);
  dsi_drawCurrentFrameBuffer();
  dsi_lcdClear(0);
  dsi_drawCurrentFrameBuffer();
}

#define HTONS(x)    (((x >> 8) & 0x00FF) | ((x << 8) & 0xFF00))

void loop() {

  // Grab frame and write to another framebuffer
  if (cam.grabFrame(fb, 3000) == 0) {

    // double the resolution and transpose (rotate by 90 degrees) in the same step
    // this only works if the camera feed is 320x240 and the area where we want to display is 640x480
    for (int i = 0; i < 320; i++) {
      int k = 320 - i;                    // this coordinate reversal swaps the image horizontally
      for (int j = 0; j < 240; j++) {
        int l = 240 - j;                  // this coordinate reversal swaps the image vertically
        if (IMAGE_MODE == CAMERA_GRAYSCALE) {
          ((uint8_t*)outfb.getBuffer())[j * 2 + (i * 2) * 480] = ((uint8_t*)fb.getBuffer())[i + j * 320];
          ((uint8_t*)outfb.getBuffer())[j * 2 + (i * 2) * 480 + 1] = ((uint8_t*)fb.getBuffer())[i + j * 320];
          ((uint8_t*)outfb.getBuffer())[j * 2 + (i * 2 + 1) * 480] = ((uint8_t*)fb.getBuffer())[i + j * 320];
          ((uint8_t*)outfb.getBuffer())[j * 2 + (i * 2 + 1) * 480 + 1] = ((uint8_t*)fb.getBuffer())[i + j * 320];
        } else {
          ((uint16_t*)outfb.getBuffer())[l * 2 + (k * 2) * 480] = HTONS(((uint16_t*)fb.getBuffer())[i + j * 320]);
          ((uint16_t*)outfb.getBuffer())[l * 2 + (k * 2) * 480 + 1] = HTONS(((uint16_t*)fb.getBuffer())[i + j * 320]);
          ((uint16_t*)outfb.getBuffer())[l * 2 + (k * 2 + 1) * 480] = HTONS(((uint16_t*)fb.getBuffer())[i + j * 320]);
          ((uint16_t*)outfb.getBuffer())[l * 2 + (k * 2 + 1) * 480 + 1] = HTONS(((uint16_t*)fb.getBuffer())[i + j * 320]);
        }
      }
    }
    dsi_lcdDrawImage((void*)outfb.getBuffer(), (void*)dsi_getCurrentFrameBuffer(), 480, 640, IMAGE_MODE == CAMERA_GRAYSCALE ? DMA2D_INPUT_L8 : DMA2D_INPUT_RGB565);
    dsi_drawCurrentFrameBuffer();
  } else {
    blinkLED(20);
  }
}

Discussion

It is very cool that the GiGa has a built in camera interface, It is a simple plug-and-play exercise to set it up. However, the example software is not taking maximum advantage of the hardware capability. It seems to be limiting the image capture to 320 x 240 pixels and the display to 640 x 480 pixels. Additionally, the image displayed by the example sketch is reversed both horizontally and vertically, which makes everything look upside down and backwards.. Fortunately the transposition is easy to accomplish in software as shown above. The camera hardware is useable as is, but I hope the Arducam library gets updated to allow camera images to properly fill the 800 x 480 display without upscalling. Incidentally, the camera video and images displayed on the GIGA Display look much better in person than what my camera can show.

Links:

Unboxing and display demo

Touch Screen and USB memory demo

GIGA display of an Arducam video camera

GIGA VU Meter and Spectrum Analyzer

GIGA WAV Player

GIGA HID Touch Keyboard

GIGA MQTT Client

Giga Paint

Giga Scope

Final Giga Road Test Blog

Giga R1 Road Test page

  • Sign in to reply
  • DAB
    DAB over 1 year ago

    Great post Douglas.

    I am impressed with the camera and video demonstrated.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • robogary
    robogary over 1 year ago

    amazing

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • cstanton
    cstanton over 1 year ago

    Great progress dougw - since this is working towards your RoadTest Review, I've moved your blogs over to  Review Blogs  , I'm not entirely surprised that the example software isn't fully taking advantage of the kit, that seems pretty typical!