Personal Blogs
  • Community Hub
  • More
Personal Blogs
NexGen Flight Simuator
  • Blog
  • Documents
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New

NexGen Flight Simuator

  • Tags
  • Subscribe by email
  • More
  • Cancel
  • Smarthab: Facial Recognition. v It's Alive!

    phoenixcomm
    phoenixcomm
    It's Alive!!
    • 10 Nov 2019
  • Smarthab: Facial Recognition. iv Progress & 3d

    phoenixcomm
    phoenixcomm
    Well, this update has been more than a few days in coming, as I have been in network hell. I have made good progress, and I am working on programming currently. This was the first time I used a Polyprinter at my local library.  The Tinkercad and...
    • 9 Nov 2019
  • Trapped in Network Hell.

    phoenixcomm
    phoenixcomm
    Since you all know by now I have moved into AT&T Land. It was not nice their router was 192.168.1.1 which normally is my base network. I placed a  Netgear N600 Gigabit router between my computer and the AT&T router (modem).   ...
    • 27 Oct 2019
  • NexGen RSS: Hacking the Gables G-1981 ATC Panel

    phoenixcomm
    phoenixcomm
    Well, here we are back at the ATC panel. The ATC panel function is to identify your aircraft to the tower via secondary radar. After a quick call to Gables Engineering in Florida. I explained what I needed and why they graciously sent me a print with...
    • 19 Oct 2019
  • NexGen: Rudder Pedals .ii Boeing 737 Overhaul

    phoenixcomm
    phoenixcomm
    Ok, you all know if you are keeping up, I scored a pair of B-737 rudder pedals on eBay for about 200 bucks. So the first thing I have to do is take the pedals apart and clean them. The parts diagrams and part numbers come from the Boeing...
    • 15 Oct 2019
  • NexGen: The New Lab .V Found My Test Equipment!!

    phoenixcomm
    phoenixcomm
    Well, another day moving or should I say un-moving? I finally found most of my missing test equipment. The list includes both of my Labda 'bricks' LXS-A-5-0V and my LM B15, an Acopian V48PT5AF rack-mounted 48 dc supply, Electronics Measure...
    • 13 Oct 2019
  • NexGen: The New Lab .IV Found Treasure!!

    phoenixcomm
    phoenixcomm
    Well, I really can not contain myself.  As you all know I moved back on Labor Day.  And I am still moving! Well, today I found treasure!! I found my Gardner Denver WireWrap Gun (model 27100AB2) this gun has back-force so it is easier to wra...
    • 9 Oct 2019
  • NexGen: Rudder Pedals: Good Bad and the Ugly!

    phoenixcomm
    phoenixcomm
    Ok, every plane needs a set of rudder peddles! There are a lot of choices, and then everything in between. The pedals show below, Figures 1 to 5, are commercial products priced from $50 to more than $500 dollars! Figure 1 is my old Thrustmaster but i...
    • 29 Sep 2019
  • NexGen: RSS Never Say Never!! ii

    phoenixcomm
    phoenixcomm
    Well, I figured it out! Since I am using an Arduino Mega with 4 serial ports so what's the problem? All Slaves and Controllers use RJ-45 connectors and ethernet cable.There is very little magic here as Arduino has built-in drivers for the serial ...
    • 27 Sep 2019
  • NeXGen: Hacking a ID-453/ARN-30 Course Indicator part ii

    phoenixcomm
    phoenixcomm
    The last time I blogged about this unit was back in October 2016. So I uncovered it in the "un-move" along with a cable which I had thought was just a spare but nope it belonged to this beast. Basically, it's a Resolver that drives the 'bug' or poin...
    • 26 Sep 2019
  • NexGen: RSS: Never Say Never!!

    phoenixcomm
    phoenixcomm
    Ok so I have messing about with Edin Lite, which is only Half-Duplex and has a fairly small package size.  So since I have an abundance of RS485 Modules I decided to try Full-Duplex. This is fairly straight forward, and I doubled my bandwidth. W...
    • 22 Sep 2019
  • Back to College: History of Single Board Computers

    phoenixcomm
    phoenixcomm
    In the dim past, computers were so large that they could take up a large amount of space and have their own cooling.  Then in the '70s, there was the minicomputer. This is an Interdata 70, in their later models they changed the color of the ...
    • 19 Sep 2019
  • NexGen: Component Documentation: Instrument, Fuel Load Selector - Indicator

    phoenixcomm
    phoenixcomm
    Repeater/Fuel Load Selector Indicator Manufacture Part Number Innovative Solutions & Support 90-00659-1 Parker 219-100-001     NOTE* This device was heavily modified. It uses two HDSP-2131TXV displays
    • 7 Sep 2019
  • NexGen: Hacking the Fuel Load Indicator vi.b Making a New Major PCB

    phoenixcomm
    phoenixcomm
    Well, the last attempt of making a circuit board was an utter disaster. Figure 1 Figure 2 Attempt number 2. I went over to my local library which has a small maker space where they walked me through Tinkercad. My goal was to use their 3D pr...
    • 7 Sep 2019
  • NexGen: Hacking the Fuel Load Indicator v - Display Board Pinouts

    phoenixcomm
    phoenixcomm
    This page has been redacted see NexGen: Fuel Load Indicator: Pinouts Redux Well, I just found out some errors in my part ii Fuel Load Indicator addendum interface table.  Apparently, I was using the wrong part's pinout, "So without further eloqu...
    • 6 Sep 2019
  • NexGen: Fuel Load Indicator iv.a Making a new major PCB

    phoenixcomm
    phoenixcomm
    Well, really need to finish something around here so I will take up where we left off with the fuel load indicator, in parts 1, 2 and 3. And I can't go on without a PC board so I decided to make one this evening. First I need a piece of Vector Bo...
    • 2 Sep 2019
  • The Phoenix Arises from the Dead or should I say Radio Shack?

    phoenixcomm
    phoenixcomm
    Is this really 2019? Did I step into the "Time Tunnel"? Did I just have a bad dream?  The answers are YES, NO, NO. This is a shot I took today coming home from my shoulder rehab. No stupid toys, Batteries, Car Batteries, etc. Component...
    • 29 Aug 2019
  • NexGen: The New Lab .III Some of my shelves arrive.

    phoenixcomm
    phoenixcomm
    Ok, it has been a slog getting my office/lab back up and running. I seem to be missing all sorts of stuff. WireWrap Gun, Thermal Strippers, Handel for my Metcal even though I have the two base units and the tips. It seems that some of my shelving has...
    • 27 Aug 2019
  • NexGen: Question is it possible to build a ARM7 Core from AM2901 Bit Slices?

    phoenixcomm
    phoenixcomm
    ARM 7 CoreAMD AM2901 Bit Slice ALUThis started with the wonderings of my rabid mind. In a comment to Project 14 You DecideThese are the two processors first I would have to add a register file. And since I like UltraSparc well it had 144 general-purp...
    • 25 Aug 2019
  • NexGen: Tech Tip V. Remove Labels and Adhesives

    phoenixcomm
    phoenixcomm
    Ever try and remove a label from plastic? Yep, WD-40, Goo Gone, and others including yep peanut butter well just don't really work, or damage the plastic that the label is attached to. Most of you have used the old stand by a hair drier as well. But ...
    • 21 Aug 2019
  • NexGen: The New Lab .II The desks arrive.

    phoenixcomm
    phoenixcomm
     Well, this has been a pain in the tush today. My friend Ed and I brought up the desk pedestals and then set the desk up. this went uneventfully.But that was far from the case in getting the damn workbench pedestals, which were made by Diebold. ...
    • 13 Aug 2019
  • NexGen: The Lab: Two is always better than one!

    phoenixcomm
    phoenixcomm
    Before I moved my very old task lamp with magnifier broke. It broke at the base where everything swivels from, as this lamp is very old I could not find any parts online.  So I disassembled most of it and put it in my hope chest.The other day w...
    • 5 Aug 2019
  • The New Lab .i

    phoenixcomm
    phoenixcomm
    Well, I finely sort of moved into my new digs. And I have nice blank space to install my lab, and office desk in one room with out all the junk, as I now have a garage where I will keep my shop for construction. Having the shop will keep all the dril...
    • 23 Jun 2019
  • Radio Set, Control Unit, C-3436A/ARN-30D (in ATR.polly)

    phoenixcomm
    phoenixcomm
    Here is what the current interface is; I have installed the prototype cards into an ATR.poly slave. It has 2 RJ45 for the RS-485 which is almost wired pin for pin. I use T-586B for my RJ45 (yellow RS-485) links downstream and upstream, as well as 2 D...
    • 14 Jun 2019
  • Where are we now 2019

    phoenixcomm
    phoenixcomm
    Well, it's about time to play catch-up with everybody.  So here is my "State of the NexGen", and to tell you what's going on in my rabid brain. The big news which I sort of leaked a few days ago with my Roadmaps! We have almost nailed down the p...
    • 8 Jun 2019
<>