Personal Blogs
  • Community Hub
  • More
Personal Blogs
NexGen Flight Simuator
  • Blog
  • Documents
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New

NexGen Flight Simuator

  • Tags
  • Subscribe by email
  • More
  • Cancel
  • NexGen: Getting the Lab Working: LAMBDA LP 411 FM - Repair 1

    phoenixcomm
    phoenixcomm
    span>Ok I'm back at it repairing stuff, the inner and outer front panels have been pressed and pounded on and then the aluminum outer panel got some new gray paint.  I have also replaced the cheap binding posts in favor of some surplus Pamona...
    • 22 May 2020
  • NexGen: Component Documentation: King Radio: ADF Panel - KFS585B

    phoenixcomm
    phoenixcomm
    NexGen: Component Documentation: King Radio: ADF Panel KFS585B DB-37M 1. 1 kHz (wht/brn) 2. 2 kHz (wht/Orn) 3. 4kHz (wht/grn)n 4. 8 kHz (wht/blu) 5. 10 kHz (yel/brn) 6. 20 kHz (yel/grn) 7. 40 kHz (yel/blu) 8. 80 kHz (Yel/wht) 9. 100 k...
    • 18 May 2020
  • Nexgen: Adventures into CANaerospace part 1

    phoenixcomm
    phoenixcomm
    Ok, this will be a new series of blogs taking you and me from sending a CAN message between two Arduinos. First without interrupts on the receiver and then with. Then with the same hardware, I will send an adequately formatted CANaerospace message. C...
    • 14 May 2020
  • Nexgen: RSS: Intercommunications: Canbus: Request for Comments.

    phoenixcomm
    phoenixcomm
    Well, here I am again, with the big question: How does the computer talk to the slaves (Arduino Megas. I have gone through USB (major problems), NASA Edin Lite via RS485 (but it has a small packet size).Then I thought of Ethernet (too costly per node...
    • 20 Apr 2020
  • NexGen: Lab:B&K Precision 3010 Function Generator - Resurrection!

    phoenixcomm
    phoenixcomm
    All is now well most of my noise was coming from two sources.Power bridge needed resoldering!Scope probe not grounded!It is now all buttoned up and on the shelf!Here are some pictures.Test SetupSine WaveSquare WaveTriangle Wave
    • 19 Apr 2020
  • NexGen: Lab: B&K 3010 Function Generator - Overhual

    phoenixcomm
    phoenixcomm
    THENNOWWell, I have this unit on the repair shelf for a since 2015/07/22 So after much sawing and filing I got the NEMA socket to fit in the damn hole. In hindsight, I am glad I used the spade lugs! I then use a Molex type plug set with some wire on ...
    • 14 Apr 2020
  • NexGen: Lab:B&K Precision 3010 Function Generator - Repair

    phoenixcomm
    phoenixcomm
    THENNOW Black (Hot) and White (Neutral) ended up switched so 110 VAC ended up on my ground-plane! Push on connectors are a must! I replaced the bridge with 4 100vdc 5 amp monsters.  It took quite a bit of heat to solder the big leads so I s...
    • 13 Apr 2020
  • Tech Tip VIII: HP 3330 Laserjet Warm Up Issues!

    phoenixcomm
    phoenixcomm
    I have to warn you this fix is not for the faint of heart! My Hp 3330 laserjet has been pushing paper for me for almost 20 years, without problems aside from every once in awhile changing the toner cartridge.About a week ago it would sit there making...
    • 15 Mar 2020
  • Nexgen: Flight Simulator: Hacking The CP-1252/ASN-128: Keyboard Switches

    phoenixcomm
    phoenixcomm
    The factor keyboard was set up for scanning. I intend to fire off an interrupt when a key is pressed. This breaks my rule number 1: Do No Harm to the Equipment! But this piece of gear has been stripped before I got them. ( I have three of them. Good...
    • 28 Feb 2020
  • Nexgen: FAA Nav Aid Station Software Design Overview

    phoenixcomm
    phoenixcomm
    Design: As an aircraft flies overhead, it receives radio signals in a 360 degrees circle around the aircraft. So these radio stations must be placed into a database, which contains the address of the main Db. This database must be updated every fift...
    • 10 Feb 2020
  • Nexgen: ATR Box Version 2

    phoenixcomm
    phoenixcomm
    So what is wrong with ATR-poly?.What's right? It's Polyethylene. It's almost impossible to glue an FR-4 PCB to it. And it's not what you call stable. For those of you that did not know I moved last Labor Day. About 4 months ago when I...
    • 7 Feb 2020
  • Tech Tip VII: To HE!! with Keyboard Scanning!

    phoenixcomm
    phoenixcomm
    Ok, am I a little harsh, maybe, but when you have a keyboard that you don't use very much, just think of the wasted CPU cycles scanning the Keyboard! I one minute, in one hour? So what to do? In steps our 8 input to 3-line, Priority Encoder TI SN74x...
    • 18 Jan 2020
  • NexGen: Getting the Lab Working: LAMBDA LP 411FM - Reassemble and Testing

    phoenixcomm
    phoenixcomm
    Well, pigs fly! And I straightened both the back panel and the front panel. But alas I have miss laid the finished front trim panel.  So I'm going to resemble it without the outer front panel, and then do it all over again when I find the damn ...
    • 16 Jan 2020
  • Display Interface a Final Look?

    phoenixcomm
    phoenixcomm
    Well, here we are again, the MAX6955 went down in flames as it will only work on LEDs. So we have to start over.The Analysis: The NCD is comprised of 4 groups: Display, Keyboard, Rotary Switches, and Thumb Wheel Switches.  The Display is compris...
    • 3 Jan 2020
  • NexGen: CP-1252: Front Panel Switches, Interrupts!! 2-level

    phoenixcomm
    phoenixcomm
    OK, last time I might have confused you with 2-level interrupts. So here it is and please refer to the schematic. So here's how it works. In this diagram, you see 4 switches 2 rotary and 2 thumbwheel switches.  You will notice that each of the t...
    • 1 Jan 2020
  • NexGen: CP-1252: Front Panel Switches, Interrupts!!

    phoenixcomm
    phoenixcomm
    Oh my lord back to this monster again. I took another look at what's really going on in this thing. Display SwitchMode SwitchThumb Switch 1Thumb Switch 2int 1int 2int 3int 4Keyboardint 5Communicationsint 0I have broken it down into functional sec...
    • 1 Jan 2020
  • Early Christmas Present from Element14 2019

    phoenixcomm
    phoenixcomm
    Well Mr. UPS just showed up late today with a package from Element14 and tariq.ahmad. Now I wondered what could it be? So I ripped it open.Inside aside from propaganda Tee Shirt and Stickers, there was an Arduino Micro 5v, a Huzzh Feather, and two an...
    • 24 Dec 2019
  • Welcome to Smart-Wiring

    phoenixcomm
    phoenixcomm
    This is what you might have in your house. A 200 amp main panel, with a sub-panel for your Basement. You will notice the four large breakers in the lower left of the main panel, One of them feeds the sub-panel. But there only separated by a few inche...
    • 14 Dec 2019
  • Smarthab: Smart Wiring II

    phoenixcomm
    phoenixcomm
    This photo is to show you what this person thinks a Smart House should be wired! And there is a ton of it. I don't consider this very smart! Rember in my last posts, I talked about smart wiring? So let us start with the Requirements for the Rooms...
    • 12 Dec 2019
  • Hacking Your Library

    phoenixcomm
    phoenixcomm
    In 2004,  Kendall Grant Clark of www.XML.com, wrote a series of articles called "Hacking The Library" they where:Geeks and the Dijalog Lifestyle (Feb 8, 2004)The Library of Congress Comes Home (March 17, 2004)Six Steps to LOC@Home (April 28, 200...
    • 1 Dec 2019
  • Smarthab: Facial Recognition ix. Last Ditch Attempt.

    phoenixcomm
    phoenixcomm
    On the benchTerminal SessionWell, I'm not done yet. I might be down. I need some more stuff for this project so off to Micro Center. And about 130 miles later. I started over from scratch here is what I did:* Please note: this information has come fr...
    • 25 Nov 2019
  • NexGen Blog Post Index VII

    phoenixcomm
    phoenixcomm
    Road Tests: Smarthab: Jul 21, 2013 Review of Anaren AIR CC2530 BoosterPack Kit Feb 5, 2019 Essentials: Automation I Sep 27, 2015 Review of  TI Multi-Node IoT Bundle Dec 24, 2019 Welcome to Smart Wiring Dec 12, 2019 Smart ...
    • 16 Nov 2019
  • Nexgen: NASA's Edian Lite, Revisited

    phoenixcomm
    phoenixcomm
    To give you all a refresher about NASA's EADIN Lite Communications Protocol, I was happy to embrace it.The problem is the downsides for me:Only an 8-bit payload.Before the Data Field, I need a Data Lenth Field of 1 byteEach board must be programmed f...
    • 16 Nov 2019
  • Smarthab: Facial Recognition. v Cleaning up power etc.

    phoenixcomm
    phoenixcomm
    Well, the power and the cables are getting under my skin. So being in Dallas, I stopped at Tanners Electronics, and I solved my cooling issues and power which now includes a 12vdc fan. So this is what I picked up today. A Pace AC Adapter 115AC to 12v...
    • 15 Nov 2019
  • Smarthab: Facial Recognition. vi Taming of the Shrew part 1.

    phoenixcomm
    phoenixcomm
    As much as l like Debian 9.x, I hate this jury-rigged Cloud 9 Interface. Just getting the BB AI on my network (static IP address) was a chore and way too many steps! This took many hours of trial, blind alleys, and miss-steps, As there is NO network...
    • 10 Nov 2019
<>