Digilent, a National Instruments Company
  • Products & Partners
  • Manufacturers
  • Digilent, a National Instruments Company
  • More
  • Cancel
Digilent, a National Instruments Company
Blog
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Digilent, a National Instruments Company to participate - click to join for free!

Blog

  • Tags
  • Subscribe by email
  • More
  • Cancel
  • Implement Fast Fourier Transform on Xilinx Zynq SoC

    alexwonglik1
    alexwonglik1
    The Fourier transform (FT) decomposes a signal into its constituent frequencies and shows that any signal can be re-written as the sum of sinusoidal functions. It is also a mathematical method for transforming a function of time into a function of fr...
    • 15 Jun 2020
  • Introducing Digilent Zmods: Cost-effective high-speed I/O expansion modules for FPGA boards

    alexwonglik1
    alexwonglik1
     Many engineers have come across Digilent Pmods standard and even included Pmods in their systems. Pmod modules allow for more effective designs by routing analog signals and power supplies only where they are needed, and away from digital contr...
    • 2 Jun 2020
  • An in-depth look into Genesys ZU-3EG, a versatile Zynq Ultrascale+ MPSoC EG Platform

    alexwonglik1
    alexwonglik1
    Digilent Genesys ZU-3EG is an advanced computing platform loaded with Xilinx Zynq Ultrascale+ MPSoC EG and a range of peripherals and interface. Let's take a closer look.   MemoryMain memory is a single-slot populated DDR4 SODIMM, alway...
    • 19 May 2020
  • Use Analog Discovery 2 to create harmonics and look at its spectrum

    alexwonglik1
    alexwonglik1
    This post shows how to create harmonics in a specific signal with the Analog Discovery 2Analog Discovery 2 and look at the spectrum through FFT mode. We will use the Oscilloscope and Waveform / Signal Generator instruments in Analog Discovery 2.&nbsp...
    • 12 May 2020
  • Audio Looper powered by Nexys Video

    alexwonglik1
    alexwonglik1
    Digilent Nexys VideoDigilent Nexys Video, Xilinx Artix 7-200T platform ( More InfoMore Info ), is an ideal development board for audio/video applications. There are three high-speed digital video ports, and a 24-bit audio codec on board.  W...
    • 19 Apr 2020
  • Using the Digital Discovery to debug a Character LCD

    alexwonglik1
    alexwonglik1
    Digilent Digital Discovery is a combined logic analyzer and pattern generator instrument and allows you to debug, visualize,and simulate signals in digital systems. LCD displays are used in a wide range of devices. The most common version uses a 2×16...
    • 8 Apr 2020
  • New Product Release: Analog Discovery Studio

    alexwonglik1
    alexwonglik1
    Analog Discovery Studio: The Portable Circuits Laboratory for EveryoneProvides an entire stack of benchtop instruments with a convenient breadboardable interface The Analog Discovery Studio is a fully-functional portable test and measurement dev...
    • 24 Mar 2020
  • Build the multiple camera streaming application with Digilent Zedboard Advanced Image Processing Kit

    alexwonglik1
    alexwonglik1
     The ZedBoard Advanced Image Processing KitZedBoard Advanced Image Processing Kit was built to use the video processing capabilities of the Zynq-7000 AP SoC's tightly coupled ARM processing system and 7-series programmable logic.Included in the ...
    • 14 Mar 2020
  • OpenLogger - Getting Started Guide

    alexwonglik1
    alexwonglik1
      OpenLogger is a high-resolution data logger designed to provide quality measurements without the limits of traditional data logging or data acquisition solutions.You can take advantage of eight analog channels, two power supplies, a funct...
    • 8 Mar 2020
  • New Product Release: Genesys ZU-3EG: Zynq Ultrascale+ MPSoC Development Board

    alexwonglik1
    alexwonglik1
     Genesys ZU-3EG: Zynq Ultrascale+ MPSoC Development BoardA powerful Zynq UltraScale+ 3EG MPSoC development board loaded with peripherals and a wide hardware ecosystem of add-on modules  The Genesys ZU-3EGGenesys ZU-3EG is a standalone ...
    • 8 Mar 2020
  • New Product Release: Eclypse Z7: Zynq-7000 SoC Development Board with SYZYGY-compatible Expansion

    alexwonglik1
    alexwonglik1
    Eclypse Z7: Zynq-7000 SoC Development Board with SYZYGY-compatible ExpansionOptimize productivity and accelerate design flow through Digilent Eclypse Z7. A perfect platform for instrumentation applications. Digilent Eclypse Z7Eclypse Z7 is the f...
    • 24 Feb 2020
  • Analyzing DAC, ADC, and SPI Data with the Analog Discovery Studio

    alexwonglik1
    alexwonglik1
     The Analog Discovery StudioAnalog Discovery Studio functions as a mixed-signal oscilloscope. In this demo, we use several instruments in Analog Discovery Studio. Oscilloscope - view analog data from a resistor ladder Digital to Analog Conv...
    • 19 Feb 2020
  • Analog Discovery 2 is now supported by MATLAB

    alexwonglik1
    alexwonglik1
    With the release of MATLAB 2018b, the Analog Discovery 2Analog Discovery 2 is now included as one of the many hardware devices supported by MATLAB.MATLAB provides libraries for data acquisition hardware in their Data Acquisition Toolbox in order to d...
    • 13 Feb 2020
  • New Product Release: Pmod ESP32: Wireless Communication Module

    alexwonglik1
    alexwonglik1
    The Pmod ESP32Pmod ESP32 provides an easy and cost-effective way to add wireless communication to any host platform or project. It uses the fully certified ESP-WROOM-32 Wi-Fi + BLE + BT module from Espressif Systems. Pmod ESP32Pmod ESP32 is suitable ...
    • 10 Dec 2019
  • Running a RISC-V Processor on Digilent Arty A7

    alexwonglik1
    alexwonglik1
     The Arty A7-100TArty A7-100T contains a Xilinx XC7A100T FPGA which is the largest FPGA available for the Arty A7Arty A7 and is ideal for deployment of softcore processors. These processors can be either proprietary or open-source. One of the mo...
    • 6 Dec 2019
  • Analog Discovery 2 is now Compatible with Raspberry Pi 4

    alexwonglik1
    alexwonglik1
     Now, you have access to a complete benchtop by combining the Analog Discovery 2’s oscilloscope, waveform generator, and logic analyzer with the RPi 4 small single-board computer.      The setup guideOnce the Raspbe...
    • 25 Oct 2019
  • Learn Embedded Systems with Basys MX3, PIC32MX Trainer Board

    alexwonglik1
    alexwonglik1
    Digilent Basys MX3 Basys MX3 enables designers to quickly begin developing and debugging an embedded application. With an exhaustive set of peripherals plus Pmod expansion headers, you can create a wide range of embedded systems applications. The bo...
    • 8 Sep 2019
  • New Product Release: Pmod AQS - Digital Gas Sensor for Air Quality

    alexwonglik1
    alexwonglik1
     With the AMS CCS811 gas sensor, you can detect a wide range of Volatile Organic Compounds (VOCs) using the micro-hotplate technology, enabling a highly reliable solution for gas sensors with very fast cycle times. Pmod AQSPmod AQS can be u...
    • 26 Aug 2019
  • New Product Release - Analog Discovery 2 Pro Bundle

    alexwonglik1
    alexwonglik1
     Start verifying and testing a wide range of projects with the Analog Discovery 2 Pro Bundle. With the addition of the BNC adapter and scope probes, professional or experienced engineers can access the full 30MHz bandwidth oscilloscope and 12MHz...
    • 25 Aug 2019
  • Infra-Red Image Processing Unit powered by Digilent Zybo Z7

    alexwonglik1
    alexwonglik1
    Embedded Vision on Digilent Zybo Z7Zybo Z7, Xilinx Zynq SoC Platform  Digilent host student design contest every year. The contest provides an opportunity to inspire future engineers in Europe. As we know, the automotive industry is leaning...
    • 18 Jul 2019
  • Introducing the OpenScope MZ

    quinn.sullivan
    quinn.sullivan
    Engineers and electronics enthusiasts listen up as the OpenScope MZ has officially launched at Digilent! The OpenScope MZ was announced on Kickstarter in January 2017 as an addition to the Digilent line of Instrumentation and remains their only open-...
    • 2 Sep 2017
  • Debugging Embedded Systems

    quinn.sullivan
    quinn.sullivan
    As a student or professional engineer it is important to pay attention to where your resources are being allocated. Time spent traveling to and from laboratories fixing minor embedded systems project issues is often disregarded for the sake of projec...
    • 29 Jul 2017
<