Say Hello to Raspberry Pi 5!

The Raspberry Pi 5 delivers over a 2x increase in CPU performance and a significant uplift in GPU performance. Available in 4GB, or 8GB LPDDR4X-4267 SDRAM, the Pi 5 comes loaded with a 2.4GHz 64-bit quad-core ARM processor, VideoCore VII GPU, 2x4 lane MIPI camera/display transceivers, real-time clock, and a convenient, on-board power button.

See the Raspberry Pi 5 4GB Technical Specification and 8GB Technical Specification.

Introducing the Raspberry Pi Compute Module 5
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
GPIO Pinout
Raspberry Pi Wishlist
Comparison Chart
Quiz
Raspberry Pi Poster
Raspberry Pi Webinars and eBooks
Featured Products
power supply

27W USB-C PD Power Supply

5.1V, 5A power supply

pi 5 case

Raspberry Pi 5 Case

Improved thermal features, built-in fan, made specifically for the Pi 5.

Active Cooler

Active Cooler

Cooling solution with a large heatsink and variable-speed fan

RECENT BLOG POSTS
  • Blog: Going bare metal on Raspberry Pi

    Introduction: If you're an avid Raspberry Pi enthusiast and have explored the world of traditional Linux-based development on the platform, it's time to embark on a new adventure. In this blog post, we'll delve into the exciting realm of ...
  • Blog: Raspberry Pi Arcade HAT

    So I thought I'll let people know I have been working on a HAT for the Raspberry Pi, to allow easier implementation of a four player arcade with revenue service capabilities. I have a YouTube video going over the circuit and PCB design.  https:...
  • Blog: Ploopy's Open Source Headphones with the RP2040

    Open source software is all the rage; open collaboration with every software developer on the planet has led to more secure and innovative code. But what about on the hardware side? Traditionally, hardware has been more proprietary and closed off, b...
  • Blog: How to improve my brachioGraph project - add something special

    hello everyone I made a project https://www.brachiograph.art/tutorial/construct.html brachioGraph with three servo motors and a raspberry pi, I need help to improve it, add something design thing, add something else that will make it better
Related Projects
  • Video: Infrared night vision with the NoIR V2

    The primary advantage of the Raspberry Pi NoIR camera is seeing in complete darkness. By using an Infrared light source - completely invisible to the human eye - images and videos can be captured with no visible illumination whatsoever. This vid...
  • A more powerful Plex media server using Raspberry Pi 3

    Recently we built a Plex Media Server using the Raspberry Pi 2, at the time the Raspberry Pi 2 was the most powerful board in the Raspberry Pi range. But on February 29th 2016 the Raspberry Pi Foundation announced their latest board, the Raspberry Pi...
  • Gesture Based TV Remote Control

    Here's the latest project I've been working on: controlling the TV using gestures instead of a remote control. Mainly inspired by my kids being able to handle a tablet but not a remote control, it could perhaps also help to Make Life Accessib...
  • 2015 Year in Review: Top 10 Raspberry Pi Projects

    RASPBERRY PI PROJECTSJust between you and me, it can sometimes be tricky finding enough content for "top lists" like these. At times it almost feels like you're settling for certain entries, rather than really wanting to put them front ...
  • Raspberry Pi Zero Internet Connected Information Display

    The Raspberry Pi Zero form factor, makes it perfect for use in smaller project. Combined with internet connectivity, a display and some kind of input, it could be used to visualise virtually anything. Using a Pi Zero, an I2C OLED display from Ad...