Browse By Tags

  • Custom device: cannot route

    Hi all, I have created a new device from scratch: a 60 pin connector. This device has a tricky part: 6 pins are rounded pins with holes, so I have used SMD pads combined with polygons (to draw the holes) in order to follow datasheet drawings: After drawing…
  • New part pads overlap once placed in schematic/layout

    Hi all, I am currently working on a project and have had to create some new parts. One of my parts has a pitch of 0.050" and looks fine in the library editor but is overlapping once placed. Could anyone suggest why this is happening and how to fix this…
  • Max/min which

    Hello, I am rather new to this and doing it for my own personal entertainment but I have a question. I am designing a component in eagle that no library has that I plan on using and it comes with max/min values for size, spots etc, should I use the nominal…
  • multiple V+ pins custom part

    I'm trying to create a custom part for a LT1210 amplifier. The problem I have is that different packages have different number of V+ pins. Do I need to create a separate schematic for each package dependent on the number of V+ pins or is there a way to…
  • New to the pi world

    So I've been scouring the internet for stuff to do with my new pi for about a week now and I've decided that what I need to do is get a small display with no audio, a compact laptop battery, and a compact keyboard. Then proceed to boot with out Xwindows…
  • newbie question about making custom SMD pad sizes

    I'm brand new to Eagle. I've created several packages so far, mostly by copying existing packages and modifying them. I'm now trying to create another package, but none of the selectable SMD pad sizes are even close to the pad size I need. How do I create…
  • ULP to build custom lib from project

    I'm looking for a ULP (or some function) to take a project (sch and brd) that I have added parts to from various libraries (some edited) and output a custom library with just the parts used in the project. Can anyone help point me to a function or ULP…
  • Custom buttons, switches, and sensors?

    Any suggestions for a good source of custom purposed buttons for projects? For example, I've owned several iOS devices and the buttons are always the first thing to go. You can replace these but I've only ever seen straight replacements. I want to swap…
  • non rectangular pad

    The Murata LXDC2HL series part is a micro-sized DC-DC converter with four pads. One is rectangular with a clipped corner as a orientation marker. I included the land layout from the spec sheet. Is there an easy way to make this non-standard pad? Or does…
  • Using multiple wildcards in device name

    Hi all, I am currently trying to overhaul my custom library, and I have a question about device names: Consider a part 9*9647-XX-YY-ZZ, where '*', 'XX', 'YY', and 'ZZ' are all variable specifications (pin length, plating, number of pins, etc.). Is it…
  • See Ben’s Hand-Built Custom Case Episode -- Episode 94

    element14's The Ben Heck Show Join the Ben Heck team every week for amazing hacks! Watch them build and mod community-inspired projects using electronics! Back to The Ben Heck Show homepage Connect with TBHS Featured Bonus Materials See All Episodes …
  • Transformers for LT3573/3574/3575 and LT3748

    Transformers for LT3573/3574/3575 and LT3748 Linear Technology launched a family of ICs for isolated flyback converters which allow a very simple. In close cooperation with Würth Elektronik, there are more than 60 standard transformers developed which…
  • LT3748 - 100V Isolated Flyback DC/DC Controller

    100V Isolated Flyback DC/DC Controller Simplifies Design & Eliminates Optocoupler V IN Range from 5V to 100V No Opto-Isolator, Transformer or Third Winding Required for Feedback Drives External N-channel Power MOSFET Current Mode Control Boundary Mode…
  • LT3575 - Isolated Monolithic Flyback Regulator

    Isolated Monolithic Flyback Regulator Simplifies Design & Eliminates Optocoupler V IN Range from 3V to 40V Onboard 2.5A, 60V Integrated Power Switch No Transformer, Third Winding or Opto-Isolator Required for Feedback Current-Mode Control Boundary-Mode…
  • LT3574 - Low Power Isolated Monolithic Flyback Switching Regulator

    Low Power Isolated Monolithic Flyback Switching Regulator Simplifies Design & Eliminates Optocoupler V IN Range from 3V to 40V Onboard 0.65A, 60V Integrated NPN Power Switch No Transformer, Third Winding or Opto-Isolator Required for Feedback Current…
  • LT3573 - Isolated Monolithic Flyback with integrated power switch

    Isolated Monolithic Flyback Simplifies Design & Eliminates Optocoupler - LT3573EMSE#PBF LT3573EMSE#PBF V IN Range from 3V to 40V Onboard 1.25A, 60V Integrated NPN Power Switch No Transformer, Third Winding or Opto-Isolator Required for Feedback Current…
  • Design Kit Demoboard for Flyback Transformers

    Flyback Converter for LT3573/LT3574/LT3575/LT3748 Linear Technologies and Würth Elektronik developed flyback transformers for the switching regulators: LT3573 , LT3574 , LT3575 and LT3748 More than 60 different transformers are available in stock. The…
  • Ben Heck's Hak5 Custom LAN Case Build-Off -- Episode 25

    element14's The Ben Heck Show Join the Ben Heck team every week for amazing hacks! Watch them build and mod community-inspired projects using electronics! Back to The Ben Heck Show homepage Connect with TBHS Featured Bonus Materials See All Episodes …
  • 3DRacers takes virtual racing games to your living room floor

    You don't have permission to edit metadata of this video. Edit media Dimensions x Small Medium Large Custom Subject (required) Brief Description…
  • Florescent Orange Raspberry Pi Case Assembly

    I wanted to show how the feet were stuck on the Raspberry Pi when you build the case and also the awesome effect that the "Florescent" Orange really kicks out ! (BTW we can laser cut what ever you want in this stuff so shout !) …
  • Created custom part and library - can only draw traces on top layer

    Hello Members, I am brand new to using Eagle s/w. I created a custom part and library. Created a package, a device, and a symbol. I can add the part to a schematic, but when I start routing traces on the board, I can only connect to pins on the part using…