FPGA
  • Technologies
  • More
FPGA
Blog Arty S7 50 ArtyBot How to Store MicroBlaze Program in the Quad-SPI Flash from Vivado
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join FPGA to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: javagoza
  • Date Created: 6 Jul 2022 7:40 PM Date Created
  • Views 7660 views
  • Likes 13 likes
  • Comments 4 comments
  • Artybot
  • 7 Ways to Leave Your Spartan-6
  • xilinx
  • vivado
  • flash
  • fpga-project
  • arty s7
  • spartan-7
  • vitis
  • Spartan_Migration
  • microblaze
Related
Recommended

Arty S7 50 ArtyBot How to Store MicroBlaze Program in the Quad-SPI Flash from Vivado

javagoza
javagoza
6 Jul 2022
Arty S7 50 ArtyBot How to Store MicroBlaze Program in the Quad-SPI Flash from Vivado

We want our Artybot to be autonomous. Until now every time we turned off the Arty S7 50 board we lost the program loaded in the board's RAM. This guide will show you how to store a Microblaze program in the SPI Flash on your Arty S7 50 device. Storing a program in Flash allows you to preserve the project program through power cycles.

This tutorial post is part 6 of my contribution to the "7 Ways to Leave Your Spartan-6" program, learning about the Xilinx Spartan-7 FPGA on the Digilent Arty S7 50 board.

"7 Ways to Leave Your Spartan-6" related posts
1 Arty S7 50 First Power Up and Hardware-Only Blinky
2 Arty S7 50 First Baremetal Software Project
3 Arty S7 50 Rapid Prototyping - Environmental Monitor
4 Arty S7 50 ArtyBot Pulse Width Modulation (PWM) for Motor Speed Control
5 Arty S7 50 ArtyBot Custom AXI4 Lite IP Peripheral for Sensing Motor Rotational Speed
6 Arty S7 50 ArtyBot How to Store Microblaze Program in SPI Flash from Vivado
7 Arty S7 50 ArtyBot - Bot Application Framework
8 Arty S7 50 ArtyBot becomes Emubot, an educational robot for young children
9 Arty S7 50 ArtyBot - Color sensing and line follower
10 Arty S7 50 The Spartan-6 Migration Path Game. Learning the Differences Between Spartan-6 and Spartan-7 FPGAs
11 Arty S7 50 ArtyBot ToF Sensor for Obstacle Avoidance. Vivado Hierarchical Blocks
12 "7 Ways to Leave Your Spartan-6 FPGA" program. My summary
13 Arty S7 50 VGA Thermal Imaging Camera


Tutorial Environment

For this tutorial you'll need, Windows 10, AMD Xilinx Vivado ML 2021.1

This tutorial assumes that you already have a Vivado Project using the Microblaze IP and a Vitis C software project using that hardware configuration.

Look at these two projects as example:  Arty S7 50 Rapid Prototyping - Environmental Monitor or Arty S7 50 First Baremetal Software Project

Hardware needed:

Product Name Manufacturer Datasheet
Arty S7 50  Digilent  Buy Now


About the  Arty S7 50 Quad-SPI Flash

The Arty S7 50 board features 16 MB Quad-SPI Flash memory. 

Since the FPGA's memory on the Arty S7 is volatile, it relies on the Quad-SPI flash memory to store the configuration between power cycles. This configuration mode is called Master SPI. The blank FPGA takes the role of master and reads the configuration file out of the flash device upon power-up. To that effect, a configuration file needs to be downloaded first to the flash.

FPGA configuration files can be written to the Quad-SPI Flash, and setting the mode jumper will cause the FPGA to automatically read a configuration from this device at power on. A Spartan-7 50T configuration file requires 17,536,096 bits of memory, leaving about 87% of the flash device (or ~13.92 MB) available for user data. 

Flash Memory Indirect Programming

When programming a non-volatile flash device, a bitstream file is transferred to the flash in a two-step process:

  1. First, the FPGA is programmed with a circuit that can program flash devices,
  2. and then data is transferred to the flash device via the FPGA circuit (this complexity is hidden from the user by the Xilinx tools).

This is called indirect programming. After the flash device has been programmed, it can automatically configure the FPGA at a subsequent power-on or reset event as determined by the mode jumper setting JP1. Programming files stored in the flash device will remain until they are overwritten, regardless of power-cycle events.

Programming the flash can take as long as four to five minutes, which is mostly due to the lengthy erase process inherent to the memory technology. Once written however, FPGA configuration can be very fast—less than a second.

We will configure Bitstream compression, SPI bus width, and configuration rate from the Xilinx tools that will affect configuration speed.

The Arty S7 supports x1, x2, and x4 bus widths and data rates of up to 50 MHz for Quad-SPI programming.

Quad-SPI programming can be done using the hardware manager in Vivado and also from Vitis IDE. For this tutorial we will use the Vivado path.

Flash Memory is callout 17 in the figure. 

image

To find out the exact memory part loaded, check the PCB revision and any stickers placed on the PCB with the flash part number printed on it. The table below lists the possible load options.

Manufacturer ​ P/N PCB Revision ​ Package Marking ​
Spansion/​Infineon ​ S25FL128SAG[M|N]FI00 ​ <= E w/o sticker OR >= E w/ sticker ​ FL128SAIF00 ​
Spansion/​Infineon ​ S25FL127SABMFx00 ​ >= E w/ sticker ​ FL127SxF00 ​

The two part numbers are highly compatible and the “​s25fl128s-3.3v-qspi-x4-single”​ part configuration can be used in Vivado Hardware Manager for both. 

Arty S7 50 Spansion Quad SPI Flash

S25FL128S/S25FL256S, 128 Mb (16 MB)/256 Mb (32 MB), 3.0V SPI Flash Memory (infineon.com)

image


Tutorial: How to Store MicroBlaze Program in the Quad-SPI Flash from Xilinx Vivado


Steps

  • Prepare a new bitstream with -bin file generation from Vivado Synthetized Design
  • Generating a new elf file from Xilinx Vitis IDE
  • Attaching the ELF file to the MicroBlaze IP Bock from Vivado Block Design
  • Programming the Quad-SPI Flash from Vivado Hardware Manager
  • Test


Prepare a new bitstream with -bin file generation

  • From your MicroBlaze based VIvado Project go to Project Settings / Bitstream: Check -bin-file.

This tells Vivado that it also has to generate the bin file in addition to the bit file with the bitstream.

image

We have to make other modifications to the bitstream build, but the setting is not enabled until Vivado builds the synthesis.

image

  • Run the Synthesis
  • and open the synthesized design.

Now you can configure the additional bitstream settings

  • Enable bitstream compression

image

  • Under configuration select a supported Configuration Rate. 

 The Arty S7 supports x1, x2, and x4 bus widths and data rates of up to 50 MHz for Quad-SPI programming.

  • I selected 33 MHz

image

  • Go to Configuration Modes
  • Check if Master SPI x4 is selected if not select it

You can have up to two selected configurations.

image

  • Click OK and save the design.

Save the new constrains to the projects constrains file.

It will add some new lines

## Configuration options, can be used for all designs
set_property BITSTREAM.CONFIG.CONFIGRATE 33 [current_design]
set_property CONFIG_VOLTAGE 3.3 [current_design]
set_property CFGBVS VCCO [current_design]
set_property BITSTREAM.CONFIG.SPI_BUSWIDTH 4 [current_design]
set_property CONFIG_MODE SPIx4 [current_design]


Generating a new elf file

  • Go to Vitis
  • and update the hardware specification.

image

  • Clean and build the wrapper
  • Clean and build the software project.
  • annotate the path to the elf file under Debug folder.

You will need later the path to the elf file.

image


Attaching the ELF file to the MicroBlaze IP

Back to Vivado we need to associate the .elf file with our MicroBlaze IP instance

  • Open the Block Design,
  • select the MicroBlaze IP
  • right click
  • and select Associate ELF files...

image

  • Find the .elf file created by Vitis
  • and add the .elf file

image

  • Regenerate the bitstream.

Vivado will add the bin file generated from the .elf file.


Flashing the program

  • Verify that the JP1 mode jumper is populated on its headers for Quad SPI programming mode.
  • Open the Hardware manager in VIvado
  • and auto-connect
  • once connected "Add Configuration Memory Device"

For the Arty S7 the Configuration Memory Device is the Quad SPI Flash Memory

image

  • Look for the s25fl128sxxxxxx0-spi-x1_x2_x4

image

  • Click OK

image

  • Tell Vivado to program the configuration memory.

image

Or you can program later from the Program Configuration Memory Device...

image

  • Look for the generated .bin file under PROJECT_NAME.runs/impl_1 directory 

Mine is C:/Xilinx/work/artys7/artybot_motor_feedback/artybot_motor_feedback.runs/impl_1/artybot_motor_feedback_wrapper.bin

image

  • Click OK

Vivado will now erase and reprogram the QSPI Flash memory on the board.


Test

  • To run the project, power cycle the board or press PROG button.

Video demonstration

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image


The application program loaded for the demo

Github repository: E14SpartanMigrationProgram/mainTestButtons.c

/*
 * test_leds_driver.c: simple test application for the Bot Leds Driver
 *
 * Author: Enrique Albertos
 * Date: 2022/07/03
 */

#include <stdio.h>
#include "platform.h"
#include "xil_printf.h"
#include "xgpio.h"
#include "xil_types.h"
#include "drivers/leds_driver.h"
#include "drivers/rgb_leds_driver.h"
#include "drivers/buttons_driver.h"
#include "drivers/switches_driver.h"
#include "sleep.h"

#define LEDS_RGBLEDS_DEVICE_ID      XPAR_AXI_GPIO_0_DEVICE_ID
#define BUTTONS_SWITCHES_DEVICE_ID  XPAR_AXI_GPIO_1_DEVICE_ID
#define HBRIDGE_CONTROL_DEVICE_ID   XPAR_AXI_GPIO_HBRIDGE_DEVICE_ID



// Get device IDs from xparameters.h

#define RGB_LED_CHANNEL 1
#define LED_CHANNEL 2

#define BUTTONS_CHANNEL 1
#define SWITCHES_CHANNEL 2


void test_leds_and_buttons();

int main() {
	init_platform();
	test_leds_and_buttons();
	cleanup_platform();
	return 0;
}

void test_leds_and_buttons() {
	LedsDriver ledsDriver;
	RgbLedsDriver rgbLedsDriver;
	ButtonsDriver buttonsDriver;
	SwitchesDriver switchesDriver;

	XGpio GpioLedsAndRgbLeds; /* Dual GPIO Driver for LEDs and RGB LEDS*/
	XGpio GpioSwitchsAndButtons; /* Dual GPIO Driver for Switchs and Push Buttons */

	LEDS_DRIVER_init(&ledsDriver, &GpioLedsAndRgbLeds, LEDS_RGBLEDS_DEVICE_ID,
			LED_CHANNEL, 0b0000);


	RGB_LEDS_DRIVER_init(&rgbLedsDriver, &GpioLedsAndRgbLeds, LEDS_RGBLEDS_DEVICE_ID,
			RGB_LED_CHANNEL, 0b000000);

	BUTTONS_DRIVER_init(&buttonsDriver, &GpioSwitchsAndButtons,
			BUTTONS_SWITCHES_DEVICE_ID, BUTTONS_CHANNEL);

	SWITCHES_DRIVER_init(&switchesDriver, &GpioSwitchsAndButtons,
			BUTTONS_SWITCHES_DEVICE_ID, SWITCHES_CHANNEL);

	unsigned long semiperiod = 250000;
	xil_printf("LED TEST Started\n\r");

	LEDS_DRIVER_set_led1_toggle(&ledsDriver);
	usleep(semiperiod);
	LEDS_DRIVER_set_led1_toggle(&ledsDriver);
	usleep(semiperiod);
	LEDS_DRIVER_set_led2_toggle(&ledsDriver);
	usleep(semiperiod);
	LEDS_DRIVER_set_led2_toggle(&ledsDriver);
	usleep(semiperiod);
	LEDS_DRIVER_set_led3_toggle(&ledsDriver);
	usleep(semiperiod);
	LEDS_DRIVER_set_led3_toggle(&ledsDriver);
	usleep(semiperiod);
	LEDS_DRIVER_set_led4_toggle(&ledsDriver);
	usleep(semiperiod);
	LEDS_DRIVER_set_led4_toggle(&ledsDriver);
	usleep(semiperiod);

	RGB_LEDS_DRIVER_set_rgb_led1_set_color(&rgbLedsDriver, COLOR_RED);
	usleep(semiperiod);
	RGB_LEDS_DRIVER_set_rgb_led1_set_color(&rgbLedsDriver, COLOR_GREEN);
	usleep(semiperiod);
	RGB_LEDS_DRIVER_set_rgb_led1_set_color(&rgbLedsDriver, COLOR_BLUE);
	usleep(semiperiod);
	RGB_LEDS_DRIVER_set_rgb_led1_set_color(&rgbLedsDriver, COLOR_CYAN);
	usleep(semiperiod);
	RGB_LEDS_DRIVER_set_rgb_led1_set_color(&rgbLedsDriver, COLOR_MAGENTA);
	usleep(semiperiod);
	RGB_LEDS_DRIVER_set_rgb_led1_set_color(&rgbLedsDriver, COLOR_MAGENTA);
	usleep(semiperiod);
	RGB_LEDS_DRIVER_set_rgb_led1_set_color(&rgbLedsDriver, COLOR_YELLOW);
	usleep(semiperiod);
	RGB_LEDS_DRIVER_set_rgb_led1_set_color(&rgbLedsDriver, COLOR_WHITE);
	usleep(semiperiod);
	RGB_LEDS_DRIVER_set_rgb_led1_set_color(&rgbLedsDriver, COLOR_BLACK);
	usleep(semiperiod);

	RGB_LEDS_DRIVER_set_rgb_led2_set_color(&rgbLedsDriver, COLOR_RED);
	usleep(semiperiod);
	RGB_LEDS_DRIVER_set_rgb_led2_set_color(&rgbLedsDriver, COLOR_GREEN);
	usleep(semiperiod);
	RGB_LEDS_DRIVER_set_rgb_led2_set_color(&rgbLedsDriver, COLOR_BLUE);
	usleep(semiperiod);
	RGB_LEDS_DRIVER_set_rgb_led2_set_color(&rgbLedsDriver, COLOR_CYAN);
	usleep(semiperiod);
	RGB_LEDS_DRIVER_set_rgb_led2_set_color(&rgbLedsDriver, COLOR_MAGENTA);
	usleep(semiperiod);
	RGB_LEDS_DRIVER_set_rgb_led2_set_color(&rgbLedsDriver, COLOR_MAGENTA);
	usleep(semiperiod);
	RGB_LEDS_DRIVER_set_rgb_led2_set_color(&rgbLedsDriver, COLOR_YELLOW);
	usleep(semiperiod);
	RGB_LEDS_DRIVER_set_rgb_led2_set_color(&rgbLedsDriver, COLOR_WHITE);
	usleep(semiperiod);
	RGB_LEDS_DRIVER_set_rgb_led2_set_color(&rgbLedsDriver, COLOR_BLACK);
	usleep(semiperiod);
	while (!BUTTONS_DRIVER_poll_button4(&buttonsDriver)) {
		LEDS_DRIVER_set_leds_state(&ledsDriver, BUTTONS_DRIVER_poll(&buttonsDriver));
        RGB_LEDS_DRIVER_set_rgb_leds_state(&rgbLedsDriver, SWITCHES_DRIVER_poll(&switchesDriver)<<2 | SWITCHES_DRIVER_poll(&switchesDriver));
	}

	xil_printf("LED TEST Finished\n\r");
}


References

  • Flashing a MicroBlaze Program : 5 Steps - Instructables
  • GitHub - javagoza/E14SpartanMigrationProgram
  • S25FL128S/S25FL256S, 128 Mb (16 MB)/256 Mb (32 MB), 3.0V SPI Flash Memory (infineon.com)
  • Arty S7 Reference Manual - Digilent Reference
  • Arty Programming Guide - Digilent Reference
  • How To Store Your SDK Project in SPI Flash - Digilent Reference
  • ug470_7Series_Config.pdf • Viewer • Documentation Portal (xilinx.com)

"7 Ways to Leave Your Spartan-6" related posts
1 Arty S7 50 First Power Up and Hardware-Only Blinky
2 Arty S7 50 First Baremetal Software Project
3 Arty S7 50 Rapid Prototyping - Environmental Monitor
4 Arty S7 50 ArtyBot Pulse Width Modulation (PWM) for Motor Speed Control
5 Arty S7 50 ArtyBot Custom AXI4 Lite IP Peripheral for Sensing Motor Rotational Speed
6 Arty S7 50 ArtyBot How to Store Microblaze Program in the Quad SPI Flash from Vivado
7 Arty S7 50 ArtyBot - Bot Application Framework
8 Arty S7 50 ArtyBot becomes Emubot, an educational robot for young children
9 Arty S7 50 ArtyBot - Color sensing and line follower
10 Arty S7 50 The Spartan-6 Migration Path Game. Learning the Differences Between Spartan-6 and Spartan-7 FPGAs
11 Arty S7 50 ArtyBot ToF Sensor for Obstacle Avoidance. Vivado Hierarchical Blocks
12 "7 Ways to Leave Your Spartan-6 FPGA" program. My summary
13 Arty S7 50 VGA Thermal Imaging Camera
  • Sign in to reply
  • Jan Cumps
    Jan Cumps over 3 years ago in reply to Jonathan101

    (late answer) In that case, you can load the bit stream generated by Vivado , via Vivado HW Manager or Vitis, and then use the debug configuration to load your program in Vitis.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • Jonathan101
    Jonathan101 over 3 years ago

    Hi! Excellent tutorial!

    If i want to program only the PL part ( and after that to program the ELF manually from Vitis), do i need only to skip the step: "Generating a new elf file" ?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • javagoza
    javagoza over 4 years ago in reply to Jan Cumps

    You don't have permission to edit metadata of this video.
    Edit media
    x
    image
    Upload Preview
    image

    Artybot is already becoming more autonomous.

    I am using Vivado 2021.1 ML Edition and it works great. Once the project is configured, I only have to regenerate the bitstream, export the hardware and flash the new bin. Just a couple of minutes total on my machine, a Microsoft Surface Studio 2.

    INFO: [Vivado 12-4896] Successfully created Hardware Platform: C:/Xilinx/work/artys7/artybot_motor_feedback/artybot_motor_feedback_wrapper.xsa
    set_property PROGRAM.ADDRESS_RANGE  {use_file} [ get_property PROGRAM.HW_CFGMEM [lindex [get_hw_devices xc7s50_0] 0]]
    set_property PROGRAM.FILES [list "C:/Xilinx/work/artys7/artybot_motor_feedback/artybot_motor_feedback.runs/impl_1/artybot_motor_feedback_wrapper.bin" ] [ get_property PROGRAM.HW_CFGMEM [lindex [get_hw_devices xc7s50_0] 0]]
    set_property PROGRAM.PRM_FILE {} [ get_property PROGRAM.HW_CFGMEM [lindex [get_hw_devices xc7s50_0] 0]]
    set_property PROGRAM.UNUSED_PIN_TERMINATION {pull-none} [ get_property PROGRAM.HW_CFGMEM [lindex [get_hw_devices xc7s50_0] 0]]
    set_property PROGRAM.BLANK_CHECK  0 [ get_property PROGRAM.HW_CFGMEM [lindex [get_hw_devices xc7s50_0] 0]]
    set_property PROGRAM.ERASE  1 [ get_property PROGRAM.HW_CFGMEM [lindex [get_hw_devices xc7s50_0] 0]]
    set_property PROGRAM.CFG_PROGRAM  1 [ get_property PROGRAM.HW_CFGMEM [lindex [get_hw_devices xc7s50_0] 0]]
    set_property PROGRAM.VERIFY  1 [ get_property PROGRAM.HW_CFGMEM [lindex [get_hw_devices xc7s50_0] 0]]
    set_property PROGRAM.CHECKSUM  0 [ get_property PROGRAM.HW_CFGMEM [lindex [get_hw_devices xc7s50_0] 0]]
    startgroup 
    create_hw_bitstream -hw_device [lindex [get_hw_devices xc7s50_0] 0] [get_property PROGRAM.HW_CFGMEM_BITFILE [ lindex [get_hw_devices xc7s50_0] 0]]; program_hw_devices [lindex [get_hw_devices xc7s50_0] 0]; refresh_hw_device [lindex [get_hw_devices xc7s50_0] 0];
    INFO: [Labtools 27-3164] End of startup status: HIGH
    INFO: [Labtools 27-2302] Device xc7s50 (JTAG device index = 0) is programmed with a design that has 1 SPI core(s).
    program_hw_cfgmem -hw_cfgmem [ get_property PROGRAM.HW_CFGMEM [lindex [get_hw_devices xc7s50_0] 0]]
    Mfg ID : 1   Memory Type : 20   Memory Capacity : 18   Device ID 1 : 0   Device ID 2 : 0
    Performing Erase Operation...
    Erase Operation successful.
    Performing Program and Verify Operations...
    Program/Verify Operation successful.
    INFO: [Labtoolstcl 44-377] Flash programming completed successfully
    program_hw_cfgmem: Time (s): cpu = 00:00:03 ; elapsed = 00:00:53 . Memory (MB): peak = 3833.391 ; gain = 10.121
    endgroup

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • Jan Cumps
    Jan Cumps over 4 years ago

    I was holding off on writing new designs to Flash, because I'd lose the out of box example. I just found that it's downloadable from the Digilent resource page. I'm going to try this out.
    Thanks for writing the process down, including the ELF part for MicroBlaze code!