FPGA
  • Technologies
  • More
FPGA
Blog VIDOR 4000: Servo Interface
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join FPGA to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: jc2048
  • Date Created: 29 Jul 2021 9:16 PM Date Created
  • Views 6059 views
  • Likes 13 likes
  • Comments 20 comments
  • intel
  • cyclone 10
  • vidor 4000
  • fpga
  • servo
  • jc2048
  • logic design
  • arduino
Related
Recommended

VIDOR 4000: Servo Interface

jc2048
jc2048
29 Jul 2021

Introduction

 

Now a little project: a servo interface. This will give me a chance to experiment with some very simple communication between the microcontroller and the FPGA on my VIDOR 4000 board.

 

image

 

I'm going to have 8 servo channels, which the FPGA will drive out on the D0 to D7 pins of the header, and the control will be via a simple, write-only SPI interface on the SCK and MOSI pins from the SAM processor [with A0 used as the SS chip select].

 

I'm sure, if I looked around, I could find an existing design, but I thought it would make for a more interesting blog if I did one for myself, from the ground up.

 

The Design

 

I don't know much at all about model servos, so I had to look at a few datasheets, the Wikipedia page [1], and a couple of websites to find out what the waveform I'm going to generate should be like.

 

It's a repetitive waveform, where the timing of the falling edge after the positive edge determines the servo angle. Like this:

 

image

 

Traditionally, the repetition rate was 50Hz (20ms period). I'll stick to that for this blog, though it wouldn't be too difficult to change it or even make it programmable.

 

Here's the waveform again as I drew it, annotated with the various counter values in a way that's probably totally confusing, but might begin to make some sense if you read the explanation below.

 

image

 

The neutral position (for the hobby servos I'm using, that will be the centre position, which I'll call 0 degrees) occurs when the falling edge is 1500us after the rising edge.

 

I had to make a decision as to the resolution I was going to work to. Since the total travel is 120 degrees, working with 8-bit data looked reasonable as a start. That gives half a degree per bit, which I believe is about the size of the deadband with cheap servos. Being a flexible design in an FPGA, I could always increase the resolution later if I didn't like the result.

 

Since -60 degrees is at 1000us and +60 degrees is at 2000u, we can quickly work out that this is 8.3333us per degree. For half degree resolution, I need half that, ie 4.1666us. I can obtain that by dividing the 48MHz FPGA clock by 200, so I'm going to have an 8-bit prescaler to generate an enable signal every 200 clocks for the servo stuff to run on.

 

So how about the other end? The processor interface.

 

I've already mentioned that it's going to be SPI. That's because it's very simple to implement (it's even simpler with a cut-down, receive-only design like this), and there's also support for it on the SAM side of things, so it's very easy to use in the processor sketch. SPI data is bit-serial, so to receive it we'll need a shift register. In hardware terms, this is little more than a serial-data-in, parallel-data-out shift register.

 

I have a choice as to how fast I make the SPI clock when I set it up with the Arduino library. Quite arbitrarily, I'm going to set it to 1MHz. [The default on the VIDOR board seems to be 4MHz, as I discovered when I misunderstood that the SPI.beginTransaction function has to come after the SPI.begin, and not before.] That's quite fast enough for what I want to do here, but is slow enough that I won't have any problems at all with dealing with it on the FPGA. Although you might think I'd use something labelled 'clock' as a clock input to the FPGA, I'm not going to. Instead I'm going to treat it as data that I'll sample to find the positive-going edge that marks the time to pick up the data.

 

SPI is sent as a byte or multiples of a byte. I'm going to choose 2-bytes for each transaction, so my shift register will need to be 16 bits. The first byte will be the address for a channel, the next the data.

 

After the SPI interface, I need some holding registers to store the data for each channel. As well as the holding registers, I'm also going to have a working register for each channel. The transfer will occur at the start of the cycle, well out of the way of the comparisons that determine the falling edges.

 

Those stored values then get compared to a counter for generating the output waveforms. Although I could design the output stage and duplicate it eight times, with a counter for each channel, a little thought shows that the counter does exactly the same thing in each case and can be shared between all eight.

 

Putting all of that together then gives me something like this as a block diagram:

 

image

 

The VHDL

 

Here's the VHDL I ended up with. It's reasonably well commented, so you should be able to follow it and what it's doing. If anything doesn't make sense, ask in the comments.

 

---------------------------------------------------------------
--- Filename: servo.vhd                                     ---
--- Target device: 16CL016YU256C8G                          ---
---                                                         ---
--- 8-Channel Servo driver with output at 100Hz             ---
---                                                         ---
--- Interfaces to microcontroller with SPI [write only]     ---
--- 16-bit data, msb first, and mode (0,0) for the clock    ---
---                                                         ---
--- msb                                     lsb             ---
--- x x x x x A2 A1 A0  D7 D6 D5 D4 D3 D2 D1 D0             ---
---                                                         ---
--- where A is the channel address                          ---
--- D is two's complement setting in half degree increments ---
---                                                         ---
--- Jon Clift 18th July 2021                                ---
---                                                         ---
---------------------------------------------------------------
--- Rev    Date         Comments                            ---
--- 1.0    18-Jul-21                                        ---
---------------------------------------------------------------


library IEEE;
use IEEE.std_logic_1164.all;  
---use IEEE.numeric_std.all;  
use ieee.std_logic_arith.all;
use ieee.std_logic_unsigned.all;


entity servo_top is port(


   --- system signals
   CLKi:             in std_logic;
   RESn:             in std_logic;
  
   --- MKR PINS
   MKR_D:            out std_logic_vector(7 downto 0);
MOSI:             in std_logic;
SCK:              in std_logic;
SS:               in std_logic;

   --- SDRAM
   SDRAM_CK:         out std_logic;
   SDRAM_CSn:        out std_logic;
   SDRAM_CKE:        out std_logic;
  
   --- NINA module
   WM10_RESn:        out std_logic

   );


end servo_top;


architecture arch_servo_top of servo_top is


signal prescaler: std_logic_vector(7 downto 0);
signal servo_en, servo_transfer_en: std_logic;
signal servo_counter: std_logic_vector(12 downto 0);
signal spi_clk_del1, spi_clk_del2, spi_en: std_logic;
signal spi_ss_del1, spi_ss_del2, spi_ss_end: std_logic;
signal spi_data_del1, spi_data_del2: std_logic;
signal spi_shift_register: std_logic_vector(15 downto 0);
signal servo_hold_0: std_logic_vector(7 downto 0);
signal servo_hold_1: std_logic_vector(7 downto 0);
signal servo_hold_2: std_logic_vector(7 downto 0);
signal servo_hold_3: std_logic_vector(7 downto 0);
signal servo_hold_4: std_logic_vector(7 downto 0);
signal servo_hold_5: std_logic_vector(7 downto 0);
signal servo_hold_6: std_logic_vector(7 downto 0);
signal servo_hold_7: std_logic_vector(7 downto 0);
signal servo_data_0: std_logic_vector(7 downto 0);
signal servo_data_1: std_logic_vector(7 downto 0);
signal servo_data_2: std_logic_vector(7 downto 0);
signal servo_data_3: std_logic_vector(7 downto 0);
signal servo_data_4: std_logic_vector(7 downto 0);
signal servo_data_5: std_logic_vector(7 downto 0);
signal servo_data_6: std_logic_vector(7 downto 0);
signal servo_data_7: std_logic_vector(7 downto 0);
signal servo_out: std_logic_vector(7 downto 0);


begin


   --- everything that runs from the 48MHz clock input on CLKi


    clocked_stuff: process (CLKi)
        begin
            if (CLKi'event and CLKi = '1') then

                --- prescaler down to 4.16666us period (divide by 200)
          
                if (prescaler(7 downto 0) = "00000000") then --- if reached 0
                    prescaler(7 downto 0) <= "11000111"; ---   preset to 199
                    servo_en <= '1'; ---   and set enable for one cycle
                else --- else count down
                    prescaler <= prescaler - 1;
                    servo_en <= '0'; ---   keeping enable low rest of time
                end if;


--- the servo counter counts every 4.16666us (equivalent to half a degree on the servo)
--- period is 4800 counts: 4.16666us x 4800 = 20ms (100Hz)

                if (servo_en = '1') then
  if (servo_counter(12 downto 0) = "1000111010111") then --- if reached 4567
servo_counter(12 downto 0) <= "1111100011000"; --- preset (skip ahead) to 7960 (-232)
servo_out(7 downto 0) <= "11111111"; --- and set all the servo outputs high
                     servo_transfer_en <= '1'; ---   
else --- else
servo_counter <= servo_counter + 1; --- count down
                     servo_transfer_en <= '0'; ---   
end if;
end if;


--- the SPI interface

spi_clk_del1 <= SCK;
spi_clk_del2 <= spi_clk_del1;

spi_ss_del1 <= SS;
spi_ss_del2 <= spi_ss_del1;

spi_data_del1 <= MOSI;
spi_data_del2 <= spi_data_del1;


if((spi_clk_del1 = '1') and (spi_clk_del2 = '0')) then
spi_en <= '1';
else
spi_en <= '0';
end if;


if((spi_ss_del1 = '1') and (spi_ss_del2 = '0')) then
spi_ss_end <= '1';
else
spi_ss_end <= '0';
end if;


if((spi_en = '1') and (spi_ss_del2 = '0')) then

spi_shift_register(15 downto 1) <= spi_shift_register(14 downto 0);
spi_shift_register(0) <= spi_data_del2;

end if;


--- at end of ss (SPI 'chip select' going high at end of transfer)
--- transfer data from spi shift register to the addressed 
--- servo data holding register
--- bit 7 is negated to convert 2's complement back to binary

if(spi_ss_end = '1') then

case (spi_shift_register(10 downto 8)) is
when "000" =>
servo_hold_0(6 downto 0) <= spi_shift_register(6 downto 0);
servo_hold_0(7) <= not spi_shift_register(7);
when "001" =>
servo_hold_1(6 downto 0) <= spi_shift_register(6 downto 0);
servo_hold_1(7) <= not spi_shift_register(7);
when "010" =>
servo_hold_2(6 downto 0) <= spi_shift_register(6 downto 0);
servo_hold_2(7) <= not spi_shift_register(7);
when "011" =>
servo_hold_3(6 downto 0) <= spi_shift_register(6 downto 0);
servo_hold_3(7) <= not spi_shift_register(7);
when "100" =>
servo_hold_4(6 downto 0) <= spi_shift_register(6 downto 0);
servo_hold_4(7) <= not spi_shift_register(7);
when "101" =>
servo_hold_5(6 downto 0) <= spi_shift_register(6 downto 0);
servo_hold_5(7) <= not spi_shift_register(7);
when "110" =>
servo_hold_6(6 downto 0) <= spi_shift_register(6 downto 0);
servo_hold_6(7) <= not spi_shift_register(7);
when "111" =>
servo_hold_7(6 downto 0) <= spi_shift_register(6 downto 0);
servo_hold_7(7) <= not spi_shift_register(7);
when others =>
end case;

end if;


--- update the data registers from the holding registers
--- do this at start of period, well before they get used

if(servo_transfer_en = '1') then

servo_data_0 <= servo_hold_0;
servo_data_1 <= servo_hold_1;
servo_data_2 <= servo_hold_2;
servo_data_3 <= servo_hold_3;
servo_data_4 <= servo_hold_4;
servo_data_5 <= servo_hold_5;
servo_data_6 <= servo_hold_6;
servo_data_7 <= servo_hold_7;
end if;

  --- set each servo output low at the appropriate time
--- (they were all set high at the same instant: see servo counter above)

                if ((servo_en = '1') and (servo_counter(10 downto 8) = "000")) then

if (servo_counter(7 downto 0) = servo_data_0(7 downto 0)) then --- if same
servo_out(0) <= '0'; --- set output low
end if;


if (servo_counter(7 downto 0) = servo_data_1(7 downto 0)) then
servo_out(1) <= '0';
end if;


if (servo_counter(7 downto 0) = servo_data_2(7 downto 0)) then
servo_out(2) <= '0';
end if;


if (servo_counter(7 downto 0) = servo_data_3(7 downto 0)) then
servo_out(3) <= '0';
end if;


if (servo_counter(7 downto 0) = servo_data_4(7 downto 0)) then
servo_out(4) <= '0';
end if;


if (servo_counter(7 downto 0) = servo_data_5(7 downto 0)) then
servo_out(5) <= '0';
end if;


if (servo_counter(7 downto 0) = servo_data_6(7 downto 0)) then
servo_out(6) <= '0';
end if;


if (servo_counter(7 downto 0) = servo_data_7(7 downto 0)) then
servo_out(7) <= '0';
end if;


end if;
         
end if;
              
end process clocked_stuff;


--- connect servo outs to the MKR pins

MKR_D <= servo_out;

--- hold some of the unused, board hardware components in inactive state
         
SDRAM_CK <= CLKI;
SDRAM_CSn <= '1';
SDRAM_CKE <= '1';
         
WM10_RESn <= '0';




end arch_servo_top;

 

(Sorry about the strange formatting. The original was fine. If I have the energy tomorrow, I'll try editing it.)

 

I haven't put a licence on this (I'm still unsure what the best way to licence something like this is). Effectively, you can do what you like with it, but there's no warranty, no claim of fitness for purpose, nor any obligation on me to support it in any way whatsoever.

 

The Sketch

 

For the sketch, I modified the template provided here [thank you, C Helmich]:

 

https://github.com/chelmich/vidor_template/tree/master/arduino/vidor_template

 

just adding in the SPI stuff for testing the interface from the processor to the FPGA.

 

Here's how the sketch part looked after I'd finished:

 

#include <wiring_private.h>
#include <SPI.h>
#include "jtag.h"
#include "defines.h"


__attribute__ ((used, section(".fpga_bitstream_signature")))
const unsigned char signatures[4096] = {
    #include "signature.h"
};


__attribute__ ((used, section(".fpga_bitstream")))
const unsigned char bitstream[] = {
    #include "app.h"
};


void FPGA_init (){
    // enable fpga clock
    pinPeripheral(30, PIO_AC_CLK);
    clockout(0, 1);


    // wait for clock to come up (unnecessary?)
    delay(1000);


    // send bitstream over jtag
    uint32_t ptr[1] = {3};
    jtagInit();
    mbPinSet();
    mbEveSend(ptr, 1);
    jtagDeinit();
}


void setup (){
    FPGA_init();


    delay(1000);


    // turn on built in LED
    pinMode(LED_BUILTIN, OUTPUT);


    // set A0 as output - this is SS (device select) for SPI
    pinMode(A0, OUTPUT);
    // start SPI
    SPI.begin();
}


void loop (){


unsigned char servoChannel;
signed char servoData[] = {-128,-120,-60,0,60,90,120,127};


SPI.beginTransaction(SPISettings(1000000,MSBFIRST,SPI_MODE0));


while(1){
  for(servoChannel=0;servoChannel<8;servoChannel++) {
    digitalWrite(A0, LOW);                  // SS low 
//    delayMicroseconds(2);
    SPI.transfer(servoChannel);             // send channel
    SPI.transfer(servoData[servoChannel]);  // send channel data
//    delayMicroseconds(2);
    digitalWrite(A0, HIGH);                 // SS high
//    servoData[servoChannel] = (signed char) random(256);  // pick new random value for next time through
    servoData[servoChannel]++;  // 
    delayMicroseconds(10);
    }
  delay(100);
  }
  
SPI.end();
}

 

 

My app.h came from my own VHDL design, and the jtag.c and jtag.h files were the same as the template.

[There's no mention of a licence, so I presume it's a generous 'do what you like with this' piece of code.]

 

The Servo Interface Working

 

Here are some oscilloscope traces from the working design. This is with the initialisation values from my code.

 

signed char servoData[] = {-128,-120,-60,0,60,90,120,127};

 

 

image

 

This first one shows the complete cycle. The logic-analyser section shows the MKR D0 to D7 outputs from the VIDOR headers. The one marked '0' is D0, and so on. The yellow, analogue trace is a duplicate of D0.

 

We can see the various pulse widths as they should be. This also shows that I've got the output frequency correct at 50Hz (give or take a little variation because of the jitter on the FPGA's clock).

 

Here it is again, in a bit more detail on a faster timebase:

 

image

 

The cursors I've placed at the 1000us and 2000us positions, which line up with values of -120 and +120 sent from the microcontroller [effectively, -60 and +60 degrees, the limits of my servos].

 

With this next one, I have the data for each of the channels incrementing 10 times a second. With the phosphor set to infinity, the analogue trace then shows all the possible positions for the falling edge [the analyser section doesn't persist in the same way as the analogue trace, so you only see the most recent trace there].

 

image

 

Finally, here's a quick look at the SPI. Trace '0' is the clock, '1' is the data, and '2' is the SS signal.

 

image

 

Conclusions

 

That didn't go too badly, and I've got the beginnings of a working design. It uses about 1.5% of the logic blocks of the FPGA, so there's plenty left for extending or elaborating the design, or for other uses entirely.

 

Later, I'll try wiring up some servos [if I can find them: I think I might have three, somewhere or other] and then I'll see if it works for real.

 

References

 

[1] https://en.wikipedia.org/wiki/Servo_(radio_control)

[2] VIDOR 4000: Johnson Counter

[3] VIDOR 4000: Clock Jitter

 

If you found this interesting and would like to see other blogs I've written, a list can be found here: jc2048 Blog Index

  • Sign in to reply

Top Comments

  • michaelkellett
    michaelkellett over 5 years ago +4
    Thanks for the blog. I'll offer a couple of suggestions re. the VHDL which I hope may be useful to you and others. LIBRARIES In your VHDL you have: library IEEE; use IEEE.std_logic_1164.all; ---use IEEE…
  • michaelkellett
    michaelkellett over 5 years ago in reply to jc2048 +4
    I have some nice little Chinese (cheap £16) boards with Cyclone 10LP and an SDRAM. I have some more on the way with a Xilinx Artix 35 and a DDRAM. I was looking for somehting interesting to do with them…
  • Jan Cumps
    Jan Cumps over 5 years ago +4
    The design works. Tested with an Sparkfun micro servo. www.youtube.com/watch I think that servo is the same as the blue ones you use, just older black housing.
Parents
  • michaelkellett
    michaelkellett over 5 years ago

    Thanks for the blog.

     

     

    I'll offer a couple of suggestions re. the VHDL which I hope may be useful to you and others.

     

     

    LIBRARIES

     

     

    In your VHDL you have:

     

     

        library IEEE; 

        use IEEE.std_logic_1164.all;   

        ---use IEEE.numeric_std.all;   

        use ieee.std_logic_arith.all; 

        use ieee.std_logic_unsigned.all; 

     

     

    The true standard is numeric_std and this should always be used.

     

    ieee.std_logic_arith and  ieee.std_logic_unsigned are not actually standards and have problems.

     

    To get lots of information and opinion about why, I suggest Googling - ieee.std_logic_arith.

     

     

    To my mind one of the major problems with ...arith and ... unsigned is that they break VHDLs strong typing.

     

     

    For example, in your code you declare signal prescaler: std_logic_vector(7 downto 0); 

     

    and then later you have:

     

    prescaler <= prescaler - 1;

     

     

    Prescalar has been declared as std_logic_vector -  which is group of logical bits. You use exactly the same declaration for servo_out.

     

     

    The intention is that prescaler is an integer and that servo_out is 8 independent logic signal bits.

     

    If you use numeric.std then you just can't subtract 1 from a std_logic_vector.

     

    You would need to decalre it as signal prescaler unsigned(7 downto 0);

     

    This is good because you are not able to make mistakes like servo_out <= servo_out - 1;

     

     

    ARRAYS

     

     

    If you made servo_hold and servo_data into arrays you could save a great deal of typing (and sources of error).

     

    But even better you could easily make you code much more flexible so that the exact same code could give you 1, 2 ....n servos.

     

    It wouldn't use any less resources but it would be much easier to maintain.

     

     

    MEMORY BLOCK

     

    You are using registers for servo_data and servo_hold, but as you mention the FPGA has a great many clock cycles available for

    each pulse width step. You could use a memory block in the FPGA for the servo registers and easily manage as many as 64 with no loss of performance.

    This is probably not worth the effort for 8 servos (swaps 128 registers for 1 memory block) but at 64 would swap 1024 regsiters for 1 memory block.

     

     

    I hope this is useful.

     

    MK

    • Cancel
    • Vote Up +4 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • michaelkellett
    michaelkellett over 5 years ago

    Thanks for the blog.

     

     

    I'll offer a couple of suggestions re. the VHDL which I hope may be useful to you and others.

     

     

    LIBRARIES

     

     

    In your VHDL you have:

     

     

        library IEEE; 

        use IEEE.std_logic_1164.all;   

        ---use IEEE.numeric_std.all;   

        use ieee.std_logic_arith.all; 

        use ieee.std_logic_unsigned.all; 

     

     

    The true standard is numeric_std and this should always be used.

     

    ieee.std_logic_arith and  ieee.std_logic_unsigned are not actually standards and have problems.

     

    To get lots of information and opinion about why, I suggest Googling - ieee.std_logic_arith.

     

     

    To my mind one of the major problems with ...arith and ... unsigned is that they break VHDLs strong typing.

     

     

    For example, in your code you declare signal prescaler: std_logic_vector(7 downto 0); 

     

    and then later you have:

     

    prescaler <= prescaler - 1;

     

     

    Prescalar has been declared as std_logic_vector -  which is group of logical bits. You use exactly the same declaration for servo_out.

     

     

    The intention is that prescaler is an integer and that servo_out is 8 independent logic signal bits.

     

    If you use numeric.std then you just can't subtract 1 from a std_logic_vector.

     

    You would need to decalre it as signal prescaler unsigned(7 downto 0);

     

    This is good because you are not able to make mistakes like servo_out <= servo_out - 1;

     

     

    ARRAYS

     

     

    If you made servo_hold and servo_data into arrays you could save a great deal of typing (and sources of error).

     

    But even better you could easily make you code much more flexible so that the exact same code could give you 1, 2 ....n servos.

     

    It wouldn't use any less resources but it would be much easier to maintain.

     

     

    MEMORY BLOCK

     

    You are using registers for servo_data and servo_hold, but as you mention the FPGA has a great many clock cycles available for

    each pulse width step. You could use a memory block in the FPGA for the servo registers and easily manage as many as 64 with no loss of performance.

    This is probably not worth the effort for 8 servos (swaps 128 registers for 1 memory block) but at 64 would swap 1024 regsiters for 1 memory block.

     

     

    I hope this is useful.

     

    MK

    • Cancel
    • Vote Up +4 Vote Down
    • Sign in to reply
    • More
    • Cancel
Children
  • Jan Cumps
    Jan Cumps over 5 years ago in reply to michaelkellett

    Thank you Michael.

     

    LIBRARIES

    Do I understand it correctly that whenever something is used for calculation, it's best to use the numeric_std types,

    and when something holds a set of bits, it should be a std_logic_vector?

     

    ARRAYS

    Use a loop like this?

     

    type servo_bits is array (0 to 7) of std_logic_vector(7 downto 0);
    signal servo_data_array: servo_bits;
    signal servo_hold_array: servo_bits;
     
    
    -- ...
      if rising_edge(i_clk) then
        l_servo_write_data: for ii in 0 to servo_hold_array'length-1 loop
          servo_data_array(ii) <= servo_hold_array(ii);
        end loop l_servo_write_data;

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • michaelkellett
    michaelkellett over 5 years ago in reply to Jan Cumps

    Keeping numbers in their proper types helps a lot, especially when you want to use  a mix of signed and unsigned in the same file.

     

    Yes, your loop is just what I meant and the big advantage is that you change that 7 to make the same code do more or less servos.

     

    MK

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • Jan Cumps
    Jan Cumps over 5 years ago in reply to michaelkellett

    I'm going to check if this works too:

    servo_data_array <= servo_hold_array;

    I've read that it should work, and that the synthesised design should be similar, because the for loop as used above gets "synthesised away".

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • jc2048
    jc2048 over 5 years ago in reply to michaelkellett

    All good suggestions and I possibly agree with you on all of them, but with some reservations.

     

    In reverse order

     

    MEMORY

     

    I really like block memory, not just for register storage, but things like swinging buffers and crossing clock domains. I umm-ed and arr-ed in this case, but went with the registers because a) I'm trying to show logic design being done, and introducing block memories is too much at once and would add complexity that would obscure the essential simplicity of data being simply shuffled across at the right time, and b) when I looked at the register usage and saw it was only 1.5% of the total available, it really didn't seem worth doing anything more complicated.

     

    ARRAYS

     

    I'm weak on the more abstract side of writing VHDL (because I had to teach myself quickly, on the job, and the focus was always achieving very specific tasks), so I need to work on this, particularly with the signal processing stuff which I can see, from the course of blogs done by fpgaguru, benefits enormously from the kind of abstraction this can bring. Curiously, I would defend not using arrays in this case for the same reason [abstraction]. We have a lot of people here who operate with the kind of abstract framework that goes with sequential processing and who are getting interested in fpga design. Unfortunately, if you show them all the language constructs and ideas that derive from the simulation side [which has to run on a sequential processor], they'll treat logic design as a coding exercise.

     

    LIBRARY (WARS)

     

    This one is about abstraction, too (and possibly the philosophy of computation, if there is such a subject). When I write +1 or -1 as an operation on a logic vector [by using _unsigned to overload the operator], I'm not really describing a numerical algorithm. I'm simply indicating to the synthesis that I want a counter that either increments or decrements. Casting it as a numeric function, to my mind, gets in the way. It generalises what I know to be a special case and moves us away from the hardware. It's giving us abstraction where we really don't need it.

     

    But you're right. Anyone in education needs to do it the way it's taught, because they have exams to pass, and anyone working in industry needs to do it, either simply because it's the 'house style', or because of the practicalities of working as part of a team, or whatever.