FPGA
  • Technologies
  • More
FPGA
Blog XuLA2 FPGA - Rotary Encoder and VHDL
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join FPGA to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: Jan Cumps
  • Date Created: 2 Feb 2017 12:34 PM Date Created
  • Views 2562 views
  • Likes 5 likes
  • Comments 4 comments
  • spartan_6
  • rotary_encoder
  • fpga
  • xula2
  • jcxula2
Related
Recommended

XuLA2 FPGA - Rotary Encoder and VHDL

Jan Cumps
Jan Cumps
2 Feb 2017

How to use a rotary encoder with the XuLA2 and the Spartan-6 FPGA.

image

Another real world example: I'm checking if the Xess Rotary Encoder library works with the encoder I use in a GaN half-bridge design.

TL;DR: yes it works


Xess has a plug-in board with a rotary encoder. I'm not using that module (called a StickIt!) - but I'm using the sample project that comes with it.

 

StickIt!

 

Hat Shield Cape Wing. All names were taken except the coolest one.

StickIt!s are tiny modules that work togethet with the XuLa.

A XuLA board is small. Still it manages to expose loads of FPGA pins. Plug the XuLA in a breadboard and you have access to them.

Alternatively,  you can go StickIt!.

 

image

To start using the StickIt! modules, there's a motherboard. You dock the XuLA onto it and the signals become available in a few ways:

  • as a Raspberry Pi Hat (it can be used as a Hat or you can plug hats onto it. Your call).
  • as StickIt! ports where you can you can plug StickIt! modules into. The motherboard can host three modules.

 

In this blog I'm attaching the rotary encoder contacts to StickIt! port PM1. I just use patch cables to make the connections between my GaN PCB and that connector.

If you don't have the motherboard, you can make the connections directly to the XuLA2. I've pasted the xref tables you need to find out the correct pins.

 

This is the schematic of my rotary encoder. It's identical to the Xess module - except that I've added debounce capacitors.

 

imageimage

 

 

The encoder is a Panasonic EVQ-VVD00203B Square SMD Encoder.

That's not the same model as the one on the Xess board but it works the same. This one doesn't have a push-button built in.

image

 

 

I'm plugging it into the PM1 of the motherboard. The power comes from the XuLA board, so you have to populate the XuLA PWR jumper and remove all others.

On this image you can see where you have to insert the jumper wires coming from the encoder.

image

Pin 6, VCC, goes to the 3V3 of the encoder circuit.

Pin 5, GND, to the circuit's GND

Pin 1, DO, to one of the encoder's switch contacts

Pin 2, D2, to the other switch contact.

The table also shows the channel numbers. Use these if you work without the motherboard. They represent the XuLA2 pins.

 

 

image

 

In this table you can find the mapping between the channel number and the FPGA signal.

You'll use that to define the pins in your project's constraint file.

image

For the pins that I've used, this is the constraint info.

 

# PM1 connections for rotary encoder module.
net rotEncA_i   loc=r7;
net rotEncB_i   loc=r16;

 

Update your project's .ucf file to reflect that.

 

image

 

I haven't changed a single line of code. I just went trough the typical FPGA build steps and generated the bitfile.

 

> xsload --fpga rotaryencodertest.bit
Success: Bitstream in rotaryencodertest.bit downloaded to FPGA on XuLA2-LX25!

 

Then I used the Python test script that's part of the project. It checks the (defined in the VHDL project)  register that holds the accumulated value, and prints it to the command line.

To start the test, execute this command:

 

> rot_enc_test.py

 

Rotate the encoder like a madman and see the results on your command prompt:

image

 

If you don't have a rotary encoder, break open an old mouse. The scroll wheel is often an encoder.

 

XuLA2 FPGA - First Impressions of the Development Tools
XuLA2 FPGA - SD Card Read and Write
XuLA2 FPGA - Rotary Encoder and VHDL
XuLA2 FPGA - PWM with Dead Band in VHDL
XuLA2 FPGA - Up the Clock
XuLA2 FPGA - Utility to Generate Pin Assignments
  • Sign in to reply

Top Comments

  • Jan Cumps
    Jan Cumps over 9 years ago in reply to Jan Cumps +2
Parents
  • Jan Cumps
    Jan Cumps over 9 years ago

    This was supposed to be my first new attempt to create a VHDL module:  a PWM signal with deadband.

    I have a few things right image 

    The frequency, the pin assignments, and the fact that the 2 signals are "almost" complementary.

     

     

    image

     

    Aaah, VHDL isn't too easy if you don't have the natural hang of it. But at least it compiles, loads and runs.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • Jan Cumps
    Jan Cumps over 9 years ago

    This was supposed to be my first new attempt to create a VHDL module:  a PWM signal with deadband.

    I have a few things right image 

    The frequency, the pin assignments, and the fact that the 2 signals are "almost" complementary.

     

     

    image

     

    Aaah, VHDL isn't too easy if you don't have the natural hang of it. But at least it compiles, loads and runs.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Children
  • Jan Cumps
    Jan Cumps over 9 years ago in reply to Jan Cumps

    ...the error is definitely in my deadband generation code. The simple complementary signal generation works sweet:

     

    image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • Jan Cumps
    Jan Cumps over 9 years ago in reply to Jan Cumps

    Yay Yay Yes

    image

     

    2 complementary signals with deadband in VHDL

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • Jan Cumps
    Jan Cumps over 9 years ago in reply to Jan Cumps