Power & Energy
  • Technologies
  • More
Power & Energy
Blog
  • Blog
  • Forum
  • Quiz
  • Documents
  • Polls
  • Events
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New

Blog

  • Tags
  • Subscribe by email
  • More
  • Cancel
  • Building a Smart Electronic Load | DAC and Initial Firmware (#2)

    Attila Tőkés
    Attila Tőkés
    Hi E14 Community!  Quick update on the Smart Electronic Load project:    Previous blog posts: Building a Smart Electronic Load | Introduction (#1)    I started testing the stages of the load one-by-one, startin...
    • 8 Jan 2025
  • Researchers Develop Carbon-14 Battery That Could Outlive Humans

    Catwell
    Catwell
    Sample of a diamond battery. (Image Credit: University of Bristol) Engineers at the University of Bristol developed the world's first nuclear-powered battery, which they claim can generate electricity via the reaction of a radioactive isotope pl...
    • 8 Jan 2025
  • LabView process to measure DC:DC converter efficiency

    Jan Cumps
    Jan Cumps
    I'm evaluating a Vishay microBRICK switch mode converter. The converter is Vishay's  Reference Design for a 4.5 V to 60 V Input, 6 A, DC/DC Synchronous Buck Module SIC967 . One of my lab tests is to validate efficiency sp...
    • 4 Jan 2025
  • DC-DC Converters Take Advantage of the Latest Transformer Tech for Next-Gen Applications

    Catwell
    Catwell
    (Image credit: Bourns) Isolated DC-DC converters are electronic circuits or electromechanical devices that convert electrical energy from one DC voltage level to another while being electrically isolated between the input and output. That isolation...
    • 31 Dec 2024
  • Building a Smart Electronic Load | Introduction (#1)

    Attila Tőkés
    Attila Tőkés
    It happens that I had a couple of LGA775 coolers laying around from an old PC. The PC these cooler belonged to was discarded a long time ago, but I kept the coolers to be used in future power electronic projects. Back in November I decided to tr...
    • 30 Dec 2024
  • Researchers Develop Triboelectric Generator for Wearables

    Catwell
    Catwell
    The created the GPE-TENG by sandwiching a gel electrode between two triboelectric ecoflex layers. (Image Credit: Dongguk University-Seoul) We're seeing a growing demand for wearables, like medical sensors, trackers, and smartwatches, and these r...
    • 12 Dec 2024
  • Building a Nickel-Metal Hydride (NiMH) Charger

    shabaz
    shabaz
    Table of Contents Introduction Charging Principle and Features Circuit Description A Worked Example: 4 x AA Cells Building It Tests Summary Introduction There was a recent discussion regarding thoughts on a circuit for charging NiMH batteries. I...
    • 22 Nov 2024
  • Today’s Smart Infrastructure Rely on the Latest Environmental and HVAC Systems to Maintain Peak Efficiency

    Catwell
    Catwell
    (Image credit: Pixabay) Smart buildings are characterized as a modern structure that uses advanced technologies to automate, connect, analyze and optimize performance across a multitude of devices, systems and platforms. In today’s world, sma...
    • 12 Nov 2024
  • Oxford Researchers Develop a Droplet Battery for Medical Devices

    Catwell
    Catwell
    The researchers developed a tiny soft rechargeable lithium-ion battery for minimally invasive medical devices. (Image credit: Yujia Zhang) University of Oxford researchers have recently developed a tiny lithium-ion battery made of biocompatible hydr...
    • 12 Nov 2024
  • Ski Slope Power Plant in Denmark Produces Enough Power for 150k Homes Annually

    Catwell
    Catwell
    The CopenHill power plant features a ski slope, garden, cross-fit area, and hiking and running trail. (Image Credit: Bhjarke Ingels Group) Five years ago, Bhjarke Ingels Group (BIG) completed the CopenHill, a waste-to-energy power plant in Copenhag...
    • 16 Oct 2024
  • Stretchable Fabric Converts Motion Energy into Electricity

    Catwell
    Catwell
    The fabric is made from a polymer that converts mechanical stress into electrical energy when pressed or squeezed. (Image credit: NTU Singapore via YouTube) Scientists from Nanyang Technical University (NTU) Singapore have developed a stretchable, w...
    • 15 Oct 2024
  • Researchers Develop Tiny Nuclear Battery that Could Provide Power for Decades

    Catwell
    Catwell
    The nuclear battery design uses a small sample of americium embedded in a polymer crystal, which was combined with a photovoltaic cell and then packaged within a quartz cell. The design is rumored to be 8,000 times more efficient than previous desig...
    • 2 Oct 2024
  • Largest Solar Plant Facility Under Construction in Illinois

    Catwell
    Catwell
    (Image Credit: Michael_Pointner/pixabay) Swift Current Energy has started building the Double Black Diamond Solar Facility, the largest solar project in southern Illinois. Once complete, the solar facility expects to produce 800 megawatts of electri...
    • 1 Oct 2024
  • E-fuse Demand Rises as Computer Chip Technology Advances

    Catwell
    Catwell
    E-fuses can be integrated into chip designs or added to a system to protect devices from multiple failure vectors, including overcurrent, overvoltage clamping, current-induced thermal protection, and short-circuit protection. (Image credit: Pixabay)...
    • 20 Sep 2024
  • Researchers Use Supercomputers to Make a New Solar Discovery

    Catwell
    Catwell
    A large hole polaron in the halide double perovskite. The arrows are indicative of atomic displacements with the hole at the center. (Image Credit: J. Lafuente-Bartolome.) Researchers at the Texas Advanced Computing Center are gaining more insight i...
    • 12 Sep 2024
  • First-Even Potassium-Ion Battery Launched and It Could Replace Lithium-Ion Batteries

    Catwell
    Catwell
    Group1 recently launched the world's first potassium-ion battery, operating at 3.7V. (Image Credit: Group1) Group1 recently developed and launched the first-ever 18650 potassium-ion battery, which could replace lithium-ion batteries powering po...
    • 8 Aug 2024
  • New Model of Ionic Transport in Porous Materials Could Bring Efficient Supercapacitors

    Catwell
    Catwell
    Researchers have discovered how tiny charged particles move within complex miniscule pores, which could be used to design more efficient supercapacitors. (Image credit: University of Colorado) Researchers from CU Boulder have discovered how small ch...
    • 31 Jul 2024
  • ITER Has Assembled Its Magnetic System – Fusion Reactor

    Catwell
    Catwell
    The toroidal field magnets surround the tokamak vacuum vessel. (Image Credit: ITER) ITER is inching closer to going online. Its massive superconducting magnets, required for the reactor core construction, were recently transported to southern France...
    • 15 Jul 2024
  • Wind Fence Could Be the Future of Power Generation

    Catwell
    Catwell
    The wind fence can generate 2,200 kW of power every year. (Image Credit: Airiva) New York-based designer Joe Doucet developed a wind fence to generate clean energy for urban landscapes. This modular fence is made of twisted wind turbines and has the...
    • 5 Jul 2024
  • Michigan to See Future Green Energy Solutions Power the State with A Massive Energy Storage Facility

    Catwell
    Catwell
    DTE Energy will build a large-scale energy storage facility where the Trenton Channel Power Plant once operated. (Image Credit: DTE) Recently, DTE Energy announced plans to build a large lithium-iron-phosphate battery storage facility at a coal-bur...
    • 11 Jun 2024
  • Researchers Improve Power Conversion Efficiency of Binary Organic Solar Cells

    Catwell
    Catwell
    The BrBACz-based binary OSC can achieve a power conversion efficiency of 19.70&. (Image Credit: NIMTE) Researchers at the Ningbo Institute of Materials Technology and Engineering (NIMTE) of the Chinese Academy of Sciences developed two self-asse...
    • 6 Jun 2024
  • They’ve Done It! Researchers Grew Diamonds That Conduct Electricity

    Catwell
    Catwell
    Chinese researchers claim they produced diamonds that conduct electricity. (Image Credit: Bas van den Eijkhof/Unsplash) We all know about diamonds and their heat-conductive properties. They also have a high cost, which sparked a new industry: treati...
    • 15 Mar 2024
  • Revolutionizing Graphene Batteries for Cordless Tools

    Catwell
    Catwell
    Graphene could be used in cordless tools, providing more run time and improved efficiency. (Image Credit: seagul/pixabay) Most of us own cordless tools, and these have improved due to lightweight, advanced, and smaller batteries. For example, we&#3...
    • 11 Mar 2024
  • Need help with a school project

    M_G
    M_G
    Hello. I am currently a student and need help in the subject of electromagnetism. What can be the maximum weight a homemade electromagnet can carry given by the power source of a 2 x 1.5 AA Battery? Afterwhich, may I ask for the type of wire, core, a...
    • 10 Mar 2024
  • Microsoft Surface Book 2 Power Supply Teardown

    shabaz
    shabaz
    Table of Contents Introduction Removing the Case and Shielding What Parts are Used? Introduction I’ve got through a lot of model “1798” power supplies! They come with Surface laptops, and they don’t seem to last much b...
    • 27 Feb 2024
<>