Test & Tools
  • Technologies
  • More
Test & Tools
Blog Keithley DMM6500: How to Create a Bitmap for a Custom App
  • Blog
  • Forum
  • Documents
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Test & Tools to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: Jan Cumps
  • Date Created: 15 Jan 2019 12:45 AM Date Created
  • Views 4576 views
  • Likes 18 likes
  • Comments 12 comments
  • RoadTest
  • dmm6500
  • rt
  • keithley
Related
Recommended

Keithley DMM6500: How to Create a Bitmap for a Custom App

Jan Cumps
Jan Cumps
15 Jan 2019

I'm road testing the  Keithley Bench Digital Multimeter DMM6500.

The instrument can run apps, and you can roll your own (what a great time do be alive image).

In this blog, I'll show how you can show images on the display.

image

 

 

Why, Jan?

 

Apps make it possible to change how the instrument operates. It can give a completely different look and feel.

When you are using this for prescribed situations, or in a fixed setup, this can help to have repeatable results.

 

You can use this to run a set op predefined scenarios, show info in an operator friendly way, show binning info, show tag cards with instructions.

There's a pre-installed app on the device that shows such an instruction card flow, called Instructions.

It's a set of 5 cards that you can scroll to, showing where the main user interface functions are.

Here's an example of one of the instruction cards.

 

image

 

Example

 

On the Keithley product page for this meter, the source for this app is available via the downloads button.

Let's change that example and replace the first card by a custom one, just to see if it works.

 

You need to have the image, in PNG format.

An image of 800 * 430 fills the whole width and fits under the title bar.

You have to convert it to BASE64.

Here's a website that can do that conversion online: https://onlinepngtools.com/convert-base64-to-png

 

Paste the BASE64 content in the application source file that you downloaded from Keithley's website, over the content of the first image.

image

 

Put it between these lines of code, replacing anything that was in there originally:

 

loadimage home intro_DMM
-- paste the content here
endimage
loadimage board2 intro_DMM

 

Save the script to a USB stick (.tspa extension). Then press the APPS button, and navigate to the USB.

Then select the app, and RUN it.

You'll see the image you created pop up first. When you press the TRIGGER button, it will navigate to the remaining original tag cards.

Home brings you back to your custom image.

 

image

 

If you want to have a look at the original images from the script, you can use this link to reverse from BASE64 to PNG:

https://onlinepngtools.com/convert-base64-to-png

 

Related Blog
Software Control Options Pt 1 - TSP Script Builder, LabVIEW, Web Interface
TSP Script Example - Measure Power
How to Create a Bitmap for a Custom App
Verify a µCurrent Manually
Verify a µCurrent in an Automated Setup
Measure Amp-Hours of a microcontroller with a µCurrent
Trigger from External Trigger Input
Trigger from External Trigger Input in LabVIEW
Software Control Options Pt 2 - Test Commands with Communicator
App to Hold Measurements
Store Multiple Measurements Manually
Keithley DMM6500: Script Example - Externally Triggered Measurements

 Keithley DMM6500: Software Control Options Pt 3 - VSCode TSP Toolkit 

  • Sign in to reply

Top Comments

  • shabaz
    shabaz over 7 years ago +2
    It's a great feature! I couldn't resist trying this procedure out. Here's a space theme: ..and the 800x430 size .png file, for anyone who wants to use it (click on it first so that it is the correct size…
  • michaelkellett
    michaelkellett over 7 years ago in reply to Jan Cumps +2
    In a rush now so may think of something else later. The neatest thing I've done with the 7510 was to use the data acquisition mode to capture data from a low frequency filter (customer had designed it…
  • michaelkellett
    michaelkellett over 7 years ago in reply to Jan Cumps +2
    Hello Jan, I'm impressed by what you have done already - I've only ever programmed these things just enough to get the immediate job done so it's great if you do it for free To help you on your way: https…
Parents
  • Jan Cumps
    Jan Cumps over 7 years ago

    I've checked the instrument's reference guide and the help from the Test Script Builder. I can't find the info on how to influence the graphs.

    I haven't found the API info for some calls that Keithley are making in their scripts. The Intro script uses ki.display, ki.getpixel, .... and I haven't found the info on those.

    The same for the drawing functions they use in some apps, like display.create() to draw lines and circles.

    There may be a public document out there, but I haven't found it yet.

     

    I found the way to display images in this blog by accident. I recognised that the intro script used BASE64 or something like that (I guessed the 64 and it was bingo the first time image ).

    I only learned the images had to be PNG because the instrument complained that the first image I tried to load wasn't PNG format image.

    At that time I knew the encoding was right and the format was wrong. A few minutes later I had a  first image on the screen.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • Jan Cumps
    Jan Cumps over 7 years ago in reply to Jan Cumps

    Jan Cumps  wrote:

     

    I've checked the instrument's reference guide and the help from the Test Script Builder. I can't find the info on how to influence the graphs.

    I haven't found the API info for some calls that Keithley are making in their scripts. The Intro script uses ki.display, ki.getpixel, .... and I haven't found the info on those.

    The same for the drawing functions they use in some apps, like display.create() to draw lines and circles.

    There may be a public document out there, but I haven't found it yet.

    ...

    An engineer from Keithley confirms that this documentation will be released later this year: New Keithley DMM6500 and now DAQ6510 - Page 14

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • Jan Cumps
    Jan Cumps over 7 years ago in reply to Jan Cumps

    Jan Cumps  wrote:

     

    I've checked the instrument's reference guide and the help from the Test Script Builder. I can't find the info on how to influence the graphs.

    I haven't found the API info for some calls that Keithley are making in their scripts. The Intro script uses ki.display, ki.getpixel, .... and I haven't found the info on those.

    The same for the drawing functions they use in some apps, like display.create() to draw lines and circles.

    There may be a public document out there, but I haven't found it yet.

    ...

    An engineer from Keithley confirms that this documentation will be released later this year: New Keithley DMM6500 and now DAQ6510 - Page 14