Test & Tools
  • Technologies
  • More
Test & Tools
Blog SCPI on a Linux Board - Part 2a: PiFace Digital C programming
  • Blog
  • Forum
  • Documents
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Test & Tools to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: Jan Cumps
  • Date Created: 16 Jun 2018 9:40 PM Date Created
  • Views 2384 views
  • Likes 7 likes
  • Comments 4 comments
  • raspberry
  • pi
  • piface_digital_2
  • piface
Related
Recommended

SCPI on a Linux Board - Part 2a: PiFace Digital C programming

Jan Cumps
Jan Cumps
16 Jun 2018

I'm building a SCPI device for Linux.

I have the basis working over TCP/IP.

This morning I received a PiFace Digital 2PiFace Digital 2 from element14 (thank you!)

This board, with digital inputs, outputs, relays and LEDs can be a nice LAB automation utility.

 

image

In this post I check if I can control the PiFace Digital 2 via C.

TL;DR yes

 

In this series, I'm focusing on the specifics for TCP/IP communication with a SCPI service.

In the previous posts I made socket server that listens for SCPI commands and parses/handles them.

This is the first post where I talk to hardware. In a later post I'll link the SCPI server and the hardware together.

 

PiFace Digital 2

 

This Pi hat is a port expander that gives you 8 digital inputs and 8 outputs, 4 buttons, 2 relays and 8 LEDs that you can control from your Pi.

Communication goes via SPI.

To get the basics working, check out this great blog from urkraft: PiFace Digital 2 - setup and use

I'm using Ubuntu on my Pi, so I had to install the raspi-config utility first before I could use it to enable SPI.

 

Control the PiFace Digital 2 with C

 

That was easy too. Piface has example code on their github.

You need the c and h files from these two repositories:

libpifacedigital

libmcp23s17

 

Both come with a makefile and you can build them right away on your Pi.

I'm developing on a windows computer and cross-compile for Linux, so I've created a project in the ARM DS-5 IDE.

image

This allows me to interactively debug the program from the windows PC.

As you can see on the photo at the start of the blog post, I was able to control a LED. I've also tested a relay.

 

Here's an action shot of the debug session:

image

 

In the next post I'll try to turn this into some server code that listens to commands and executes any requests.

That's the next step to get a SCPI programmable LAB controller on the Pi.

 

 

 

related blog
SCPI on a Linux Board - Letter of Intent

SCPI on a Linux Board - Part 1: Proof of Concept

SCPI on a Linux Board - Part 2a: PiFace Digital C programming

SCPI on a Linux Board - Part 2b: PiFace Digital C++ programming
SCPI on a Linux Board - Part 3: TCP/IP Socket C++ programming
SCPI on a Linux Board - Part 4: TCP/IP SCPI and Instrument Service
SCPI on a Linux Board - Part 4b: TCP/IP SCPI and Instrument Service 100% Working
SCPI on a Linux Board - Part 4c: TCP/IP SCPI and Instrument Service - Run as a Daemon
SCPI on a Linux Board - Part 5a: LabVIEW Driver for LAB Switch: Open, Close and Switch functions
  • Sign in to reply

Top Comments

  • jomoenginer
    jomoenginer over 8 years ago +2
    Very cool. At my day gig, we have a ton of automated tests that include sending SCPI and GPIB/HPIB over multiple protocols such as Ethernet, USB and Serial on Windows, Linux and Solaris but mainly with…
  • DAB
    DAB over 8 years ago +1
    Good post Jan. DAB
Parents
  • jomoenginer
    jomoenginer over 8 years ago

    Very cool. At my day gig, we have a ton of automated tests that include sending SCPI and GPIB/HPIB over multiple protocols such as Ethernet, USB and Serial on Windows, Linux and Solaris but mainly with Python.  This series has looked like an interesting implementation.     

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • jomoenginer
    jomoenginer over 8 years ago

    Very cool. At my day gig, we have a ton of automated tests that include sending SCPI and GPIB/HPIB over multiple protocols such as Ethernet, USB and Serial on Windows, Linux and Solaris but mainly with Python.  This series has looked like an interesting implementation.