Test & Tools
  • Technologies
  • More
Test & Tools
Documents Programmable Electronic Load - Analyse the Summing Node Zero Point
  • Blog
  • Forum
  • Documents
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Test & Tools to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Engagement
  • Author Author: Jan Cumps
  • Date Created: 1 Dec 2017 4:08 PM Date Created
  • Last Updated Last Updated: 15 May 2020 3:38 PM
  • Views 12858 views
  • Likes 8 likes
  • Comments 107 comments
Related
Recommended

Programmable Electronic Load - Analyse the Summing Node Zero Point

This blog documents investigates the feedback node of the electronic load that Robert Peter Oakes, jc2048 and Jan Cumps are designing.

It's an important spot in the load's design. It measures the set point and the feedback from the output.

When the output is driven to 0, it should be on a potential as close as possible to 0 V.

On the first prototype it's -0.2 V. Not so much off, but the negative value  influences our ADC measurements.

This document checks how we can get this node to 0 V.

image

 

Because this document is evolving, some comments below may be out of sync with the content. That's because the content is adapted based on the conversation.

The measurements taken here are based on the original design, without R32 in place and U3B + tied to ground.

The current sense side of R7 is connected to ground, and a variable negative voltage from 0 V down is applied to the current sense side of R8 to simulate current being sensed.

 

The circuit isn't complex. The set point is driven by a DAC. It's set to 0 for this test.

The second input to this node is OpAmp 3C. It has both inputs tied to ground so should theoretically have 0 V at the output.

On my board I measure a potential of -0.212V at the left side of R33.

I hope to get this closer to 0 V to ease the ADC a bit - its performance degrades with negative voltage at its inputs.

Like the other blogs for the electronic load, this is a working document that will be updated with findings from anyone who wants to chime in.

 

Behaviour at 0V

 

buzy image

  • metrology
  • differentiator
  • boosterpack
  • opamp
  • msp432
  • launchpad
  • analog
  • laboratory
  • instrument
  • Share
  • History
  • More
  • Cancel
  • Sign in to reply

Top Comments

  • jc2048
    jc2048 over 8 years ago in reply to Robert Peter Oakes +4
    As you say, changing the op-amp is one possibility. There are bipolar op-amps with much lower bias currents, but an alternative nowadays is a precision CMOS op-amp (you'd have to check whether other characteristics…
  • Robert Peter Oakes
    Robert Peter Oakes over 8 years ago +3
    To hopefully simplify things a little We have this, Upper op amp is simply to provide an inversion of the measured value back tot he ADC, hence the gain of -1 Lower right op amp measures the volts across…
  • jc2048
    jc2048 over 8 years ago in reply to Jan Cumps +3
    Love the advertisement for "John's excellent probes". It's like one those things from the old days of American TV where the presenter would suddenly turn, look very earnestly at the camera, and start reading…
Parents
  • Jan Cumps
    Jan Cumps over 8 years ago

    I'm going to redo this exercise now that the OpAmps are replaced with lower bias ones and I have more precise measurement tools.

    From the blog Programmable Electronic Load - LabVIEW Test Automation: Characterise the Instrument we can see that the behaviour is very linear.

    But we have a non-0 start point. When th DAC is driven to 0, there is an output current flowing of a few mA.

    image

    I assume that it's our control circuit that's doing that, because if I disable the output (pull the gate to ground), the current that flows is neglectable. And it's the same FET that's fully blocking the current flow then.

     

    I've re-stacked the load so that the control board is on top and I have easier access to the measure point.

    I can't use the LCD display in that case. I'll use the SCPI interface to set values.

    image

     

    I'll measure DAC output and the voltages at relevant control circuit points to see what drives the FET to conduct a little.

    I think I'll document the results in new blog post. We can then think on measures to get the lowest current lower than 2 mA.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • Jan Cumps
    Jan Cumps over 8 years ago in reply to Jan Cumps

    I've been checking for a while and get 0.6 µA when measuring with a multimeter. I usd a fairly high input voltage of 14 V to compensate for any cable resistance.

     

    image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • Jan Cumps
    Jan Cumps over 8 years ago in reply to Jan Cumps

    When I shortcut the DAC1 output, I get almost the same as when the output is off. So it seems that the offset is caused by offset of the DAC.

    image

     

    When driving the DAC to 0, I get 0.731 mV output. The measured voltage over the sensor resistor is then 0.054 mV.

    If I shortcut DAC A, I measure 0.005 mV over the 0R05 sense resistor. That's virtually the same as INPUT OFF (0.003 mV).

     

    I'll have to check if I can deal with the positive DAC offset ...

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • Jan Cumps
    Jan Cumps over 8 years ago in reply to Jan Cumps

    When I remove everything from the DAC, the offset voltage is 0.529 mV.

    image

    Same as when the eload is connected, the ADC DAC only starts to ramp up from that offset once the DAC value is close to 100.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • Jan Cumps
    Jan Cumps over 6 years ago in reply to Jan Cumps

    Jan Cumps  wrote:

     

    Pushing the offset higher doesn't solve the issue. It just pushes it uphill.

    In this graph, I set DAC B, that creates the offset correction, to 300.

     

    image

    Behaviour is the same, a steep jump from nothing to > 2 mA, but at a higher starting point of DAC A.

     

     

    1840,00051850,00251860,00251870,00261880,00281890,00291900,003

     

    (are we fighting against the diodes at the backside of the integrator?)

    The conclusion may be premature, but the cause for the bump seems to be the offset in the current sense opamp.

    When working that offset in the U3C away to under 200 µV, I get nicer behaviour when the regulation circuit starts.

    image

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • Jan Cumps
    Jan Cumps over 8 years ago in reply to Jan Cumps

    image

     

    Here's a long running sample. 5400+ samples. Ignore the blip at 2400 because that's when I paused the test to go out with my youngest daughter. I don't want to burn my house.

    It's still running. I'll stop it when I close for the night (bloody early flight, need to be up at 4:00 image ).

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • jc2048
    jc2048 over 8 years ago in reply to Jan Cumps

    For a comparatively simple circuit, it's been a very good vehicle for blogging. I'm learning a lot from it, though I think it will be a while before you give me my diploma in servo systems (I never was any good at maths, and I'm certainly not now).

     

    One worry I have about those blogs you refer to is that I'm not an expert in this. All the simple project stuff [I'm thinking about Arduino stuff here] doesn't matter too much (it's just fluff, though it's fun and serves a useful purpose in getting people interested and acts as a way of introducing concepts), but those blogs were moving into the area of theory, but theory that I'm not qualified to teach. I think, on balance, it's worth doing this stuff (as much because it gives an idea of how electronic design is done and how you think about things and solve problems as the actual detail of what you're blogging about), but I often think that there are lots of people out there who could do it so much better than I could.

     

    To extend the range down you just need a higher value sense resistor (though you obviously lose the top end). A 5R sense resistor should get you down a couple more decades. You might need to swap the MOSFET (though it would be an interesting experiment to try the 5R in the existing circuit and see what happens with the MOSFET if you take the drain current down further). That then leads to the idea you could switch the load resistors into circuit, but that falls on the difficulty that anything you use as a switch has a significant resistance compared to the 50mOhm. Another possibility would be the two resistors in series, with a relay to short out the 5R for higher currents, but you'd need two sense circuits and some way to switch between them.

     

    A further idea, if the current when forced off is very low, is two parallel two circuits with either being allowed to operate - a high current one and a low current one. You might even be able to arrange for both to be operating together, though I suspect the loop stuff gets a bit hairy if you do that. [One thing to watch, though, is that the clever scheme of shifting the ground point to the source of the MOSFET rather than the negative load connection would compromise that.]

     

    I've got a much, much lower cost design using transistors (a completely op-amp free zone!) - I did that a while back as a challenge to myself to see if I could design something more complex than a textbook circuit. I haven't prototyped it yet but it works ok in the simulator. (I'm a bit slow in my old age - it was only after I'd started it that I realised I was actually designing a discrete op amp, though it does differ a bit from the traditional do-anything op-amp design). It's nothing like the precision of this one and it's not a true servo system, but it's much faster. Component cost would be a few pounds. I'm saving it for the next DIY Test Equipment contest.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • Jan Cumps
    Jan Cumps over 8 years ago in reply to jc2048

    jc2048  wrote:

     

    ...

    It doesn't matter to you because the loop seems to be dealing with it quite happily.

     

    ...

    Yes, it's impressive that the control mechanism gets such a good grip on the current with the MOSFET being a tough device to control in this range of operation.

     

    ...

     

    But do you actually need the load to be able to do this? Do you need the load to operate continuously over more than 4 decades of current?

    ....

     

    No. My main goal was to see if I could turn Peter's design into a programmable one. I started from that point, with no other goals.

    It's certainly not a perfect exercise.  I learned and re-learned a lot while doing this (I'm expected to be a diploma'd control mechanism guy but I needed loads of studying to get hold of the theory and practice again - this exercise bumped me back into the stratosphere of control theory image ). And I'm pleased that it yielded those blog posts you made that explain the behaviour of the control part.

     

    I think this instrument as it stands now is useful in its operating range. Mine is fairly stable and linear between 2 mA and 6 A for the control part. The measurement part I have only roughly tamed. It needs more work before we can see how well that behaves.

     

    Maybe, because everything is published, there is a chance that someone improves on it. Maybe by increasing range and precision. Or by reducing the costs by factoring out some of the ridiculously expensive components I used ... (and improving the PCB design)

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • Jan Cumps
    Jan Cumps over 8 years ago in reply to jc2048

    jc2048  wrote:

     

    ...

    It doesn't matter to you because the loop seems to be dealing with it quite happily.

     

    ...

    Yes, it's impressive that the control mechanism gets such a good grip on the current with the MOSFET being a tough device to control in this range of operation.

     

    ...

     

    But do you actually need the load to be able to do this? Do you need the load to operate continuously over more than 4 decades of current?

    ....

     

    No. My main goal was to see if I could turn Peter's design into a programmable one. I started from that point, with no other goals.

    It's certainly not a perfect exercise.  I learned and re-learned a lot while doing this (I'm expected to be a diploma'd control mechanism guy but I needed loads of studying to get hold of the theory and practice again - this exercise bumped me back into the stratosphere of control theory image ). And I'm pleased that it yielded those blog posts you made that explain the behaviour of the control part.

     

    I think this instrument as it stands now is useful in its operating range. Mine is fairly stable and linear between 2 mA and 6 A for the control part. The measurement part I have only roughly tamed. It needs more work before we can see how well that behaves.

     

    Maybe, because everything is published, there is a chance that someone improves on it. Maybe by increasing range and precision. Or by reducing the costs by factoring out some of the ridiculously expensive components I used ... (and improving the PCB design)

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
Children
  • jc2048
    jc2048 over 8 years ago in reply to Jan Cumps

    For a comparatively simple circuit, it's been a very good vehicle for blogging. I'm learning a lot from it, though I think it will be a while before you give me my diploma in servo systems (I never was any good at maths, and I'm certainly not now).

     

    One worry I have about those blogs you refer to is that I'm not an expert in this. All the simple project stuff [I'm thinking about Arduino stuff here] doesn't matter too much (it's just fluff, though it's fun and serves a useful purpose in getting people interested and acts as a way of introducing concepts), but those blogs were moving into the area of theory, but theory that I'm not qualified to teach. I think, on balance, it's worth doing this stuff (as much because it gives an idea of how electronic design is done and how you think about things and solve problems as the actual detail of what you're blogging about), but I often think that there are lots of people out there who could do it so much better than I could.

     

    To extend the range down you just need a higher value sense resistor (though you obviously lose the top end). A 5R sense resistor should get you down a couple more decades. You might need to swap the MOSFET (though it would be an interesting experiment to try the 5R in the existing circuit and see what happens with the MOSFET if you take the drain current down further). That then leads to the idea you could switch the load resistors into circuit, but that falls on the difficulty that anything you use as a switch has a significant resistance compared to the 50mOhm. Another possibility would be the two resistors in series, with a relay to short out the 5R for higher currents, but you'd need two sense circuits and some way to switch between them.

     

    A further idea, if the current when forced off is very low, is two parallel two circuits with either being allowed to operate - a high current one and a low current one. You might even be able to arrange for both to be operating together, though I suspect the loop stuff gets a bit hairy if you do that. [One thing to watch, though, is that the clever scheme of shifting the ground point to the source of the MOSFET rather than the negative load connection would compromise that.]

     

    I've got a much, much lower cost design using transistors (a completely op-amp free zone!) - I did that a while back as a challenge to myself to see if I could design something more complex than a textbook circuit. I haven't prototyped it yet but it works ok in the simulator. (I'm a bit slow in my old age - it was only after I'd started it that I realised I was actually designing a discrete op amp, though it does differ a bit from the traditional do-anything op-amp design). It's nothing like the precision of this one and it's not a true servo system, but it's much faster. Component cost would be a few pounds. I'm saving it for the next DIY Test Equipment contest.