1 Meter of Pi
  • Challenges & Projects
  • Design Challenges
  • 1 Meter of Pi
  • More
  • Cancel
1 Meter of Pi
Blog Gr0G - 01 - Introduction
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
  • Author Author: amgalbu
  • Date Created: 18 Oct 2020 11:32 AM Date Created
  • Views 1067 views
  • Likes 4 likes
  • Comments 3 comments
  • 1meterofpi
  • gr0g
  • 1meter of pi
Related
Recommended

Gr0G - 01 - Introduction

amgalbu
amgalbu
18 Oct 2020

Here is a list of the posts in this challenge

Gr0G - 01 - Introduction

Gr0G - 02 - Why aeroponics?

Gr0G - 03 - High-pressure system design

Gr0G - 04 - Mechanical design

Gr0G - 05 - Electrical design

Gr0G - 06 - Building the box

Gr0G - 07 - Playing with the Gertbot

Gr0G - 08 - Installing LEDs

Gr0G - 09 - The control board

Gr0G - 10 - Software design

Gr0G - 11 - Building the box (2)

Gr0G - 12 - Building the high-pressure system

Gr0G - 13 - Building the high-pressure system (2)

Gr0G - 14 - Piping

Gr0G - 15 - Improvements

Gr0G - 16 - Remote UI

Gr0G - 17 - Remote UI (2)

Gr0G - 18 - Conclusions

 

Source code available at https://github.com/ambrogio-galbusera/gr0g, https://github.com/ambrogio-galbusera/gr0g-ble-android and https://github.com/ambrogio-galbusera/gr0g-ble

Introduction

Growing crops in microgravity is in many way different from farming on earth. In particular, the challenges of growing plants is space are

  • Space is an important resource on a spaceship, so it must be exploited to the utmost. However, in a microgravity environment, there is also a big opportunity in that there is no up or down: plants simply grow towards the light
  • Plants are exposed to stresses like hypoxia and oxidation due to poor soil aeration
  • At your destination site, there are no resources, so everything on the starship should be reusable

 

Proposed project

The proposed project for this project is to build a growing box that tries to solve the above-mentioned challenges. In particular

  • seed are planted on all the six internal faces of the cubs
  • an aeroponic system will be devised to overcome all the issues related to the presence of soil

The overall structure of the growing box is shown in picture below

image

 

All the six internal faces of the cube are equipped with housing for plants. Seed will be implanted in rockwool

At destination, the cube will be opened to provide fertile soil for the colony

 

image

Project plan

Research

  • The problems related to building an aeroponic system will be researched
  • The best accomodation for all required components will be investigated

 

System design

  • Block diagram
  • Mechanical design
  • Piping
  • Software design

System Build

  • Electronics build, Mechanical Build, Software programming

Developmental Testing

  • System electrical testing, System software testing, System mechanical testing

System Application Tests

  • The system will be tested and lattuce will be cultivated

Documentation & Conclusions

  • Each of the project plan tasks will include a related blog
  • Sign in to reply

Top Comments

  • amgalbu
    amgalbu over 5 years ago in reply to ralphjy +1
    Yes, thanks: it's aeroponic but nevertheless I will include "creating a new music genre" in the project goals
Parents
  • DAB
    DAB over 5 years ago

    Nice update.

     

    DAB

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • DAB
    DAB over 5 years ago

    Nice update.

     

    DAB