1 Meter of Pi
  • Challenges & Projects
  • Design Challenges
  • 1 Meter of Pi
  • More
  • Cancel
1 Meter of Pi
Blog Gr0G - 04 - Mechanical design
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
  • Author Author: amgalbu
  • Date Created: 25 Oct 2020 6:13 AM Date Created
  • Views 1215 views
  • Likes 3 likes
  • Comments 4 comments
  • 1meterofpi
  • gr0g
  • 1meter of pi
Related
Recommended

Gr0G - 04 - Mechanical design

amgalbu
amgalbu
25 Oct 2020

Here is a list of the posts in this challenge

Gr0G - 01 - Introduction

Gr0G - 02 - Why aeroponics?

Gr0G - 03 - High-pressure system design

Gr0G - 04 - Mechanical design

Gr0G - 05 - Electrical design

Gr0G - 06 - Building the box

Gr0G - 07 - Playing with the Gertbot

Gr0G - 08 - Installing LEDs

Gr0G - 09 - The control board

Gr0G - 10 - Software design

Gr0G - 11 - Building the box (2)

Gr0G - 12 - Building the high-pressure system

Gr0G - 13 - Building the high-pressure system (2)

Gr0G - 14 - Piping

Gr0G - 15 - Improvements

Gr0G - 16 - Remote UI

Gr0G - 17 - Remote UI (2)

Gr0G - 18 - Conclusions

 

Source code available at https://github.com/ambrogio-galbusera/gr0g, https://github.com/ambrogio-galbusera/gr0g-ble-android and https://github.com/ambrogio-galbusera/gr0g-ble

 

In this post, I will give some sketches of Gr0G box from a mechanical point of view.

The structure will be built with aluminum extrusion. I found some bars designed to house LED strips (see picture). These bars will made up the top and bottom panels of the cube.

image

image

 

The four lateral panels will be made up with a bar for the LED strip, two L-shaped aluminum extrusion (at the top and the bottom) and a 20 x 1 mm aluminum bar.

 

imageimage

image

This is the detail of the junction between two adjacent lateral panels

 

image

 

The four lateral panels are joined to the bottom panel by means of a joint to allow the box t be folded and unfolded. The top panel will be joined to one of the lateral panels in the same way

 

image

 

The aluminum bars will be riveted

 

The structure will be covered with transparent Plexiglas panels. Lateral and top panels will be covered with 2mm panels, the bottom with a 4 mm one, in order to hold up the compressor and the other pneumatic components. Plexiglas panels will be kept in place by tapping screws

  • Sign in to reply

Top Comments

  • amgalbu
    amgalbu over 5 years ago in reply to dougw +3
    Hello Douglas I found the aluminum estrusion and the plexiglas panels at a warehouse close to me and I spent about 25 euros. Regarding the bars for LED, there any many offers on the Internet and I think…
  • dougw
    dougw over 5 years ago +1
    Wow, top notch materials - with a price to match, no doubt.
Parents
  • genebren
    genebren over 5 years ago

    Looks like a solid plan and enclosure.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • genebren
    genebren over 5 years ago

    Looks like a solid plan and enclosure.