1 Meter of Pi
  • Challenges & Projects
  • Design Challenges
  • 1 Meter of Pi
  • More
  • Cancel
1 Meter of Pi
Blog Gr0G - 09 - The control board
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
  • Author Author: amgalbu
  • Date Created: 12 Nov 2020 7:34 PM Date Created
  • Views 1910 views
  • Likes 3 likes
  • Comments 10 comments
  • 1meterofpi
  • gr0g
  • 1meter of pi
Related
Recommended

Gr0G - 09 - The control board

amgalbu
amgalbu
12 Nov 2020

Here is a list of the posts in this challenge

Gr0G - 01 - Introduction

Gr0G - 02 - Why aeroponics?

Gr0G - 03 - High-pressure system design

Gr0G - 04 - Mechanical design

Gr0G - 05 - Electrical design

Gr0G - 06 - Building the box

Gr0G - 07 - Playing with the Gertbot

Gr0G - 08 - Installing LEDs

Gr0G - 09 - The control board

Gr0G - 10 - Software design

Gr0G - 11 - Building the box (2)

Gr0G - 12 - Building the high-pressure system

Gr0G - 13 - Building the high-pressure system (2)

Gr0G - 14 - Piping

Gr0G - 15 - Improvements

Gr0G - 16 - Remote UI

Gr0G - 17 - Remote UI (2)

Gr0G - 18 - Conclusions

 

Source code available at https://github.com/ambrogio-galbusera/gr0g, https://github.com/ambrogio-galbusera/gr0g-ble-android and https://github.com/ambrogio-galbusera/gr0g-ble

 

Let's now start to build the control board. This is the electrical circuit we are going to build (it's a bit difficult to read, but the original Fritzing file is attached)

image

Some notes about this diagram

  • The control board takes a 12V dc power supply. It converts the 12V dc to 5V dc through a 7805. Since the output of a 7805 is not very "clean" (it has ripple and spikes that may cause damages to the Raspberry Pi and the other boards), I choose to connect the 7805 output to the USB connector of the Raspberry Pi. The USB connector has a Zener to eliminate spikes and some circuitry to level the ripple. Then the 5V and 3.3V to power up external boards is taken from the 40-pin header connector
  • Raspberry Pi absorbs a lot of current (up to 2A), so the 7805 is going to get very hot
  • The Keypad connector uses four GPIOs to read the status of keys to allow the user to navigate through the screens shown on the display of the PiMoroni Automation Hat. I could have connected the keypad to the PiMoroni Automation Hat inputs, but
    • PiMoroni Automation Hat has just three inputs (I need four inputs)
    • The library provided to control the PiMoroni Automation Hat tries to access the I2C bus as soon as you initialize the library itself, but I am going to use the sensors on the Enviro Hat
    • The PiMoroni Automation Hat inputs are connected directly to the Raspberry Pi GPIO pins

        For all these reasons, it's not so bad to connect keypad directly to the Raspberry Pi

  • The Automation Hat connector takes the SPI signals plus a GPIO (to control display backlight) and power supply (both 3.3V and 5V). The SPI bus is required to control the PiMoroni Automation Hat display. This display will be mounted on one of the vertical panels of the Gr0G box to show astronauts information about the status of the box
  • The Enviro Hat connector takes the I2C signals and power supply (both 3.3V and 5V). The I2C is required to access hat's sensors. The hat will be mounted on a bracket. The display on the EnviroHat will not be used
  • The Gertbot board requires an UART to be commanded and controlled. The power section will be connected to the 12V dc (for fan, condenser, and solenoid valve) and 5V (for LEDs)

 

The Raspberry Pi, the Gertbot board, the PiMoroni Automation Hat will be mounted on a plywood board

 

imageimage

The boards have been then put in place. First, the Raspberry Pi

image

Then, the PiMoroni Hacker board with the connectors for the external boards

image

Finally, the Gertbot board

image

Then, the PiMoroni Automation Hat board has been installed on the front side of the plywood panel

image

 

UPDATE:

PWM output can not handle the current required by both the dehumidifier (fans + Peltier cell) and cooler. So I disconnected the Peltier cell from the PWM output pins and now I am going to switch on and off the cell itself by means of opendrain output 1. Since opendrain output are rated for 5A maximum (and the Peltier cell draws 6A) I used the opendrain output to drive a relay, and the relay NO pin will then be connected to the Peltier cell. The new diagram in shown in picture

image

  • Sign in to reply

Top Comments

  • balearicdynamics
    balearicdynamics over 5 years ago in reply to amgalbu +2
    Just FYI, if the board of Pimoroni is a real HAT – I mean, following the Pi HAT specifications – it should be identified by an EEPROM encoded in a specific way accessed by the I2C 0. This is just to make…
  • amgalbu
    amgalbu over 5 years ago in reply to balearicdynamics +2
    Yes Enrico I think it's possible to use two display by using two GPIOs as CSes for the two displays I didn't investigate this option but I think it's not too difficult but for sure this does not make possible…
  • dules
    dules over 5 years ago in reply to balearicdynamics +2
    You can check my solution for this problem here: Aquaponics Box: #2 - Hacking the HATs (both HATs from the challenger kit on single RPi)
Parents
  • DAB
    DAB over 5 years ago

    I would add a heat sink to the 7805. They tend to fail if they get too hot.

     

    DAB

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • DAB
    DAB over 5 years ago

    I would add a heat sink to the 7805. They tend to fail if they get too hot.

     

    DAB

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Children
  • amgalbu
    amgalbu over 5 years ago in reply to DAB

    Thank you DAB

    I will do... the raspberry pi 4 draws 3.4 watts.

    That's a lot of current and the 7805 is going to get very hot