Design for a Cause - Design Challenge
  • Challenges & Projects
  • Design Challenges
  • Design for a Cause - Design Challenge
  • More
  • Cancel
Design for a Cause - Design Challenge
Blog Audio4Vision #12 - Putting it all together, wrap up and thanks!
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
  • Author Author: pranjalranjan299
  • Date Created: 15 Sep 2018 3:52 AM Date Created
  • Views 2654 views
  • Likes 6 likes
  • Comments 10 comments
Related
Recommended

Audio4Vision #12 - Putting it all together, wrap up and thanks!

pranjalranjan299
pranjalranjan299
15 Sep 2018

Hi! Welcome to our 12th blog post. This would be the final blog post, which will talk about putting it all together to form a harmonious system.

 

The whole idea behind making this project (and this challenge) was to create an idea which would have some real-world weight for people less fortunate than us. We wanted to build a project which was capable of bringing at least a tiny bit of convenience for those people, and today we're proud to say that we've reached to the end with a device that can do that.

The world is full of so many visually appealing scenes and events. It's a shame that some people are blocked out from this beauty of nature, for no fault of their own. While our device may not come close to fully convey the elegant nature of visual reality to these people, we think this is one small step in the right direction.

 

Two months ago, we published our 1st blog post. We had an idea planned out then, which was this:

image

 

Today, we're happy that this system has finally come to fruition. The device, centered around the powerful MKR1000, is small, lightweight and user-friendly. All the user has to do is connect it to a portable power source, and it will automatically start periodically describing the surroundings to the person.

The following block diagram is a bit more refined, and captures the working rather nicely:

image

 

Here's the list of components that went into this project:

Components

Cost (USD)
Arduino MKR100034.99
ArduCAM Mini OV2640 2MP25.99
PAM 8403 Amplifier1.00

Speaker (4 Ohms, 3 Watts)

3.00
SD Card and SD Proto Shield
Total64.98

 

The server code was written in Python 3.6.2, using the Flask web microframework. The model used for captioning was the Show and Tell model. Audio files were generated from the captions using a TTS library.

The Arduino sketches were naturally written, compiled and uploaded via the Arduino IDE.

 

Final connection diagram -

 

image

 

Here's the finished prototype:

image

 

Our plans for the future are to:

  1. Remove breadboard dependency, make it low-profile
  2. Shift to earphones (Speaker is just for demonstration purpose, can be replaced with earphones)

 

Here's a little video we made of our creation in action, it was a bit tough to get more samples from outside but it works in the same way as shown in earlier samples. All you have to do is take pictures from the camera and the .wav file of its captions are produced in the same way.

 

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

 

The image that it works on -

image

 

This is how it looks on the serial monitor -

 

image

image

For other examples like -

image

The audio produced is -

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

Now for this image,

image

The generated audio caption for this image is -

 

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

 

This is our Arduino sketch (which took only 20% of the MKR's memory):

 

#include <SPI.h>
#include <WiFi101.h>
#include<SD.h>
#include <ArduCAM.h>
#include <Wire.h>
#include <AudioZero.h>
#include "memorysaver.h"


int n=1;
File myFile;
File theFile;
//#include "arduino_secrets.h"


boolean currentLineIsBlank = true;
#define SD_CS 4
const int SPI_CS = 0;
ArduCAM myCAM( OV2640, SPI_CS );
char ssid[]="MTNL_094550_1";
char pass[]="pranjal299";
int keyIndex=0;
WiFiClient client;


int status=WL_IDLE_STATUS;
WiFiServer server(80);


void setup() {
  Serial.begin(115200);
  while (!Serial) {
    ; // wait for serial port to connect. Needed for native USB port only
  }
  Serial.print("Initializing SD card...");


  if (!SD.begin(4)) {
    Serial.println("initialization failed!");
    //return;
  }
  Serial.println("initialization done.");


  if(WiFi.status()==WL_NO_SHIELD) {
    Serial.println("WiFi shield not present");
    while(true);
  }


  while(status!=WL_CONNECTED) {
    Serial.print("Attempting to connect to Network named: ");
    Serial.println(ssid);


    status=WiFi.begin(ssid,pass);
    delay(3000);
  }
  server.begin();
  cam_setup();
  Serial.println("");
  Serial.println("");
}


void img_POST() {
  Serial.begin(115200);
  while (!Serial) {
      ; // wait for serial port to connect. Needed for native USB port only
   }
  Serial.println("");
  //Load Normal Picture
  while (SD.begin(4));
  String normalFilename = String(n)+".JPG";
  File normPicture = SD.open(normalFilename);


  // Get the size of the image (frame) taken
  while (!normPicture.available());
  long jpglen = normPicture.size();
  Serial.println("Sending "+String(n)+"th image of");
  Serial.print(jpglen, DEC);
  Serial.println(" bytes");


  // Prepare request
  String start_request = "";
  String end_request = "";
  start_request = start_request + "\n" + "--AaB03x" + "\n" + "Content-Type: image/jpeg" + "\n" + "Content-Disposition: form-data; name=\"file\"; filename=\"" + normalFilename + "\"" + "\n" + "Content-Transfer-Encoding: binary" + "\n" + "\n";
  end_request = end_request + "\n" + "--AaB03x--" + "\n";
  long extra_length;
  extra_length = start_request.length() + end_request.length();
  //Serial.println("Extra length:");
  //Serial.println(extra_length);
  long len = jpglen + extra_length;
  
  //Serial.println(start_request);
  Serial.println("Starting connection to server...");
  char flask_hostname[]="192.168.1.109";
  // Connect to the server, please change your IP address !
  if (client.connect(flask_hostname, 5000)) {
    Serial.println("Connected");
    client.print("POST ");
    client.print("/");
    client.println(" HTTP/1.1");
    client.println("Host: " + String(flask_hostname));
    client.println("Content-Type: multipart/form-data; boundary=AaB03x");
    client.print("Content-Length: ");
    client.println(len);
    client.print(start_request);
    //Serial.println("Connected1");


    if (normPicture) {
      //Serial.println("Connected2");
      int count = 0;
      byte clientBuf[128];
      int clientCount = 0;


      while (normPicture.available()) {
        clientBuf[clientCount] = normPicture.read();
        clientCount++;
        count++;


        if (clientCount > 127) {
          //Serial.println(".");
          client.write(clientBuf, 128);
          clientCount = 0;
        }
      }
      if (clientCount > 0) client.write(clientBuf, clientCount);
      Serial.println(String(count));
      normPicture.close();
    }
    //Serial.println("Connected3");
    client.print(end_request);
    client.println();


    Serial.println("Transmission over");
  }
  else {
    Serial.println("Connection failed");
  }
  char sentence[100];
  Serial.println("HEARING STARTS");
  Serial.println("Sentence "+String(n)+" is ");
  while (client.connected()) {
    int flag=0;
    int i=0;
    while (client.available()) {
      // Read answer
      char c = client.read();
      if(c=='$')
      {
        flag=flag+1;
        //Serial.println(flag);
        //Serial.println(c);
        continue;
      }
      if(flag==1)
      {
        Serial.print(c);
        //sentence[i]=c;
        //i=i+1;
        //Serial.print(c);
      }
      //Serial.print(c);
    }
  }
  //Serial.println("Sentence "+String(n)+" is ");
  //Serial.println(sentence);
  Serial.println("");
  Serial.println("HEARING ENDS");
  delay(100);
  client.stop();
  //while(true);
}


void wav_GET()
{ Serial.println("");
  Serial.println("Starting connection to server...");
  char flask_hostname[]="192.168.1.109";
  // Connect to the server, please change your IP address !
  if (client.connect(flask_hostname, 5000)) {
    Serial.println("hello");
    client.println("GET /output"+String(n)+".wav HTTP/1.1");  // change resource to get here
    client.println("Host: 192.168.1.109");                 // change resource host here
    client.println("Connection: close");
    client.println();}
  else{
    Serial.println("Connection failed");
  }
  Serial.println("Creating file.");
  theFile = SD.open("output"+String(n)+".wav", FILE_WRITE);  // change file name to write to here
  if (!theFile) {
    Serial.println("Could not create file");
    while (1);
  }
  Serial.println("Created");
  int x=1;
  Serial.println("Loop starts");
  while(x!=0)
  {
    if (client.available()) {
    char c = client.read();
    //Serial.println("Available");
    if (c == '\n' && currentLineIsBlank) {
      // end of HTTP header, now save requested file
      while (client.connected()) {
        // stay in this loop until the file has been received
        if (client.available()) {
          c = client.read();  // get file byte
          theFile.print(c);   // save file byte
          //Serial.println("reading");
        }
      }
    }
    // detect the end of the incoming HTTP header
    if (c == '\n') {
      // starting a new line
      currentLineIsBlank = true;
    }
    else if (c != '\r') {
      // got a character on the current line
      currentLineIsBlank = false;
    }
  }


  // if the server's disconnected, stop the client:
  if (!client.connected()) {
    Serial.println();
    Serial.println("disconnecting.");
    client.stop();
    theFile.close();
    Serial.println("Finished writing to file");
    
    // do nothing forevermore:
    //while (true);
    x=0;
  }
  }
  Serial.println("loop ends");
}


void loop() {
   for(int i=1;i<6;i++)
   {
    cam_2_SD();
    delay(200);
    img_POST();
    delay(200);
    wav_GET();
    delay(200);
    play_WAV();
    n=n+1;
    delay(1000);
   }
   while(true);
}


void cam_setup()
{
  uint8_t vid, pid;
  uint8_t temp;
  Wire.begin();
  Serial.begin(9600);
  while (!Serial) {
      ; // wait for serial port to connect. Needed for native USB port only
   }
  Serial.println(F("ArduCAM Start!"));
  //set the CS as an output:
  pinMode(SPI_CS,OUTPUT);
  digitalWrite(SPI_CS, HIGH);
  // initialize SPI:
  SPI.begin();
  //delay(2000);
  //Reset the CPLD
  myCAM.write_reg(0x07, 0x80);
  delay(100);
  myCAM.write_reg(0x07, 0x00);
  delay(100);
  
  while(1){
    //Check if the ArduCAM SPI bus is OK
    myCAM.write_reg(ARDUCHIP_TEST1, 0x55);
    temp = myCAM.read_reg(ARDUCHIP_TEST1);
  
    if (temp != 0x55){
      Serial.println(F("SPI interface Error!"));
      delay(1000);continue;
    }
    else{
      Serial.println(F("SPI interface OK."));break;
    }
  }
  while(1){
    //Check if the camera module type is OV2640
    myCAM.wrSensorReg8_8(0xff, 0x01);
    myCAM.rdSensorReg8_8(OV2640_CHIPID_HIGH, &vid);
    myCAM.rdSensorReg8_8(OV2640_CHIPID_LOW, &pid);
    if ((vid != 0x26 ) && (( pid != 0x41 ) || ( pid != 0x42 ))){
      Serial.println(F("Can't find OV2640 module!"));
      delay(1000);continue;
    }
    else{
      Serial.println(F("OV2640 detected."));break;
    } 
  }
  myCAM.set_format(JPEG);
  myCAM.InitCAM();
  myCAM.OV2640_set_JPEG_size(OV2640_1024x768);
  delay(1000);
}


void cam_2_SD(){
  Serial.println("");
  Serial.println("");
  Serial.println("IMAGE NO. "+String(n));
  char str[8];
  byte buf[256];
  static int i = 0;
  static int k = 0;
  uint8_t temp = 0,temp_last=0;
  uint32_t length = 0;
  bool is_header = false;
  File outFile;
  //Flush the FIFO
  myCAM.flush_fifo();
  //Clear the capture done flag
  myCAM.clear_fifo_flag();
  //Start capture
  myCAM.start_capture();
  Serial.println(("Start Capture"));
  while(!myCAM.get_bit(ARDUCHIP_TRIG , CAP_DONE_MASK));
  Serial.println(("Capture Done."));  
  length = myCAM.read_fifo_length();
  Serial.print(("The fifo length is :"));
  Serial.println(length, DEC);
  if (length >= MAX_FIFO_SIZE) //384K
  {
    Serial.println(("Over size."));
    return ;
  }
  if (length == 0 ) //0 kb
  {
    Serial.println(("Size is 0."));
    return ;
  }
  //Construct a file name
  //k = k + 1;
  //itoa(k, str, 10);
  //strcat(str, ".jpg");
  //Open the new file
  outFile = SD.open(String(n)+".JPG", O_WRITE | O_CREAT | O_TRUNC);
  if(!outFile){
    Serial.println(("File open failed"));
    return;
  }
  myCAM.CS_LOW();
  myCAM.set_fifo_burst();
  while ( length-- )
  {
    temp_last = temp;
    temp =  SPI.transfer(0x00);
    //Read JPEG data from FIFO
    if ( (temp == 0xD9) && (temp_last == 0xFF) ) //If find the end ,break while,
      {
        buf[i++] = temp;  //save the last  0XD9     
        //Write the remain bytes in the buffer
        myCAM.CS_HIGH();
        outFile.write(buf, i);    
        //Close the file
        outFile.close();
        Serial.println(("Image No. "+String(n)+" save OK."));
        is_header = false;
        i = 0;
      }  
    if (is_header == true)
      { 
        //Write image data to buffer if not full
        if (i < 256)
        buf[i++] = temp;
        else
          {
            //Write 256 bytes image data to file
            myCAM.CS_HIGH();
            outFile.write(buf, 256);
            i = 0;
            buf[i++] = temp;
            myCAM.CS_LOW();
            myCAM.set_fifo_burst();
          }        
      }
    else if ((temp == 0xD8) & (temp_last == 0xFF))
      {
        is_header = true;
        buf[i++] = temp_last;
        buf[i++] = temp;   
      } 
  } 
}


void play_WAV()
{ AudioZero.begin(44100);
  File myFile = SD.open("output"+String(n)+".wav");
  if (!myFile) {
    // if the file didn't open, print an error and stop
    Serial.println("error opening test.wav");
    while (true);
  }


  Serial.print("Playing");
  
  // until the file is not finished  
  AudioZero.play(myFile);
  Serial.println("Finished playing");
  delay(300);
}

 

Links to other blogs:

  1. Audio4Vision #01 - Introduction and Plan of Action
  2. Audio4Vision #02 - Initial research: ResNet as a starting point
  3. Audio4Vision #03 - SD card and WiFi setup in MKR1000
  4. Audio4Vision #04 - Show and Tell: Image Caption Generator Neural Network
  5. Audio4Vision #05 - Show and Tell: More Iterations and Finetuning
  6. Audio4Vision #06 - Initial prototyping with OV7670
  7. Audio4Vision #07 - The ArduCAM Mini OV2640 2MP and saving images to SD card
  8. Audio4Vision #08 - Deploying the Show and Tell model on a server
  9. Audio4Vision #09 - Interfacing Amplifier and Speaker with MKR1000
  10. Audio4Vision #10 - TTS: Text to Speech library
  11. Audio4Vision #11 - Arduino MKR1000, its code and HTTP methods
  12. Audio4Vision #12 - Putting it all together, wrap up and thanks!

 

 

Finally, we would like to thank Element14 and Arduino, for giving us the opportunity to break from the cookie-cutter education system and indulge in this extra-curricular creative exercise. We want to thank other challengers for providing a sense of friendly competition, and the mentors to keep us motivated, their suggestions were really valuable. We want to thank all those who have been following our blogs and we want to thank the programming gods for seeing us through this project

 

Hope this blog is considered in your judgment phase! Cheers!

 

Regards,

 

Pranjal Ranjan,

Sarvesh Patil,

Utkarsh Sharma

  • Sign in to reply

Top Comments

  • 14rhb
    14rhb over 8 years ago +3
    Hi Pranjal, That is a great system you've made there - congratulations. Apart from making a really applicable 'Design For A Cause' project you have also helped to enlighten us about some of these other…
  • pranjalranjan299
    pranjalranjan299 over 8 years ago in reply to dixonselvan +3
    Thanks a lot dixonselvan !
  • prashanth.nagendrappa
    prashanth.nagendrappa over 8 years ago +2
    Great Work Bro
Parents
  • prashanth.nagendrappa
    prashanth.nagendrappa over 8 years ago

    Great Work Bro

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • prashanth.nagendrappa
    prashanth.nagendrappa over 8 years ago

    Great Work Bro

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
Children
  • pranjalranjan299
    pranjalranjan299 over 8 years ago in reply to prashanth.nagendrappa

    Thanks a lot bro!