Design for a Cause - Design Challenge
  • Challenges & Projects
  • Design Challenges
  • Design for a Cause - Design Challenge
  • More
  • Cancel
Design for a Cause - Design Challenge
Blog Cue System for Anosmia and Smart WheelChair #1 - Introduction
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
  • Author Author: dixonselvan
  • Date Created: 3 Jul 2018 6:38 AM Date Created
  • Views 3318 views
  • Likes 12 likes
  • Comments 10 comments
  • dixonselvan
  • accessibility_projects
  • ardexpert
  • design for a cause - design challenge
  • mkr_projects
  • design for a cause
Related
Recommended

Cue System for Anosmia and Smart WheelChair #1 - Introduction

dixonselvan
dixonselvan
3 Jul 2018

<<<<Previous Blog     Next Blog>>>>

 

Audio & Visual Cue System for Anosmia (Smell Disorder) and Smart WheelChair - Ft. Amazon's Alexa

Week 1: July 3 - 9

     I am glad to be selected as a sponsored contestant for the 'Design for a Cause' Design Challenge. Thanks to the Element14 Community team and the sponsor Arduino. This blog is to introduce my project's cause and provide an overview of its design.

 

Cause:

  • This project is to enhance the lives of people suffering from Anosmia, an inability to sense smell. It has been reported that 5% of the population suffer from Anosmia [Source - Link].
  • I was also moved to help the characters in Design for a Cause Challenge: Meet The Users. They had a common objective to be fulfilled which is to control appliances (TV, Charge Cell Phone). This project will also help them to meet this objective.

 

Design for the Cause:

     This project can be split into two separate systems as below,

    1. Audio & Visual Cue System
    2. Smart Wheel Chair

 

1. Audio & Visual Cue System    

     This system is for people suffering from Anosmia. The Arduino MKR1000 with a to be developed machine learning algorithm will be able to predict the name of smell it is exposed to. This way it can then give out cues to the people. Amazon's Alexa will feature here to voice out the cue.   

 

     What's the use?

    • The person suffering from Anosmia will be able to understand the smell in the environment they are in.
    • They can be alerted in case of a smoke or when potentially harmful gases leak out.

 

2. Smart Wheel Chair

     The Smart Wheel Chair will be able to sense the environment and get updates (like temperature), also it can control appliances (TV, Chargers etc.) through voice commands. Amazon's Alexa will feature here to serve as the mediator to decode the voice commands to Arduino MKR1000 which will then control appliances. Also, the accelerometer and Ultrasonic sensor will be used to alert the person in the wheelchair for chances of a fall or a collision.

 

Design Overview:

image

Progress made so far,

|||||  5%

Table of Contents

 

{tabbedtable} Tab LabelTab Content
IntroductionThis Blog
Unboxing of KitCue System for Anosmia and Smart WheelChair #2 - Official Kit and Amazon Echo Dot Unboxing
Plan

Cue System for Anosmia and Smart WheelChair #3 - The Plan

Hardware - Cue System for Anosmia and Smart WheelChair #7 - Hardware Explained and Case

Smart WheelChair

Cue System for Anosmia and Smart WheelChair #4 - IoT Temperature Monitoring [DIY]

Steps for connecting Arduino MKR1000 with thinger.io for reading temperature data

Cue System for Anosmia and Smart WheelChair #6 - Fall and Collision Detection [DIY]

Cue System for Anosmia and Smart WheelChair #8a - Home Appliance Control

Cue System for Anosmia and Smart WheelChair #8b - Home Appliance Control

Cue System for Anosmia and Smart WheelChair #9 - Smart WheelChair Integration

Exploring Amazon Alexa

Cue System for Anosmia and Smart WheelChair #5 - Exploring Amazon Alexa

Exploring Amazon Alexa - Getting started with the Alexa app

Exploring Amazon Alexa - Blueprints

Cue System for Anosmia

Cue System for Anosmia and Smart WheelChair #10 - Gas Sensors and Machine Learning

Cue System for Anosmia and Smart WheelChair #11 - Machine Learning and Demo [Completed]

 

<<<<Previous Blog     Next Blog>>>>

  • Sign in to reply

Top Comments

  • three-phase
    three-phase over 8 years ago +3
    Good luck with your project(s) Kind regards
  • carmelito
    carmelito over 8 years ago +3
    Sounds like a cool project, will be interesting to follow your progress ..- Carmelito
  • dixonselvan
    dixonselvan over 8 years ago in reply to genebren +2
    Nice question genebren There is actually no connection between the condition and the need for a wheelchair. I just wanted to help them both ( A person suffering from Anosmia and person who need to use…
  • prashanth.nagendrappa
    prashanth.nagendrappa over 8 years ago

    Good Luck bro

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • dixonselvan
    dixonselvan over 8 years ago in reply to three-phase

    Thank you three-phase

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • three-phase
    three-phase over 8 years ago

    Good luck with your project(s)

     

    Kind regards

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • dixonselvan
    dixonselvan over 8 years ago in reply to genebren

    Nice question genebren There is actually no connection between the condition and the need for a wheelchair. I just wanted to help them both ( A person suffering from Anosmia and person who need to use a Wheel Chair) in a single design challenge.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • genebren
    genebren over 8 years ago

    Dixon,

     

    Nice start to your design challenge project.  Sounds like a very useful project for those suffering with Anosmia.  I am a little confused, is there a connection between this condition and the need for a wheelchair?  Or is this targeted to unique person?

     

    Good luck!

    Gene

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
<