The Experimenting with Sensor Fusion Design Challenge, sponsored by AMD Xilinx, and featuring Spartan-7 SP701 FPGA Evaluation Kit has officially concluded. We had 4 participants, including the Grand Prize Winner and Runner-up. Our judges have read each…
Table of Contents
Introduction
Project Description (Recap)
Design Process
Task #1: Implement an unaccelerated OpenCV application which handles the pose graphics.
Task #2: Simplify the OpenCV functions.
Task #3: Accelerate the OpenCV functions…
Sensor Fusion for Firefighters Summary
At the end of October 2022 I was selected to participate in the Experimenting with Sensor Fusion Challenge sponsored by element14 and Xilinx.
Since we received the SP701 evaluation kit, it has been two months…
By incorporating a low resolution thermal imaging overlay using the MLX90640 thermal array, we have already integrated all the sensors planned into the system.
Table of Contents
Project Update
Fusion of Sensors
Viewing in the dark
…
We added a hardware accelerated compass synthesized from C in Vitis HLS to our environmental HUD monitor on the AMD Xilinx SP701 development board. We have tested two different magnetometers: the ST's LSM9DS1 of the Digilent PmodNAV module and the Memsic…
The project is progressing well. I added some sensors to be able to monitor the environment through the heads-up display. I also built a customizable module with Vitis HLS to display up to 16-digit virtual seven-segment display modules overlaid on the…
Table of Contents
Introduction
Project Description
Hardware
Task Breakdown
Graphics
Video Capture and Display Pipeline
Integration
Current Status
About Me
Introduction
Greetings Element14 community! This is my introductory…
In this blog, I rebuild from scratch the demo application from the Spartan-7 SP701 FPGA Evaluation Kit Demo Project designed by Adam Taylor ( adamtaylorcengfiet ). The challenging element of that project is to show a Heads-Up display during the live broadcast…
I'm still learning more about image processing before I start building my Experimenting with Sensor Fusion Challenge project. In this blog I share my experiences rebuilding the Xilinx MIPI CSI-2 RX subsystem IP Core sample application. The application…
In this post I describe my first contact with the AMD Xilinx SP701 evaluation board . I briefly review the contents of the evaluation kit. Then I connect the evaluation board for the first time and launch the execution of the built-in tests.
The kit…
This is the introductory blog of my participation in the Experimenting with Sensor Fusion Challenge . First of all, I would like to thank the sponsors: Element14 and AMD Xilinx, for choosing my application to participate in this challenge. In this blog…