Safe and Sound
  • Challenges & Projects
  • Design Challenges
  • Safe and Sound
  • More
  • Cancel
Safe and Sound
Blog Safe & Sound - Example Code for the Challenge Kit
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
  • Author Author: Jan Cumps
  • Date Created: 16 Feb 2017 7:39 PM Date Created
  • Views 1071 views
  • Likes 6 likes
  • Comments 6 comments
  • msp432_launchpad
  • safe and sound
  • cc3100boost
  • cc3100_boosterpack
  • safe & sound
  • msp432
  • safe&sound
  • ti_rt
Related
Recommended

Safe & Sound - Example Code for the Challenge Kit

Jan Cumps
Jan Cumps
16 Feb 2017

An overview of Example Programs for some of the parts that you get in the kit.

 

They are grouped by Kit Part. You can scroll to the part that you're planning to use and check the example project.

All blogs involve the MSP432 LaunchPad.

 

image

 

Some of these articles can give your project a head start. Most of them use TI-RTOS. Each one is a working mini-project.

 

 

 

MSP-EXP432P401R LaunchPad

MSP432 LaunchPadMSP432 LaunchPad

 

 

 

image

 

Blog:

  • MSP432 and TI-RTOS: Getting Started Pt. 1 - Set Up and 1st RTOS Task
  • MSP432 and TI-RTOS: Getting Started Pt. 2 - Add an ADC Sample Task
  • MSP432 and TI-RTOS: Getting Started Pt. 3 - USB with Minimal CPU Use
  • MSP432 and TI-RTOS: PWM
  • MSP432 and TI-RTOS: PID Library Part 1 - Intro
  • MSP432 and TI-RTOS: PID Library Part 2 - Real World Example
  • MSP432 and TI-RTOS: another I2C example - talk to a DAC

 

 

SimpleLink Wi-Fi CC3100 module BoosterPack

CC3100 BoosterPackCC3100 BoosterPack

 

image

 

Blog:

  • WiFi with MSP432 and SimpleLink CC3100: Basic Setup

 

BOOSTXL-SENSORS Sensors Booster Pack

BOOSTXL-SENSORSBOOSTXL-SENSORS

 

image

 

Blog:

  • MSP432 and TI-RTOS: I2C Configuration for Sensors BoosterPack

 

 

430BOOST-SHARP96 Memory LCD Booster Pack

430BOOST-SHARP96430BOOST-SHARP96

 

image

 

Blog:

  • MSP432 and TI-RTOS: Sharp LCD BoosterPack

 

 

If you're writing a how-to during the challenge, make sure to promote it. It 'll make it an interesting happening.

  • Sign in to reply

Top Comments

  • ipv1
    ipv1 over 9 years ago in reply to ipv1 +3
    BTW thanks Jan Cumps sir. I usually start with tutorials but since you have taken care of most of em, I am forced to get actual work done.
  • ipv1
    ipv1 over 9 years ago in reply to mcb1 +2
    Im gonna spend the extra time experimenting with the RTOS software and making a schematic and ordering samples and stuff. Gonna try sending PCBs to multiple fabs this time. Hope to get some video blogs…
  • DAB
    DAB over 9 years ago +1
    Great point Jan. DAB
Parents
  • jkutzsch
    jkutzsch over 9 years ago

    Jan Cumps What would you suggest we look at while waiting for the Kits to arrive?  Something we can tinker a bit with maybe...  :-)

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • Jan Cumps
    Jan Cumps over 9 years ago in reply to jkutzsch

    If you haven't installed the software yet, you can do that and check out the example code. There are many, it'll keep you busy for a while.

    you can also download the quickstart guides of each kit and make yourself familiar with the pinouts of the boosterpack connectors.

     

    if you plan to build custom electronics you could start designing the PCBs. This tends to be a long process if you include the shipping - for me in Belgium ordering and receiving typically takes 3 weeks when I use OSHPark or Seeed.

     

    if you are planning to use SPI or I2C, you can check out how to develop that on an MSP432 and read what the slave IC is expecting.

     

    Check out how you wil make housing or how you 'll integrate it in the clothes/helmet/...

     

    pick or build a battery pack that you can carry along. How are you going to recharge a battery?

    try to collect your energy budget. How much power does each part consume. How can you get that as low as possible?

    how much battery do you need to get a decent lifetime out of your design.

    This is a particular complex area because virtually any design decision you make (or don't make) impacts battery life. You don't want to have a critical safety design that runs out of battery. That makes it a risk because the wearer relies on it for her safety.

     

    Things that you will not have time for at the end of the challenge, when you often struggle to get your separate ideas integrated into one gizmo.

     

    walk in the woods and enjoy nature.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • Jan Cumps
    Jan Cumps over 9 years ago in reply to jkutzsch

    If you haven't installed the software yet, you can do that and check out the example code. There are many, it'll keep you busy for a while.

    you can also download the quickstart guides of each kit and make yourself familiar with the pinouts of the boosterpack connectors.

     

    if you plan to build custom electronics you could start designing the PCBs. This tends to be a long process if you include the shipping - for me in Belgium ordering and receiving typically takes 3 weeks when I use OSHPark or Seeed.

     

    if you are planning to use SPI or I2C, you can check out how to develop that on an MSP432 and read what the slave IC is expecting.

     

    Check out how you wil make housing or how you 'll integrate it in the clothes/helmet/...

     

    pick or build a battery pack that you can carry along. How are you going to recharge a battery?

    try to collect your energy budget. How much power does each part consume. How can you get that as low as possible?

    how much battery do you need to get a decent lifetime out of your design.

    This is a particular complex area because virtually any design decision you make (or don't make) impacts battery life. You don't want to have a critical safety design that runs out of battery. That makes it a risk because the wearer relies on it for her safety.

     

    Things that you will not have time for at the end of the challenge, when you often struggle to get your separate ideas integrated into one gizmo.

     

    walk in the woods and enjoy nature.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
Children
  • mcb1
    mcb1 over 9 years ago in reply to Jan Cumps

    Good suggestions.

     

    Try to do your blog plan.

    You'll find areas that you can do without the kits, despite them being further down the challenge.

    eg. ipv1 has wireless charging planned, so he can do some preliminary work on the mounting, attaching, and testing.

     

     

    mark

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • ipv1
    ipv1 over 9 years ago in reply to mcb1

    Im gonna spend the extra time experimenting with the RTOS software and making a schematic and ordering samples and stuff. Gonna try sending PCBs to multiple fabs this time. Hope to get some video blogs out this time image

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • ipv1
    ipv1 over 9 years ago in reply to ipv1

    BTW thanks Jan Cumps sir. I usually start with tutorials but since you have taken care of most of em, I am forced to get actual work done.

     

    image

    • Cancel
    • Vote Up +3 Vote Down