Upcycle It
  • Challenges & Projects
  • Design Challenges
  • Upcycle It
  • More
  • Cancel
Upcycle It
Blog [Upcycle It] Interactive Race Car Driver - 3D Printed Parts
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
  • Author Author: Workshopshed
  • Date Created: 7 May 2017 8:21 PM Date Created
  • Views 2474 views
  • Likes 7 likes
  • Comments 14 comments
  • interactiveracecardriver
  • upcycle_it
  • upcycled_interactiveracecardriver
Related
Recommended

[Upcycle It] Interactive Race Car Driver - 3D Printed Parts

Workshopshed
Workshopshed
7 May 2017

Recycled filament

I had intended to use some recycled filament from a Kickstarter. However, as with many Kickstarters it has been delayed. So Instead I ordered some filament from a dutch firm, Refil. They get their filament from 2 different places. The first is from bottles, these are a material called "PET" and comes in a transparent but coloured materials. The second is ideal for my chassis, it is black (dark grey) ABS which comes from old car dashboards, it seems fitting that an old car should become part of a new car.

 

Software

I've used different CAD packages over the years but recently I've been doing a lot with OpenSCAD. This is different from a lot of CAD packages in that the only way you can create objects is via scripting.

 

Here's a simple example of a cylinder joined to a circle which has been extruded around a 70degree corner.

 

module Exhaust() {
    union()
    {
    translate([1.81,4.66, 0])
        rotate([-20,-90,0])
            cylinder(r1=1.5,r2=2.5,h=30, $fn=100);

    rotate_extrude(convexity = 10, angle=70, $fn=100)
        translate([5, 0, 0])
            circle(r = 1.5, $fn = 100);
    }
}

image

I find it is good for 3D printing as you can tune the parameters as you build different models. As it's a coding language naturally parts that are repeated in arrays or circles are easy to reproduce. It's less good at producing organic items such as trees although you could use "fractal" algorithms for that kind of thing.

I have been working around a bug where the "difference" function causes things to disappear on one of my Win10 machines. Something to do with Java and incompatible video drivers apparently.

Parts

One technique I used on several of the parts was to print out a couple of layers and then cancel the print to give a floppy template. This allowed me to cross check the dimensions and ensure things would fit together.

 

Chassis

The chassis serves several purposes: it's there to strengthen the middle section that was weakened by the cutting down; it provides mounting for the battery and Edison, and it provides an attachment point for the bumpers. This has gone through many iterations, the initial models were massively over engineered with 10mm thick struts and would have taken many many hours to print. So it's been slimmed down and simplified. The other key design feature was making it short enough to fit on my 210mm printer bed. After watching a video by Vicki Somma, I realised that the buffers that held the bumpers in place would be better as octagons so that when I print the sockets on the mating parts they won't have a big span to cross. The design changes cut the predicted print time from 4hrs to 2hrs 20minutes and also the amount of filament used is reduced.

image

Bumpers

I had initially thought about attaching the bumpers with rods and springs but I realised that I can use the springy properties of the PET plastic and just attach them directly to lugs on the chassis. Here's my sketch and models of how these might be built.

imageimageimage

Edison Support

The Edison needs attaching to the car so I wanted something that looked like it was part of a car. I created a part with a fuel tank, exhaust, battery and a belt driven pulley. To reduce the material used in the print (and hence reduce print time) I added some hollowing out below the parts. I printed the part in draft-mode using some green ABS that I had available. I've a selection of self-tapping screws harvested from various old computer parts over the years so I'll use those to attach the Edison to the support.

imageimageimage

Battery Clip

My initial model for the battery clip was all in one part. I realised that this would mean that the clips would be quite tall. This has two issues, firstly a long print time and secondly, it was a risky print as the vertical parts might move during the print and cause failures. So I redesigned it in 3 parts connected with a dovetail joint. This meant that the clip parts could be printed on their sides and hence would be a lot shorter and more stable. Initially, the material seemed to bond well to the bed but there were a couple of failures where it broke off. So I fined tuned the temperature settings and sizes and re-printed, I also added a brim although I'm not sure that was strictly necessary.

imageimageimage

image

Drivers Seat

The seat is there to hold the Furby driver in place, it will also hold the motor driver board in place. Key design features will be that it will straddle the chassis and need space for routing the cables. As the photo below shows the driver board will likely be mounted vertically on the back of the chair.

image

Car Body

I've not started designing the car body yet but the plan is to use a green recycled PET for that. Hopefully, it will be possible to print a thin walled model so the electronics can be seen through the plastic.

 

Reference

OpenSCAD - The Programmers Solid 3D CAD Modeller

Refil - The makers of recycled filament

Embedding Nuts into 3D Printed Tap Handles

 

Previous Posts

[Upcycle It] Interactive Race Car Driver - Plan of action

[Upcycle It] Interactive Race Car Driver - Software

[Upcycle It] Interactive Race Car Driver - Lights

[Upcycle It] Interactive Race Car Driver - Detailed Plan

[Upcycle It] Interactive Race Car Driver - Edison

[Upcycle It] Interactive Race Car Driver - Drive Motor Testing

[Upcycle It] Interactive Race Car Driver - Car modification

[Upcycle It] Interactive Race Car Driver - Furby Hacking

[Upcycle It] Interactive Race Car Driver - Powering Motors

[Upcycle It] Interactive Race Car Driver - Bumper switches and wiring loom

[Upcycle It] Interactive Race Car Driver - Securing MQTT

  • Sign in to reply

Top Comments

  • Workshopshed
    Workshopshed over 9 years ago +3
    Light testing players.brightcove.net/.../index.html
  • mcb1
    mcb1 over 9 years ago +2
    Good post. Workshopshed and fvan need to stop showing me how useful a 3D printer is for these things.
  • fvan
    fvan over 9 years ago in reply to mcb1 +2
    What? Why? What ?! I'm innocent!
  • DAB
    DAB over 9 years ago in reply to Workshopshed

    Looks great.

     

    DAB

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • Workshopshed
    Workshopshed over 9 years ago

    Light testing

    You don't have permission to edit metadata of this video.
    Edit media
    x
    image
    Upload Preview
    image

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • Workshopshed
    Workshopshed over 9 years ago in reply to carmelito

    Hi carmelito the printer is a Cel Robox. Have been using it for a couple of years now. Mostly with ABS but also PLA and now PET.

    image

    CEL Robox 3D Printer - Review

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • Workshopshed
    Workshopshed over 9 years ago

    Lighting bar, headlights and indicators work in progess

    image

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • mcb1
    mcb1 over 9 years ago in reply to fvan

    But, is the beer any good?

    The Tui Blonde is okay, but generally don't drink it.

     

    Apparently the monks have nothing to do with the brewing process

    https://www.youtube.com/watch?v=F0o6EznQkvo

    https://www.youtube.com/watch?v=7O94GIT9Uo0

    https://www.youtube.com/watch?v=uFUJSaZLnCw

    https://www.youtube.com/watch?v=6-npWEcRaQ4

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
>