Real quick: IDEC-TUI is a command line utility for reading, writing, and monitoring IDEC PLC registers and assets. Operates over usb serial, and it is still very much a work in progress. However there has been some new features added:
Scrip...
SensoredHacker's On The Line Challange with PLCs, HMIs, Arduinos
R&D from May through June 2026
The original FC6A library began after a work project where I needed to log basically every PLC event in a testing array. I wrote the functions I neede...
The main concept was to build a clock generator that supported at least a 50 MHz frequency. I have decided to use a module with Si5351. This module supports the three simultaneous outputs for which it is possible to set individual output frequencies....
A few weeks ago, I was asked to check the car's radio that had an issue with power on. It was the Blaupunkt Bremen 975, which is one of those radios with Android. The initial check and measurements showed that, from the perspective of electronic...
For a few months, I was the owner of Siglent SDS824X HD, which is a really good device in case of performance and price ratio. But I have decided to perform an upgrade and get one more advanced device which supports higher bandwidth, sampling a...
ESP32 Bit Pirate is open-source firmware that turns your device into a multi-protocol development and analysis tool, inspired by the legendary Bus Pirate.
When I started working on ESP32 Bit Pirate, the idea was simple: take the spirit of the origina...
ESP32 Bit Pirate is an open-source firmware that turns your device into a multi-protocol hacker's tool, inspired by the legendary Bus Pirate.
It supports sniffing, sending, scripting, and interacting with various digital protocols (I2C, UART, 1-Wir...
Oh Boy, Ive really done it now. When I told our OEM PLC supplier that we need to delete old log files, They just about lost it. We can write files, every second of everyday, but when the on board memory gets full, there is no method ...
Background
The Analog Discovery 3 has support for two programmable power supplies with a voltage range 0.5V to 5V and -0.5V to -5V. These power supplies have support for voltage readback, but there is no information about current usage. Even t...
Hi everyone,
I’m working on a small tool idea around STM32 / Cortex-M debugging, and I’d like honest feedback before building too much.
The problem I’m trying to validate is this:
When a Cortex-M firmware crashes into HardFault_Hand...
The WaveForms has a nice feature that allows us to perform characterization of elements like diodes or transistors. By default, it requires a dedicated adapter. However, there is an option to use a breadboard and a simple circuit. For example, to ch...
I received this surprise swag bag last week, but unfortunately I was not able to make a post because I was having problems with my desktop. Now that the issue has been resolved, I am finally able to share it.
First of all, I was completely surprised ...
Bebe the green parakeet explores the underwater world In a DiY submarine built by Steven Lawyer. (Image Credit: bebebirdparrot/Instagram)
Parakeets are great pets with high intelligence and social skills. However, they can’t dive in the water,...
Some time ago, I occasionally bought an HP 5082-7010 LED display, which I did not have time to test if working properly. Today I decided to do this with the help of Analog Discovery 3.
The HP 5082-7010 is a single-digit red LED numeric display modu...
I received by Swag bag yesterday, Being mentioned as a Rising Contributor in 2025 Year in Review & Celebrating You It has been a honor to be part of this community. I started being active on this community almost an year ago and ...
I was taken by surprise when a package had my name on it and it wasn't something I remembered ordering.
It was full of swag from e14.
Happy days. Thank you so much. It's always appreciated.
As a fan of e14 I just love the fan... after la...
Today, I decided to check the pattern generator and logic analyzer features of the Analog Discovery 3. I have used a Microchip development board from the Curiosity Nano series with AVR16EB32 MCU, as a device under test unit. The AVR16EB32 MCU has su...
Save as Draft
I just arrived home from an extended trip and what did my wandering eyes see but a swag bag from E14.
My friends and family are enjoying the spoils. I typically share the stuff. The miniature USB fan I think I will keep. That has ...
Thanks E14Alice and element14 for the surprise swag package for contributing to the community.
Here is a quick video showing all the goodies.....
https://youtu.be/4bk5VVIOIsY
Thanks Element14 and E14Alice for the 2025 Contributor Swag package that arrived just in time for my 14th Anniversary next Tuesday! Very rewarding (literally!) to be part of this engineering community. Looking forward to participati...
It looks like the Easter Bunnies have been busy again at e14.
Many thanks for the mention in 2025 Year in Review & Celebrating You and many thanks for all the lovely surprise swag received today. Much appreciated.
Thank you element14 and E14Alice ! Earlier this morning, a package appeared on my front porch. What a great way to start a Monday. And inside the package was... e14 stuff!!! Whoo-hoo!!!
As you can tell, I'...