Personal Blogs
  • Community Hub
  • More
Personal Blogs
NexGen Flight Simuator
  • Blog
  • Documents
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New

NexGen Flight Simuator

  • Tags
  • Subscribe by email
  • More
  • Cancel
  • Nexgen: CANaerospace: RSS: C-3436A Radio: Build iv: Code Review

    phoenixcomm
    phoenixcomm
    I have been fighting with the Arduino for the last few years. this time I wanted to simplify my code base by using a struct in my header file: // typdef struct frequency {   int bits[20][5] = {{1,1,0,0,1},{1,1,0,0,0},{1,1,1,0,0},{1,0,0,0,1},...
    • 16 Sep 2021
  • Nexgen: CANaerospace: RSS: C-3436A Radio: Build iiia

    phoenixcomm
    phoenixcomm
    So, before I waste some more of my time, I have decided to test the frequency selector pin-outs on P1. So what I decided was to put 5 LEDs on some perf-board with their resistors. Then connect them to the P1 (H-L and then (N-R) with wires between the...
    • 4 Sep 2021
  • Nexgen: CANaerospace: RSS: C-3436A Radio: Build ii

    phoenixcomm
    phoenixcomm
    Well, here I am again, what is this the third time? I last took this up in the blog Nexgen: CANaerospace: RSS: C-3436A Radio: Build i. So this is part II of the build, covering the hardware, 2x RS232 cutouts, securing the CAN interface, as well as t...
    • 26 Aug 2021
  • Nexgen: CP-1252/ASN-128: Decoding the Keyboard

    phoenixcomm
    phoenixcomm
    Ok, the Keyboard is comprised of 3 columns, the two outer columns have 5 switches each, and the center column has 4 switches. The switches are all lights.  Pins 1 are white, are lamp Ground, pin 8, gray is lamp power. One side of the switch...
    • 8 Aug 2021
  • What You Can get away with on Television: 6: The Battery Daddy Case

    phoenixcomm
    phoenixcomm
    www.youtube.com/watch They claim and I quote "Loose Batteries can touch and lose power" are they nuts? This claim is about 1 minute in. Did the world of physics or electronics change??  In the words of PT Barnum "There's a su...
    • 28 Jul 2021
  • MCU-128 Backpanel

    phoenixcomm
    phoenixcomm
    PROBLEM:I have been struggling to find a solution to a mess that has stopped me from doing much with this project. The interconnection is weird 0.025" square, on a 0.1" center. Nothing fits this dam thing to make matters worse there are no ...
    • 24 Jul 2021
  • Nexgen: CANaerospace: RSS: C-3436A Radio: Build i

    phoenixcomm
    phoenixcomm
    This is a how-to I build a typical node, this will show you my methodology. You will need to gather your goodies. In this case, I will need the following: ( this is a complication of the Info, Manufac, and Category tables the only thing not included ...
    • 15 Jun 2021
  • Nexgen: CANaerospace: RSS: C-3436A Radio

    phoenixcomm
    phoenixcomm
    I have talked about this radio back in the day. Please See NexGen Simulator Blog Index iii. You will see 13 prior entries. So why 14? This post is using my current schematic for the wiring which will do the decoding very straightforward.  The C-...
    • 6 Jun 2021
  • Nexgen: Protocol Conversion: Ethernet <> CANaerospace - I

    phoenixcomm
    phoenixcomm
    Ok, what is a protocol converter, and why do I need one? Well, a CANaerospace frame is defined as an 8-byte message with the first four (4) bytes comprising the header and the remaining four (4) bytes as Message Data which is type-specific (see diagr...
    • 3 Jun 2021
  • Nexgen: ATR Box Version 3 FINAL!!!

    phoenixcomm
    phoenixcomm
    So why do I need a version 3? Version 2, takes forever to print and the printers are in the library (still closed). So that leaves me to go look for a better solution. Along comes The Container Store. They have an acrylic box (Kid's Shoe Box, clear a...
    • 10 May 2021
  • NexGen: Multi-Purpose Color Display (F/A-18C/D MPCD): Hardware / Software Interface II

    phoenixcomm
    phoenixcomm
    I have been down this road before but now I have the final solution. I found it in my old Motorola M6800 Applications Handbook, section 5-1.1.2 NonEncoded Keyboards. It used a PIA or Peripheral Interface Adapter, but since I am using an Arduino I ne...
    • 27 Mar 2021
  • NexGen: RSS: Radio Set C-3436A/ARN-30D: Interface Cable REDO  FINS!!

    phoenixcomm
    phoenixcomm
    I have been working on my C-3436A radio for quite a while after it worked I took it apart to install it in its new home and I could never get the damn thing to work again.  So with way too much time on my hands, I decided to ring out the damn c...
    • 12 Mar 2021
  • Tech Tip IX: SN74HC595N tips and tricks!

    phoenixcomm
    phoenixcomm
    Well, a lot of folks have written about the SN74HC595x as an 8-bit shift register. The major use is to expand ports in the Arduino. (image 1) This is the classic way to expand your Arduino for 8 more ports, without resorting  I2C or CAN bus.&nb...
    • 1 Mar 2021
  • NexGen: CDU Pinlite Displays: Final Word !! REDACTED!!!!

    phoenixcomm
    phoenixcomm
    STATEMENT:  I have a problem refreshing, the  20 odd displays in less than 1/4 second each, which would let them seem that there all bright, but they will be dim, to begin with. So multiplexing is now out for the 7 segment displays, but I s...
    • 20 Feb 2021
  • NexGen: Fuel Load Meter: New Plan of attack

    phoenixcomm
    phoenixcomm
    Well, here we are back again, with the Fuel Load Meter. This thing has given me nothing but grief. So I am going to take another whack at it. I still have to make sure that the wiring is correct. and then write the code. The problem I was/am having i...
    • 12 Feb 2021
  • NexGen: The Lab: Found More Test Equipment: SMD Rework Station 853D

    phoenixcomm
    phoenixcomm
    This unit is most likely made by YIHUA.  The 853D is broken down into three functional blocks.SMD Rework Wand. This has a digital temperature control and has interchangeable tips. Solder Station Wand. This has a digital temperature control and i...
    • 5 Feb 2021
  • NexGen: Unboxing the Multicomp PRO - Raspberry Pi 4 Starter Kit

    phoenixcomm
    phoenixcomm
    I have been waiting a few months for this little gem. So without further ado, let us get to the pictures 1 The Box? 2. Instructions? 3. Raspberry PI 4 4. 16GB Module with OS 5. A little plastic case for the thing. 6. Power Sup...
    • 23 Jan 2021
  • NexGen: KiCAD: Arduino Mega 256 Library

    phoenixcomm
    phoenixcomm
    Hi Gang, I just compted a schematic pinout for the Mega, Enjoy If you want to use it you can find it at www.NexGen-Simuattion.com  give me a day or two I just erased it but you still can use it. open in Gimp REMOVE BLACL Vertical and Horizontal ...
    • 22 Jan 2021
  • NexGen: Landing Gear and Rudder Subsystem: Ancillary Circuits.

    phoenixcomm
    phoenixcomm
    OK, I have worked the past few days on getting the RED lamp wiring finished. I have decided to get my 1Hz blink rate from a NE555 timer, instead of messing about with Arduino Timers or delay()! The Red Lamp can be 24vdc or 5vdc. The only thing that I...
    • 19 Jan 2021
  • NexGen: Landing Gear Subsystem

    phoenixcomm
    phoenixcomm
    This subsystem is part of the Pilot Controls (node id 100) consisting of the following subsystems. Inter-subsystem is handled by CAN.Side StickThrottleLanding Gear Lever lamps and sensorsRudder Pedals with differential braking.The subsystem consists ...
    • 14 Jan 2021
  • The Lab: HP 436A Power Meter

    phoenixcomm
    phoenixcomm
    Well, as you all know I love junk and test equipment even if I don't have a use for it now. Maybe 4 years ago I was at a garage sale where they were selling a lot of IC's etc.  He said, "Would you like a power meter?" I think h...
    • 8 Jan 2021
  • NexGen: The Lab:  How To Find Parts in Your Lab.

    phoenixcomm
    phoenixcomm
    I find my parts in a relational database. Why a DB? Well I have a lot of parts, everything from hardware, printed parts, and electronics, to avionics. Now, this is a pain. So there are a few tables that need to be created Info, Manufac, Category, and...
    • 29 Dec 2020
  • NexGen: Fuel Indicator: Wire & Power-up: 3

    phoenixcomm
    phoenixcomm
    In this post, I will be talking about my switches which are done with an interrupt on Arduino Mega's pin#2, and just to keep my head on straight the interrupt service routine's name is isr2. First, let me digress. The Fuel Load Indicator has two (2) ...
    • 22 Dec 2020
  • NexGen: Fuel Load Indicator: Aftermath!

    phoenixcomm
    phoenixcomm
    These three images are  from  "Embed With Elliot: Debounce Your Noisy Buttons" Why do I say aftermath? Well to put it simply it might have been a bit of an overreach.  I spent more than a few days trying in vain to...
    • 22 Dec 2020
  • NexGen: Fuel Load Indicator: It's Alive? (software testing)

    phoenixcomm
    phoenixcomm
    Header Pins Mapping to Arduino Mega   HeaderPins Color Signal Mega Pins HeaderPins Color Signal Mega Pins Pins.h pinModes.h 1 RED Power Ext 30 BLACK GroundExt #define INT5 5   #define SDA 20#define SCL 21   #define CE1 4...
    • 22 Dec 2020
<>