Personal Blogs
  • Community Hub
  • More
Personal Blogs
NexGen Flight Simuator
  • Blog
  • Documents
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New

NexGen Flight Simuator

  • Tags
  • Subscribe by email
  • More
  • Cancel
  • NexGen: Specifications: Indicator, Slip and Turn

    phoenixcomm
    phoenixcomm
    Indicator, Slip and TurnManufacture:R.C. AllenPart Number: M3520-4Connector:Connector Mate:MS3106-14S-2SPin A: +28vPin B: -28vPin C: +5v (lighting)Pin D: -5VPin E: SpareNote: This unit will have to be modified as the indicator is gyroscopically driv...
    • 10 Dec 2020
  • NexGen: Component Documentation: Panel, Processor Select

    phoenixcomm
    phoenixcomm
    PROCESSOR SELECT PANEL Part Number: 7-511F00121-1National Stock Number 1290-01-438-6575 Connector: MIL-DTL-38999 III, 13 pins Mate: Pin 1: DS2, COMMON Pin 2: n/a Pin 3: n/a Pin 4: CR2, ANODE Pin 6: S1.SP1 = CR1 + CR...
    • 2 Dec 2020
  • NexGen: Navigation Computer Display: Keyboard Switch Interface: v2

    phoenixcomm
    phoenixcomm
    I have blogged about the Navigation Computer Display's Keyboard here. I was moving a 6821 PIA to its resting place and checked my Databooks where I found a pdf copy of the 6800 application manual. where they had a 4x4 keyboard interface. It was b...
    • 23 Nov 2020
  • NexGen: Fuel Indicator: Wire & Power-up: 2

    phoenixcomm
    phoenixcomm
    This is now round two. last night I wondered if I popped the MCP23017 or, is the scanner software bad? So the first this I did was to stick an MCP2327  on a breadboard and ran the scanner. It still said No I2C address found. As I relooked at the...
    • 18 Nov 2020
  • NexGen: Fuel Indicator: Wire & Power-up: 1

    phoenixcomm
    phoenixcomm
    Well, I am working to get the Indicator done today or tomorrow, the slight tremors in my hands make Wire-Wrap a real pain. I will not get to a point where this will be buttoned up, as there will be a lot of jumpers! I also have to trim down the inter...
    • 16 Nov 2020
  • NexGen: Fuel Indicator: Testing The Display

    phoenixcomm
    phoenixcomm
    This picture on the left is just to remind you all of what I am trying to get working.  Each HDSP-2131 display has 24 pins that give you 48 pins to deal with. Now let us complicate the issue the pins come out on a 30-pin connector of which 4 are...
    • 4 Nov 2020
  • NexGen: Fuel Load Indicator: Switches on Interrupts!

    phoenixcomm
    phoenixcomm
    Well, for starters there are problems with the Arduino CAN bus library, as ANY node in the system can be a master or a slave. Currently, the Arduino CAN supports a SLAVE - MASTER, relationship. On the MCP2515_CAN module, you have the following connec...
    • 2 Nov 2020
  • NexGen: Fuel Indicator: Redux v2

    phoenixcomm
    phoenixcomm
    I have been fighting to get my dual display board to function. The first attempt was to use a 50-pin breakout board: FAIL; The second attempt was to pin the ICs to the connector which is an IDC male with a notch (upper-left 1, lower-left, etc.  ...
    • 24 Oct 2020
  • The Lab: PanaVice

    phoenixcomm
    phoenixcomm
    Well, while at the local Goodwill Junk Store, everything under 7 pounds is $1.50 and over is well just $5.00, I found a PanaVice with a  vacuum base (model 380) with a set of PCB arms. Now the picture is from the internet. Mine is much worse for...
    • 16 Oct 2020
  • NexGen: Fuel Load Indicator: Architecture

    phoenixcomm
    phoenixcomm
    As this node will be fairly busy, I have decided to implement this with interrupts.  The interrupts come from one of three (3) devices: CANaerospace Bus interface, USB term, one (1) of 2 switches, each with two(2) positions.   CANaerospace ...
    • 14 Oct 2020
  • NexGen: Using BJTs to drive pinlite displays

    phoenixcomm
    phoenixcomm
    Redacted April 10, 2024 Statement: Driving Pinlight Lamps is very challenging. The design requirements are 4vdc @ 15ma per segment, if you are interested look here. So for the 7-segment displays, the total current is 7 x 15ma. or 105 ma. Now multiply...
    • 8 Oct 2020
  • Smarthab Thermostat? Or maybe a better name Life Support: Monitor and Control.

    phoenixcomm
    phoenixcomm
    I am calling this Life Support: Monitor and Control. Why you ask? This is a complete system that can control heating or cooling without changing settings. run the fan automatically for air quality and also handle a dehumidifier as well as detection&...
    • 28 Sep 2020
  • NexGen: Fuel Load Indicator: Wiring Plan

    phoenixcomm
    phoenixcomm
    Analysis: The first hurdle is that an Arduino has only GPIO pins but you can not get to a bus from here, without a lot of bit-banging by the CPU.Second, the Displays are smart devices and designed to have both Address and Data Buses.The only thing is...
    • 24 Sep 2020
  • HDSP-213x, Eight-Character 5.0-mm (0.2-in.) Glass/Ceramic Intelligent 5 × 7 Alphanumeric Displays for Military Applications

    phoenixcomm
    phoenixcomm
    The Broadcom , HP , HDSP-2131 (yellow), HDSP-2179 (orange), HDSP-2132 (high efficiency red) and the HDSP-2133 (green) are eight-digit, 5 × 7 dot matrix, alphanumeric displays. The 5.0-mm (0.2-in.) high characters are packaged in a standard 7.64...
    • 23 Sep 2020
  • NexGen: Fuel Load Indicator: Pinouts Redux

    phoenixcomm
    phoenixcomm
    I have decided to update my Fuel Load Indicator which has only outputs for a human. My goal is to Recycle & Retrofit this indicator so that it can talk over the CANaerospace network. The network responds to node 0 for multicast, and also nodes 66...
    • 22 Sep 2020
  • NexGen: Aircraft Data Base (Universal)

    phoenixcomm
    phoenixcomm
    The question is how can you put ALL the parts into one database? And then make some sense of the thing. I designed my database similar to the one we used at Interdata in the late '70s. So why do I call this universal? Well, I have separated parts by ...
    • 11 Aug 2020
  • NexGen: Component Documentation: Navigation Display Unit: ASN-1252/ASN-128

    phoenixcomm
    phoenixcomm
    NexGen: Component Documentation Doppler Navigation Display Unit: ASN-1252/ASN-128 Note: As this unit has been gutted I will have to do all the work.You can find a user manual here TM-1-1520-240-10 or you can find a nice pdf version here...
    • 6 Aug 2020
  • NexGen: The New Lab: DB-25 pinout tester - I

    phoenixcomm
    phoenixcomm
    Well, I'm just flat tired of fighting with my DB-25M interface connectors, at first, I thought of LEDs with pull up resistors. After dinner, my mind wandered back to my cable tester, hey, an Arduino Mega, which I have a bunch of, has 52 digital p...
    • 2 Aug 2020
  • Nexgen: Demystifying MySQL in Debian Buster

    phoenixcomm
    phoenixcomm
    As you may be aware that my hosting service eliminated my shared plan. So I did what I did before bring the damn thing down and host it myself. This is an ongoing fight with some wins. Since AT&T offered me IP space and a 1Gb line which I have n...
    • 31 Jul 2020
  • Nexgen: The Lab: B&K Precision 3010 Function Generator: Installing new power connector

    phoenixcomm
    phoenixcomm
    This project is well overdue as I started it over 2 years ago. If you remember the power cord set was unobtainium, and they had just soldered in a cable and tied a knot in it and called it a day.  So I decided to mount an STD IEC power connector...
    • 20 Jul 2020
  • NexGen: Collins Radio 813H-1 CDU - Tear down.

    phoenixcomm
    phoenixcomm
    +5vdc regulator+12vdc / +15vdc regulator-12vdc / -15vdc regulatorVideo MonitorChar DecemptyLine MemoryPOS DECDIOCK/DI dug this CDU out of my shed. The only document that I have was the pinout of the two rear connectors. I wish to thank KG at Collins ...
    • 14 Jul 2020
  • NexGen: CDU Component Documentation type 813H-1

    phoenixcomm
    phoenixcomm
    CDU TYPE 813H-1 / Number 792-6301-001 for a better view please see E14/NexGen:Componets/CDU:813H/images/CloseUPfrontview.png FAA-RD-79-1 - FAA-RD-79-2 - 3D/4D AREA NAVIGATION SYSTEM DESIGN, DEVELOPMENT, AND IMPLEMENTA...
    • 12 Jul 2020
  • NexGen: The Lab: Revolution 3

    phoenixcomm
    phoenixcomm
    It seems like the best intentions go by the wayside. If there was not enough turmoil in my life my hosting company whose tech support is based in the UK is the worst.  So I have decided to bring the server back home. I now only have till the end...
    • 15 Jun 2020
  • Nexgen: Adventures into CANaerospace part 2

    phoenixcomm
    phoenixcomm
    Oh well, after hooking up my 4x20 LCD (that was held over from the Beagle Bone AI project, that I could never get to work) it still failed on my Arduino Mega. I ordered one, off eBay. The first thing I  did was to run the test program. Vola it ...
    • 14 Jun 2020
  • Eclipse Pioneer Magnesian

    phoenixcomm
    phoenixcomm
    Well in my unpacking I came across this old piece of history, a one-inch diameter  Magnesian. It was made g-d knows when. This device has only four pins, which threw me for a loop. I did not understand how it worked until I found figure 2. Norma...
    • 31 May 2020
<>