Single-Board Computers
  • Products & Partners
  • Dev Tools
  • Single-Board Computers
  • More
  • Cancel
Single-Board Computers
Blog
  • Blog
  • Forum
  • Documents
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Single-Board Computers to participate - click to join for free!

Blog

  • Tags
  • Subscribe by email
  • More
  • Cancel
  • AI on the rise: Watson saves a life and Apple gets on the AI bandwagon

    Catwell
    Catwell
    IBM's Watson uses hospital data to save a patient's life; Apple's latest acquisition is an AI startup company. Supercomputer Watson isn't just really smart; it's a life saver(Photo from IBM)  Remember super computer Watson by...
    • 18 Aug 2016
  • Wall climbing robots create web-like creations

    Catwell
    Catwell
    The Mobile Robotic Fabrication System for Filament Structures used small robots and carbon fiber to create structures. The robot isn't trapping her; it built her a hammock. (via University of Stuttgart) Some would argue spiders and robots on...
    • 16 Aug 2016
  • Baby Exoskeletons Assist with Early Cerebral Palsy Risk

    Catwell
    Catwell
    This tyke is getting some motor support by wearing an electrical exoskeleton onesie. A combination of electrical sensors and motor supports helps detect infants’ risk of cerebral palsy when early intervention is possible to alter the course of the di...
    • 10 Aug 2016
  • Neural Programming Makes Robots Even More Humanoid

    Catwell
    Catwell
    Advanced programming techniques could turn robots into the next dance floor phenomenon...but much remains to be done before they’re less terrifying. This humanoid robot moves on its own due to advances in neural programming (via Osaka University via ...
    • 8 Aug 2016
  • Odroid C0

    mconners
    mconners
    I recently picked up one of these sweet little boards, and I have to say I'm pretty pleased. It is a stripped down version of the Odroid C1+, designed to be lighter, and more configurable to suit your end purpose.It is based on a quad core Amlogic S8...
    • 25 Feb 2016
  • Cooling the Inforce IFC6410 Plus

    e14 Contributor
    e14 Contributor
    Applies to both the Inforce IFC6410 and IFC6410 Plus Parts needed: 1x 28MM CPU HEATSINK1x 5V FAN1x Epoxy (can probably find it cheaper at a local hardware store)1x 2-pin header cable (optional). I cut off the HDD LED connector from an old P...
    • 5 Feb 2016
  • Cooling the Dragonboard 410c

    e14 Contributor
    e14 Contributor
    A bottom mounted cooling solution is best for the Dragonboard 410c due to layout and top-side interference shield with air gap. This will work for all current and future Dragonboards that follow the same 96boards CE spec. Here's a summarization o...
    • 1 Feb 2016
  • Automotive gauge cluster

    e14 Contributor
    e14 Contributor
    Hey not sure where to post this but o well. I have a project car im building and im looking to covert my cluster into a digital touch screen cluster.  I was going to use a tablet at first but single boards caught my eye. I have built a few deskt...
    • 31 Jan 2016
  • How To: 3D Space Orientation (yaw, pitch, roll) of IMU (accelerometer+gyro) on the Beaglebone Black Platform

    e14 Contributor
    e14 Contributor
    Here's a full length tutorial on how to get complete orientation knowledge (yaw, pitch and roll angles) on the Beaglebone Black embedded Linux platform using an IMU (MPU-6050 from Invensense). This platform can be used to create mini rovers, quad-cop...
    • 29 Nov 2015
  • Sound Synthesis and the Billion Dollar Paper

    shabaz
    shabaz
    Table of Contents Introduction Programmable Analog Sound Synthesis Synthesis Goes Digital Digital Sound Synthesis Improves a Lot: FM Synthesis Selling FM Synthesis Yamaha Replicating Chowning’s Work Summary References Introduction This bl...
    • 29 Nov 2015
  • Building a USB UART Serial Adapter

    shabaz
    shabaz
    Introduction This blog post covers a quick project to build-you-own USB Serial Adapter. It can be used for connecting up computers to other computers or microcontrollers. Note: For more modern USB-C circuits, see either  Building a USB-C ...
    • 15 Nov 2015
  • Miracast/WfdSink on Allwinner based SBC

    rzr
    rzr
    WfdSink on Allwinner  We previously shared a demos of our miracast solution running on different flavor of Linux, Buildroot, yocto and Tizen and different architectures (Intel x86, Freescale’s iMX6 …).Today we’re happy to show a working set...
    • 2 Sep 2015
  • 5 gaming projects using the popular ZX Spectrum home computer

    Catwell
    Catwell
    Retro Computers’ ZX Spectrum Vega is based on the UK’s popular microcomputer and can play 40,000 or more games (via indiegogo) If you were alive in any way in the UK during the early 80’s, chances are you were playing games on the popular ZX Spe...
    • 14 Aug 2015
  • Building a Digital PCB Inspection Microscope with the Gizmo 2

    shabaz
    shabaz
    IntroductionMagnifiers and other visual inspection tools are essential with working with small electronics. This blog post does a quick round-up of several low-cost ways to achieve this for hobbyists, and shows how to assemble a digital video microsc...
    • 30 Jul 2015
  • [RPi2] Work in progress! Xbox 360 Arcade Box

    e14 Contributor
    e14 Contributor
    Hey everyone,  I got introduced to the RPi2 at my work, and have been addicted ever since. I have wanted to RGH an Xbox 360 console for a long time, but with 5 failed attempts and thus now bricked or molten consoles I decided to take a diff...
    • 23 Jul 2015
  • Lava Ball

    oneleggedredcow
    oneleggedredcow
    Lava ball is a fairly simple game where you try to keep the ball out of the lava. You move the ball around by tilting the controller and then every so often, the white square moves and you have to make it back to safety before the ground gets too hot...
    • 25 Jun 2015
  • Accelerometer readings over WiFi with the STM32F4 Discovery Board

    oneleggedredcow
    oneleggedredcow
    PrerequisitesSTM32F4 DiscoverySTM32F4 DiscoverySTM32F4 Discovery WiFi BoardSTM32F4 Discovery WiFi BoardUART8000-U CableUART8000-U Cable IntroductionWe are going to use the STM32F4 Discovery BoardSTM32F4 Discovery Board and the STM32F4 Discover W...
    • 21 Jun 2015
  • Nine bucks can net you a CHIP from Next Level Co that can fit in your pocket

    Catwell
    Catwell
    Next Thing Co’s CHIP is a pocket-sized powerhouse that lets you code, play games and everything else a basic PC can do (via the CHIP kickstarter) Small pocket-sized PCs can be found everywhere. Most come in the form of maker tools such as the Ra...
    • 5 Jun 2015
  • Meet Modulo, modular boards created by a Pixar developer

    Catwell
    Catwell
    The new hobbyist modular boards created by Pixar developer Erin Tomson. Hey, Modulo...I still prefer "back in the day." (via Modulo)Pixar Developer, Erin Tomson left her position to found Modulo Labs, a company that is dedicated to taking t...
    • 3 Jun 2015
  • Inexpensive and Reliable: Professional Industrial PCs Based on Thin Mini-ITX SFF

    PRismaPR
    PRismaPR
    Display and panel PCs require highest graphics performance. If they also need to provide control functions, the specifications become even more demanding: High computing performance and extreme reliability are then also required. At the same time, de...
    • 28 Apr 2015
  • Resize an SD Card

    oneleggedredcow
    oneleggedredcow
    Most of the single board computer images out there are set up for a 4GB SD card, but what if you have a 16 GB card?  When you fire up the image and check the disk size with: df -h .Sometimes it reports that the size of the drive is just 4GB...
    • 30 Dec 2014
  • Gizmo 2 – The New Batch

    shabaz
    shabaz
    IntroductionThe Gizmo 2 is an ultra-small computer that fits in the palm of the hand and is the successor to the earlier Gizmo from GizmoSphere. Unlike a lot of single board computers, this one contains a 64-bit CPU (x86-64 compatible - actually an A...
    • 27 Dec 2014
  • ADC on the Odroid

    mconners
    mconners
    One of the biggest features that the ODROID-C1 (odroid, from now on) has that is different than the Raspberry Pi B+ is the ADC. This is a welcome addition and will allow you to interface with analog sensors in a very simple way. I figured I woul...
    • 23 Dec 2014
  • ODroid - Oh Boy!

    mconners
    mconners
    I recently picked up one of these little ODROID C1 development boards and i have to say I couldn't be happier! It's a Quad Core ARM dev board based on the Amlogic S805 Cortex A5 processor with a Dual Core Mali 450 GPU. It comes with 1 GB of RAM ...
    • 23 Dec 2014
  • 'Tis the Season for Inventing and Great Prizes!

    lbittner
    lbittner
    'Tis the Season for Inventing is Here! Submit Your Project Ideas to Win! As visions of inventions dance in your heads, don’t let the costs fill you with dread. Come to element14 instead.  Submit your dream project idea incorporating a Raspb...
    • 25 Nov 2014
<>