Panasonic
  • Products & Partners
  • Manufacturers
  • Panasonic
  • More
  • Cancel
Panasonic
Blog
  • Blog
  • Forum
  • Documents
  • Polls
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Panasonic to participate - click to join for free!

Blog

  • Tags
  • Subscribe by email
  • More
  • Cancel
  • Update on FN Series: Panasonic's latest advancements in Aluminum Electrolytic Capacitors

    riyo@panasonic
    riyo@panasonic
    In the world of passive components, aluminum electrolytic capacitors have been a popular choice due to their impressive capacitance-to-volume ratio, making them ideal for applications where every bit of space counts. They are commonly used for func...
    • 28 Mar 2025
  • Panasonic ensures film capacitor supply, offering alternatives to competitors' EOL announcements

    riyo@panasonic
    riyo@panasonic
    Panasonic Industry is committed to supporting its customers with a comprehensive range of film capacitor solutions, even as certain suppliers announce an "End of Life" for their products. This development has impacted various film capacitor...
    • 21 Feb 2025
  • What is a cooling system pump? Circulating water to prevent equipment overheating

    riyo@panasonic
    riyo@panasonic
    The cooling system pump is responsible for moving water through the cooling system, helping to prevent overheating of various equipment. This pump typically requires between 30 W and 100 W of power to function. It consists of an impeller, a motor, an...
    • 19 Feb 2025
  • The impact of polymer capacitors on advancing GaN-based AC/DC converters

    riyo@panasonic
    riyo@panasonic
    AC/DC converter trends and GaN Different kinds of electronic devices employ AC/DC converters as instrument to transform commercial AC power into DC power. They are necessary since the majority of electrical loads operate on DC rather than AC...
    • 23 Jul 2024
  • Small-scale, diversified but utterly useful: A new roadmap on the variety of Power Inductors

    riyo@panasonic
    riyo@panasonic
    Known as pioneers of metal composite power inductor technology, Panasonic Industry has undoubtedly made a name for itself - but the industries’ rapid developments and increased demands on the specs of passive components wouldn’t allow any...
    • 10 Jul 2024
  • Resolving MLCC Problems by Switching to Conductive Polymer Capacitors

    riyo@panasonic
    riyo@panasonic
    MLCC problems - and their solution  MLCCs (Multi-layered Ceramic Capacitors) are used in a wide variety of applications but have problems due to inherent characteristics of MLCCs. Some of these problems can be solved by adopting conductive polym...
    • 16 May 2024
  • Are Electrolytic Capacitors still a core technology?

    marcom
    marcom
    Despite the emergence of alternative capacitor technologies like hybrids, electrolytic capacitors continue to stand out as the optimal choice across various applications. Their enhanced performance, extended lifespan, and cost-effectiveness solidif...
    • 11 Dec 2023
  • PAN1770 BLE®︎ data throughput rate and metal enclosures: a short test on some facts – and one solution

    marcom
    marcom
    As developers and engineers, you are familiar with the challenges that arise and understand the power when metal enclosures or housings shield or disrupt a decent flow of BLE data throughput. Join us for the following video on a short investigative j...
    • 11 Dec 2023
  • Passive components tailored to Solar Inverters

    marcom
    marcom
    As the world moves towards making more eco-friendly responsible choices, the demand for sustainable and renewable energy has driven consistently high growth in the solar inverter market. A solar inverter (also called a photovoltaic or PV inverter) co...
    • 17 Aug 2023
  • Ready for your ideas – and available on short lead times: Panasonic Industry’s range of BLE modules

    marcom
    marcom
    Despite the tense situation on the semiconductor markets for the past two years, Panasonic Industry has invested heavily in stocks - and now reports that, for instance, the Bluetooth® Low Energy modules from the PAN1780 family are available in ex...
    • 16 Jan 2023
  • Panasonic Industry's GraphiteTIM: Optimizing the thermal path for your power module

    marcom
    marcom
    Everyone knows that heat is a system killer. A general rule of thumb is that the life-time of a device decreases by 50 percent each time when the temperature rises an additional 10 degrees Celsius. To look at it from another angle, the MTBF (meanti...
    • 21 Dec 2022
  • State-of-the-art Smart NIC design: Why Panasonic Industry’s Polymer capacitors are a perfect choice

    marcom
    marcom
    Communications service providers are contributing intensely to large and hyper-scale data centres to deliver data processing, content, and communications services. The applications delivering these services must have access to high-speed storage and ...
    • 14 Dec 2022
  • Polymer Capacitors – a superior alternative for MLCCs in every regard?

    Polymer Capacitors – a superior alternative for MLCCs in every regard?

    moritzcehak
    moritzcehak
    It is not only since the widespread introduction of 5G... ...that the demand for Multilayer Ceramic Chip Capacitors (MLCCs) is growing: Applications in the field of consumer electronics, data processing, telecommunications and many others have not ...
    • 8 Apr 2022
  • Large current SMD Power Inductor for automotive applications - ETQP8M***J** & ETQPAM***JFW

    panasonic_inductors
    panasonic_inductors
    The increasing requirement of performance of automotive devices leads to higher electric current flowing trough electric circuits. Also the number of ECUs mounted on vehicles is gradually increasing. As space inside vehicles is limited, ECU boards mu...
    • 18 Mar 2022
  • 180°C resistance for Panasonic automotive power inductors

    panasonic_inductors
    panasonic_inductors
    180°C specified – What does it really mean? Panasonic Power Inductors are specifically designed for harsh environmental conditions in engine,  transmission, braking systems and powertrain applications. The target was from the beginning...
    • 1 Mar 2022
  • Compact, robust, reliable: Panasonic Industry's power inductors - the coil of choice for demanding automotive applications?

    moritzcehak
    moritzcehak
    When Panasonic started the development of the first metal composite power inductor nearly two decades ago, the key target was to design a product that would be able to withstand severe conditions and provide the highest reliability for automotive...
    • 25 Nov 2021
  • Panasonic Industry’s new ESP32-S2 based PAN9520 Wi-Fi module: a step by step introduction for easy videostreaming

    moritzcehak
    moritzcehak
    Admittedly, Wi-Fi technology is not the latest thing – but it’s still state of the art when it comes to processing higher data rates, especially in personal area networks.Now, Panasonic Industry is breaking new ground with its new PAN9520 wireless mo...
    • 3 Nov 2021
  • It's all about patterns: Insights on stability and resistor laser trimming

    moritzcehak
    moritzcehak
    Far more than constructive or material differences, it is the principle – or more specifically: the pattern – of laser trimming that makes the difference for a SMD chip resistor’s reliability and performance. Let us investigate, why:Resistors - seemi...
    • 3 Nov 2021
  • Some facts on Passives in Smart Metering applications

    moritzcehak
    moritzcehak
    The relevance of smart metering has increased globally during the last couple of years for different applications such as water, gas and electricity – on both the supplier and the consumer side. Additionally, the global shipment of smart meters...
    • 18 Oct 2021
  • The evolution of "small": New video on reliable downsizing with chip resistors

    moritzcehak
    moritzcehak
    Undoubtedly, downsizing is a trend in the electronics industry - watch this latest and comprehensive short video and learn what Panasonic Industry has to offer for resistor downsizing - while ensuring the highest power range in smallest case sizes an...
    • 1 Jul 2021
  • Avoiding fatal contact failures in electronic components: a whitepaper on red phosphorous flame retardants

    moritzcehak
    moritzcehak
    In plastic materials that are flame retardant with red phosphorous, outgassing can occur. This has an impact on electronic components – in relays, for example, it can cause increased contact resistance, and some corrosion phenomena of components...
    • 18 Jun 2021
  • Miniaturized, but great: Panasonic Stacked Metallized Chip Type Film Capacitors - high performance in a small housing

    moritzcehak
    moritzcehak
    Did you know that not all film capacitors are big fellows with two or four legs as you would commonly guess? And also, that besides the well-known PP and PET dielectric there are film capacitors using PPS or PEN as a dielectric material? "T...
    • 18 Jun 2021
  • Many reasons why Panasonic Industry wide terminal resistors suit the downsizing of your applications

    moritzcehak
    moritzcehak
    A higher level of power in smaller parts – this is undoubtedly the overriding direction where the electronic component market is currently heading.  That also applies for resistors, being the smallest and most accessible components in any elect...
    • 18 Jun 2021
  • Technical benefits and cost efficiency for PCB: Panasonic Industry Polymer Capacitors as an alternative to tantalum capacitors

    moritzcehak
    moritzcehak
    Pure tantalum capacitors – also in modern electronics design they stand for extremely high capacitance values for any given volume. But as beneficial as their constructive principle appears - it also reveals pitfalls that make engineers investigate s...
    • 4 May 2021
  • Meeting the needs of tomorrow's mobility: Panasonic Industry Automotive Grade Metallized PP Film Capacitors

    moritzcehak
    moritzcehak
    Doubtlessly, there is a shift towards an entirely new and more environmental-friendly perception of individual mobility. Apparently, we are talking of electric vehicles and the corresponding charging infrastructure. The goals are set – more and more ...
    • 22 Apr 2021
<>