TDK
  • Products & Partners
  • Manufacturers
  • TDK
  • More
  • Cancel
TDK
Documents Documents
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join TDK to participate - click to join for free!
Document Actions
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Related
Recommended
  • Low Voltage Models Added to ZWS300BAF Series

    TDK Corporation introduces the addition of 12V and 15V models to its TDK-Lambda ZWS300BAF series of high reliability power supplies. Operating from a universal input...
    • Revision #1
    • on 8 Oct 2021 7:52 AM
  • The advantages of using a power supply incorporating digital control to power non-linear loads

    I was recently tasked with doing a presentation on the advantages of power supplies incorporating Digital Control to power non-linear loads, so I thought I would share...
    • Revision #1
    • on 8 Oct 2021 7:52 AM
  • Higher Efficiency AC-DC Full-Brick Power Modules Have a Five Year Warranty

    TDK Corporation introduces the TDK-Lambda PFE-SA series of AC-DC full brick power modules, representing a significant upgrade to the popular PFE-S series launched five...
    • Revision #1
    • on 8 Oct 2021 7:52 AM
  • Reducing Switching Power Supply Radiated & Conducted EMI

    One application issue that comes across my desk on a regular basis is where a customer has gone to an outside lab to certify their equipment for EMC, and they have failed...
    • Revision #1
    • on 8 Oct 2021 7:51 AM
  • HWS-A offers significant performance improvements to established HWS

    TDK Corporation announces the introduction of the TDK-Lambda HWS-A series of AC-DC power supplies, comprising of five power levels rated from 15-150W. The HWS-A is a...
    • Revision #1
    • on 8 Oct 2021 7:51 AM
  • “Brute Force” Parallel of Power Supplies

    You will see in many of our instruction manuals a warning about not connecting power supplies in parallel that do not have current share capabilities. At first it would...
    • Revision #1
    • on 8 Oct 2021 7:50 AM
  • Quarter Brick DC-DC Converters have a 200-425VDC Input

    TDK Corporation announces the introduction of the TDK-Lambda PH-A280 series of DC-DC power modules with high voltage DC input. These quarter-brick modules operate from...
    • Revision #1
    • on 8 Oct 2021 7:50 AM
  • What Makes Switching Power Supplies Hiss

    I attended a technical briefing two years ago given by one of our Product Managers on TDK-Lambda’s 400W CFE series, and was shown the various ways the product could potentially...
    • Revision #1
    • on 8 Oct 2021 7:50 AM
  • High Efficiency DIN Rail Mount Power Supplies Feature Compact Sizes

    TDK Corporation announces the introduction of the TDK-Lambda DRB series of DIN rail power supplies for low power applications that require less space on the mounting...
    • Revision #1
    • on 8 Oct 2021 7:49 AM
  • Power Supply Filter Capacitor Values Can Change with the Applied Voltage

    I read an article in one of the publications we advertise in recently where an Engineer had designed a timing circuit, but when he tested it, the frequency was too high...
    • Revision #1
    • on 8 Oct 2021 7:49 AM
  • Applications of DC-DC converters For Base Station RF Power Amplifiers

    When a DC-DC converter is in proximity to the Power Amplifier (PA) in an RF transmitter, regardless of whether it is located at the top or at the base of the antenna...
    • Revision #1
    • on 8 Oct 2021 7:48 AM
  • Compact, Low-Voltage Power Supplies Suit Many Applications

    TDK Corporation announces the extension of the TDK-Lambda GWS500 series power supplies with the addition of two low output voltage models. Combining the same high efficiency...
    • Revision #1
    • on 8 Oct 2021 7:47 AM
  • What Size Heatsink Do I Need?

    Today there are a large array of high power modules in the range of 300 to 1,000-watts, both DC-DC converters as well as AC-DC power modules, which are commonly referred...
    • Revision #1
    • on 8 Oct 2021 7:46 AM
  • New 250W Convection-Cooled Power Supply Features Low Profile, High Efficiency and Wide AC Input Range

    TDK Corporation announces the release of TDK-Lambda's new CUS250LD series low profile AC-DC power supplies. These single-output supplies provide 250-watts of output power...
    • Revision #1
    • on 8 Oct 2021 5:48 AM
  • Power Supply "Remote Sense" Mistakes and Remedies

    Most medium to high power AC-DC power supplies and some DC-DC converters include "Remote Sense" connection points (+ and - Sense) that are used to tightly regulate the...
    • Revision #1
    • on 8 Oct 2021 5:43 AM
  • Ultra Compact 800-Watt Programmable Power Supply Features Advanced Digital Controls

    TDK Corporation announces the expansion of TDK-Lambda's Z+ Series of programmable power supplies, which now includes the new 800-watt models in addition to the previously...
    • Revision #1
    • on 8 Oct 2021 5:34 AM
  • What does SELV mean for Power Supplies?

    SELV stands for S afety E xtra L ow V oltage. Some AC-DC power supply installation manuals contain warnings concerning SELV. For example, there may be a warning about...
    • Revision #1
    • on 8 Oct 2021 5:33 AM
  • New 400W Quarter Brick Converters Feature 95% Efficiency in Standard DOSA Footprint

    TDK Corporation announces the new TDK-Lambda iQG Series of DC-DC converters that are ideal for intermediate or distributed bus power architectures. Featuring a low profile...
    • Revision #1
    • on 8 Oct 2021 5:33 AM
  • Power Supply Rise and Fall Output Characteristics

    A common question asked by our customers is “what are the power supply’s rise and fall output characteristics?” Our usual answer “it depends” sometimes raises an eyebrow...
    • Revision #1
    • on 8 Oct 2021 5:33 AM
  • New 1600 Watt Power Supply Features 92% Efficiency with Digital Controls

    TDK Corporation announces the new TDK-Lambda RFE1600 Series ; a 1600W single-output AC-DC power supply in a low profile package (less than 1U high) for stand alone or...
    • Revision #1
    • on 8 Oct 2021 5:32 AM
>