Raspberry Pi
  • Products & Partners
  • More
Raspberry Pi
Blog SCPI on a Linux Board - Part 5a: LabVIEW Driver for LAB Switch: Open, Close and Switch functions
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
GPIO Pinout
Raspberry Pi Wishlist
Comparison Chart
Quiz
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: Jan Cumps
  • Date Created: 7 Aug 2018 11:31 AM Date Created
  • Views 7964 views
  • Likes 9 likes
  • Comments 21 comments
Related
Recommended
  • piface digital
  • raspberry pi
  • labview
  • scpi
  • diytestinstruch
  • piface

SCPI on a Linux Board - Part 5a: LabVIEW Driver for LAB Switch: Open, Close and Switch functions

Jan Cumps
Jan Cumps
7 Aug 2018

I'm building a SCPI programmable Lab switch with a Raspberry Pi and PiFace Digital.

Communication is over TCP/IP.

In this post: the LabVIEW drivers

image

 

What is this Lab Switch?

 

This is a lab instrument. A switch that can be controlled via commands, over the network.

The switch hardware is a combination of two off-the-shelf components: a Raspberry PiRaspberry Pi and a PiFace DigitalPiFace Digital.

All inputs and outputs of the PiFace Digital are accessable via commands. You can read the inputs and set the outputs. All on the 3V3 logic level.

Two of the outputs are connected to a relay. You can use them to switch in and out signals or devices in your automated lab setup.

 

What is this LabVIEW Driver?

 

The driver is a library of controls that help you to talk to the Lab Switch.

You use these controls in your LabVIEW process flows. They allow you to make a connection, control the hardware, then close the used resources.

The LabVIEW blocks that are finished are the Open and Close block to start and finish communication with the Pi, and the Switch control.

The Read component to retrieve the status of both inputs and outputs is on the todo list.

 

Here's an example that shows how these blocks can fit in a process.

I'm using a GUI here to talk to the instrument, because it's helpful to show visibly that the drivers work.

In an automated flow the inputs will very likely be some logic.

 

image

 

This video shows the example in action:

 

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

 

 

The article builds upon the previous posts. They explain what software needs to run.

You'll need to run the SCPI and Instrument service on your Pi. You can find the sources in previous posts.

(they are not attached I see. I'll do that if there's interest in this subject)

Here are the commands to execute them. No sudo needed on ubuntu.

 

./linux_piface_digital_service_cpp 2223 &
./linux_scpi_socket 2222 2223 &

 

 

Init block

 

image

 

image

 

In this block you set the connection parameters. At runtime, LabVIEW will use these to initiate the communication with your instrument.

It will verify that the ID of the instrument is what's expected (if you switch on the ID Query button).

On exit, you have an active instrument connection (VISA resource in LabVIEW lingo) that can be used to send commands and get info.

 

image

 

The three blocks that are surrounded by a structure have different subflows based on the conditions.

The first block queries the instrument ID if the ID Query is set to true, as shown above.

When you switch  ID Query off, the structure does nothing:

image

The other two conditional blocks perform a reset if requested (not implemented image  because it's todo) and close the instrument connection if any error was thrown while connecting or querying the id.

 

image

 

If you make a GUI for your automation, you typically copy the Visa Name in control and paste it on your flow's screen. Then connect that control to the init block.

For a flow without a GUI, you would put the connection string in a constant or property, then pass it on.

It's not recommended to change the setting in the Init block's GUI itself, because that can be shared across projects and flows.

 

Close block

 

image

This block, typically the last one in a process, nicely closes the instrument resources. It releases the connection.

 

image

I'm not showing the GUI for this one because all inputs are expected to come from the process flow.

 

Switch Control block

 

image

image

This block controls the outputs of the PiFace.

There are controls for Enable and Pin. In your flow, you either copy them to your GUI orfeed them the info from other flow elements.

Like in the other blocks, please do not alter these elements in the Switch Control GUI themselves. It's a shared object.

 

This block will send the requested state and pin number to the Pi. It forms a SCPI command string and shoots that over the network.

A typical string would be like this:

:DIGITAL:OUTPUT0 ON

 

image

 

You can use this block anytime you need to control one of the instrument's outputs.

The outputs 0 and 1 on the PiFace are linked to the two relays on that hat. Very useful to switch in and out some components or circuits in your setup.

 

Example

 

Let's have a look at the example from the begin again.

I've coloured the controls that are copied from the library building blocks orange. The ones added for this flow are in a purple rectangle.

image

 

image

In the beginning of the flow, there's an init block that gets the connection parameters from the GUI element we copied from that init's block GUI.

We then enter a set of while loops that allow us to keep on controlling the process until you check the Exit button.

The values for Enable and Pin are retrieved, and sent to the Switch Control when you press Apply.

If you have the exit check button on, this will also cause the flow to go to the Close block and stop.

As long as you keep that checkbox off, you can keep on controlling the instrument.

Check the video above to see how it works.

 

The LabVIEW library is attached to this post.

 

related blog
SCPI on a Linux Board - Letter of Intent

SCPI on a Linux Board - Part 1: Proof of Concept

SCPI on a Linux Board - Part 2a: PiFace Digital C programming

SCPI on a Linux Board - Part 2b: PiFace Digital C++ programming
SCPI on a Linux Board - Part 3: TCP/IP Socket C++ programming
SCPI on a Linux Board - Part 4: TCP/IP SCPI and Instrument Service
SCPI on a Linux Board - Part 4b: TCP/IP SCPI and Instrument Service 100% Working
SCPI on a Linux Board - Part 4c: TCP/IP SCPI and Instrument Service - Run as a Daemon
SCPI on a Linux Board - Part 5a: LabVIEW Driver for LAB Switch: Open, Close and Switch functions
Attachments:
PiFace.zip
3463.linux_piface_digital_service_cpp.zip
  • Sign in to reply

Top Comments

  • 14rhb
    14rhb over 8 years ago +3
    Hi Jan, You can't beat a good bit of Labview automation and remote interfacing . I'm realling enjoying your series of blogs and am learning along the way also - thank you. I used Labwindows CVI in the…
  • shabaz
    shabaz over 8 years ago +2
    Hi Jan, Awesome project : ) That's a unique demo too! I like how your computer desktop actually becomes a desktop
  • genebren
    genebren over 8 years ago +2
    Hi Jan, Very nicely done. You have developed some great tools and great LabVIEW skills! Gene
  • kabatom
    kabatom over 7 years ago in reply to Jan Cumps

    Thanks for the rapid response!

    linux_piface_digital_service_cpp refuses to run & reports libboost_system.so.1.58.0 is missing and installing libboost doesn't appear to help. Could you provide some insight by any chance?

    The other service starts fine, it just refuses to continue beyond the initial few steps due to obvious reasons image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • Jan Cumps
    Jan Cumps over 7 years ago in reply to kabatom

    kabatom  wrote:

     

    Hey Jan,

    ... Do I need to recompile them on my RBP ...

    The executables are available in previous blog post: SCPI on a Linux Board - Part 4b: TCP/IP SCPI and Instrument Service 100% Working

    There are 2 ZIP files, each of them has a DEBUG folder.

    In that folder you will find a file without extension (it's also the biggest file in that folder). sFTP that over, in binary mode, set the executable flag, and you're ready to go.

     

    I don't compile anything on the RPi. I use ARM's DS-5 development environment, with GCC 5.3.1 Arm Toolchain for linux, on a windows10 laptop.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • Jan Cumps
    Jan Cumps over 7 years ago in reply to kabatom

    I've never written the service wrappers. There was little interest in this blog. You could, since you are looking for something quick, add both executables to the startup script.

     

    As far as I can recall, the code only relies on libraries available in the arm linux compiler. It has no special dependencies. Everything is statically linked (not sure anymore. It's been a while). So no extra install on linux. Just move the binaries over and set the executable flag.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • kabatom
    kabatom over 7 years ago

    Hey Jan,

    I'm currently investigating the possiblitity to use LabVIEW coupled with a RBP 3B and PF2 for an ad-hoc supervising solution. The time I can devote to this is extremely limited, so I'd like to replicate your demo setup and proceed from there on.

    Likely due to having virtually zero experience in linux based systems, I'm having a hard time getting the services on the RBP to run. Do I need to recompile them on my RBP and if so, what additional resorces besides libmcp23s17 and libpifacedigital do I require?

     

    I hope this thread necromancy works.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • jack.chaney56
    jack.chaney56 over 8 years ago in reply to Jan Cumps

    Last bit of code. Not much good without the activity at the end of the nodes I guess.

    UByte ieee_CLS(UByte c)  {
      if ((c == 13)||(c == ';')) {
        stCls(); /* perform the *CLS activity */
      }
      return 0;
    }
    UByte ieee_ESEs(UByte c) {
      if ((c == 13)||(c == ';')) {
        stEseS(parm[0]); c = 0; /* perform the ESE {parm} activity */
        } else {
        c = parsNum(c); /* parse the parameter string
        } return c;
    }
    UByte ieee_ESEq(UByte c) { if ((c == 13)||(c == ';')) { stEseQ(); } return 0; }
    UByte ieee_ESRq(UByte c) { if ((c == 13)||(c == ';')) { stEsrQ(); } return 0; }
    UByte ieee_IDNq(UByte c) { if ((c == 13)||(c == ';')) { stIdnQ(); } return 0; }
    UByte ieee_OPCs(UByte c) { if ((c == 13)||(c == ';')) { stOpcS(parm[0]); c = 0; err = 0; nest = 0; offs = 0; neg = 0; } else { c = parsNum(c); } return c; }
    UByte ieee_OPCq(UByte c) { if ((c == 13)||(c == ';')) { stOpcQ(); } return 0; }
    UByte ieee_RST(UByte c)  { if ((c == 13)||(c == ';')) { stRst(); } return 0; }
    UByte ieee_SREs(UByte c) { if ((c == 13)||(c == ';')) { stSreS(parm[0]); c = 0; err = 0; nest = 0; offs = 0; neg = 0; } else { c = parsNum(c); } return c; }
    UByte ieee_SREq(UByte c) { if ((c == 13)||(c == ';')) { stSreQ(); } return 0; }
    UByte ieee_STBq(UByte c) { if ((c == 13)||(c == ';')) { stStbQ(); } return 0; }
    UByte ieee_TSTq(UByte c) { if ((c == 13)||(c == ';')) { stTstQ(); } return 0; }
    UByte ieee_WAI(UByte c)  { if ((c == 13)||(c == ';')) { stWai(); } return 0; }

    If there are any questions, please let me know

     

    Jack

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
<>