; Farnell i Microchip zapraszają na poranne warsztaty USB Dowiedz się jak dodać łączność USB do swojego kolejnego projektu. Farnell i Microchip zapraszają na szkolenie techniczne dotyczące rozwiązań USB oferowanych przez Microchip. Podczas warsztatów…
USB-"Breakfast"-Workshops mit Microchip 17 Städte in Europa im Mai und Juni 2011 Lernen Sie, wie Sie Ihr nächstes eingebettes Design USB-tauglich gestalten können. Dieser "Breakfast"-Workshop bietet Hard- und Softwareingenieuren die Gelegenheit ihre regionalen…
Microchip USB 'Breakfast' Workshops 17 European Cities during May / June 2011 Learn how to add USB connectivity to your next embedded design. This 'Breakfast' Workshop provides an opportunity for hardware and software engineers to meet with their local…
Les « matinales » USB de Microchip 17 villes européennes courant mai/juin 2011 Apprenez à ajouter la connectivité USB à vos systèmes embarqués Ces séminaires d'une demi-journée, baptisés « matinales », constituent pour les développeurs logiciel et ingénieurs…
Seminarios 'Desayuno' USB de Microchip 17 ciudades europeas durante Mayo / Junio 2011 Aprenda a añadir conectividad USB a su próximo diseño embebido. Este Seminario 'Desayuno' ofrece la oportunidad de que ingenieros de hardware y software se reúnan con…
Ben Heck recently broke down the Sega Genesis and a Super Nintendo to scientifically prove which 16 Bit console was the best . Which console do you think was better?
to
Coordinated Universal Time
Microchip France
Vous souhaitez vous former aux microcontroleurs 16 bits Microchip, à MPLAB et au compilateur C30 ? Vous utilisez les dsPIC et souhaitez implémenter du contrôle de moteur Brushless avec ou sans capteurs dans votre système ? Vous souhaitez implémenter du...
to
Coordinated Universal Time
Microchip France, Immeuble Mac Kinley, 1av. de l'Atlantique, 91976 LES ULIS
Bonjour, Un cursus de formation 16bits (PIC24 et dsPIC) et contrôle moteur Brushless aura lieu du 5/9 au 8/9 au centre de formation de Microchip France. Les formations sont ponctuées d'exercices pratiques avec un poste par participant. A l'issue de la...
Besides having to take a class in Matlab in college, back almost 10 years now. I have never used it for anything. Recently, I have been seeing Matlab being a requirement for new jobs. Is it a language I should learn? What is the benefit of it? And can…
The pursuit of money; what separates the hobbyist and the entrepreneur. Though, sometimes there doesn't seem to be an apparent difference in capital raised between the two, but that is another story. Which side would you align yourself? In this economy…
I happened across an embedded open source speech recognition toolkit in my internet travels recently. The software is compact and efficient enough to fit on small uCs. And after watching the video demonstration, it seems to be fairly accurate.
…
I want to some Bluetooth connected devices, and I have no idea where to begin in designing with this technology. Are there pre-packaged Bluetooth development kits available? Is it difficult to design for from your experience? I am jumping on board long…
IC based brushless 3-phase motor controllers are on the rise, though I am not sure what is available past remote control airplane drive circuitry. I want an IC that has the commutation functions built in, H-bridge built it, and anything above that would…
I am in the urgent need of a Data Logger / Data acquisition module with companion software. One stipulation, I need the software to be comfigurable without programming. What have you used? What's good? I need any and all options. Cabe
I have a bit of an issue. I need to multiply two 16 bit numbers, (2 bytes each). But here is the difficulty, the uC registers are only 8 bits wide, (1 byte). And the uC I am using has no multiply command, so I have to use the shift left & right, add process…
Anyone try anything besides encoders or potentiometers for motion feedback? If so, how did it work out? I want to make a feedback systems, but have found encoders to be too expensive. I want high precision and low cost, like anyone would. I willing to…
Does this happen to you? I work on programs, drawings, spreadsheets, and websites, generating countless files over the years. A lot of which I do for my own personal projects. And as such, I do not have elaborate version control software like I did during…
When it comes to schematic layout, element symbols, wirejump techniques, and other practices inside all the companies I have ever encountered, there seems to be no standards. For example, one fire protection company I worked with had real messy drawings…
During a visit to the ESC expo in Chicago, I stumbled across Microchip's PIC16F707 microcontroller. The next big thing from Microchip, as they told me. The main feature making this particular uC stand out is the mTouch, projected capacitive touch-screen…
I'm sure you all have used circuit simulation software in the past. But, how about motor simulation software. A recent design direction I am taking is farcing me to design custom motors and motor drivers, including stepper, servo, other DC, and AC induction…
Element-14 is a year old. In the short amount of time I've been on the site, I have come to find that it's an invaluable tool to all my design worries. I was so surprised how useful the site became to my work. I once needed a particular enclosure , and…
Several instances in the past I have come across the need for virtual grounds, often in audio and communication situations. Working with datasheets and application notes, on one particular audio design, I could not find anything in their designs that…
I held a job at a company whose product line was designed in the late 1970s. When I came onboard there, they repeatedly told me that all the engineering, up and to that point, was just in redesigning and maintaining the legacy boards. So, for several…