Embedded and Microcontrollers
  • Technologies
  • More
Embedded and Microcontrollers
Blog STM32H7B3I - First Experience with CubeIDE
  • Blog
  • Forum
  • Documents
  • Quiz
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Embedded and Microcontrollers to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: Jan Cumps
  • Date Created: 2 Aug 2020 11:59 AM Date Created
  • Views 8067 views
  • Likes 5 likes
  • Comments 22 comments
  • stm32h7b3i
  • rt
  • stm32h7b3i-dk
Related
Recommended

STM32H7B3I - First Experience with CubeIDE

Jan Cumps
Jan Cumps
2 Aug 2020

I'm selected for the STM32H7B3I-DK -  DISCOVERY KIT.

I have just set up a clean CubeIDE install, and also installed the resource packages for this kit.

Additional I installed TouchGFX and the standalone Cube Programmer.

Versions:

  • STM32CubeIDE Version: 1.4.1
  • GNU for STM32, 7-2018 -q2 update
  • TouchGFX Designer 4.14.0
  • STMCubeProgrammer  2.5.0

 

The kit has arrived, and the first results have been mostly successful, except for graphic projects using TouchGFX.

 

image

 

What works for me:
image A graphical STemWin project. I imported the example in CubeIDE, built it, loaded via STLink and debugged it.

image Out of Box binary downloaded from product page and then upload it via STLink using the STMCube Programmer.

 

image

 

 

image what I can't get to work yet: Compile a ToughGFX (example import or a self-made project) and load it on the board from CubeIDE.

The compilation / build succeeds. The STLink debug session starts but then the firmware load fails.

 

Error in final launch sequence:

Failed to execute MI command:
load D:\\users\\jancu\\STM32CubeIDE\\workspace_1.4.0\\TouchGFX\\STM32CubeIDE\\TouchGFX-STM32H7B3I-DK_OoB-Release\\TouchGFX.elf 

Error message from debugger back end:
Load failed
Failed to execute MI command:
load D:\\users\\jancu\\STM32CubeIDE\\workspace_1.4.0\\TouchGFX\\STM32CubeIDE\\TouchGFX-STM32H7B3I-DK_OoB-Release\\TouchGFX.elf 

Error message from debugger back end:
Load failed
Failed to execute MI command:
load D:\\users\\jancu\\STM32CubeIDE\\workspace_1.4.0\\TouchGFX\\STM32CubeIDE\\TouchGFX-STM32H7B3I-DK_OoB-Release\\TouchGFX.elf 

Error message from debugger back end:
Load failed
Load failed

 

Some investigation to do ...

(solved, see comment below)

 

Related Posts
First Experience with CubeIDE
Create a TouchGFX Project with support for the Designer, CubeIDE and Debugger - Pt 1: Screen Works
Create a TouchGFX Project with support for the Designer, CubeIDE and Debugger - Pt 2: Touch Works
TouchGFX Simple Example: react on a button click
USB, freeRTOS ,Task Notifications and Interrupts
the Development Kit STMod+ Connector and Using UART2
TouchGFX Application Framework: Model, View, Presentation, Message Queue
TouchGFX Application Framework: A Mock GUI - Show Statuses, Switch Screens
TouchGFX Application Framework: MVP and the ModelListener
Write a CubeIDE MX application: Hardware Cryptography with DMA
Attachments:
STM32H7B3I-DK-TGFX-eload.zip
  • Sign in to reply

Top Comments

  • Jan Cumps
    Jan Cumps over 6 years ago in reply to Jan Cumps +3
    I have it working on the CubeIDE too now. I reused a .ioc file from a TouchGFX generated project for this board, and created a new CubeIDE project based on that. Then used the generated hyperlink to load…
  • Jan Cumps
    Jan Cumps over 6 years ago +3
    Yes, got the CubeIDE and debugger integration working with the screen! www.youtube.com/watch
  • jomoenginer
    jomoenginer over 6 years ago +3
    There must be a config file somewhere in TouchGFX to allow for setting the path to STM32CubeProgrammer and such. One option would be to set it in the gcc/Makefile for the project: stm32cubeProgrammer …
Parents
  • ipv1
    ipv1 over 6 years ago

    hi,

    I hav'nt read all the comments so forgive me if I am being redundant. My experience with graphics was that you will hit bottlenecks with the memory available when you put graphics in your projects. Try and limit the res as well as number of files. I am working with an STM32F7 with a different discovery and the optimization will be the death of me.

    for all purposes, select auto generated code wisely and if nothing works, try using a different optimizer setting. I am at the point where I am compiling using a custom make script but setting up things is a bit of a waste. Also I intend to pass this on to a customer who will have developers with 'simpler' minds so I need to package it such that they don't shoot themselves in the foot.

     

    Please also share a blog or video with steps for your final process as it will be helpful. image

    Cheers!

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • ipv1
    ipv1 over 6 years ago

    hi,

    I hav'nt read all the comments so forgive me if I am being redundant. My experience with graphics was that you will hit bottlenecks with the memory available when you put graphics in your projects. Try and limit the res as well as number of files. I am working with an STM32F7 with a different discovery and the optimization will be the death of me.

    for all purposes, select auto generated code wisely and if nothing works, try using a different optimizer setting. I am at the point where I am compiling using a custom make script but setting up things is a bit of a waste. Also I intend to pass this on to a customer who will have developers with 'simpler' minds so I need to package it such that they don't shoot themselves in the foot.

     

    Please also share a blog or video with steps for your final process as it will be helpful. image

    Cheers!

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
Children
  • Jan Cumps
    Jan Cumps over 6 years ago in reply to ipv1

    ipv1  wrote:

     

    hi,

    I hav'nt read all the comments so forgive me if I am being redundant. My experience with graphics was that you will hit bottlenecks with the memory available when you put graphics in your projects. Try and limit the res as well as number of files. I am working with an STM32F7 with a different discovery and the optimization will be the death of me.

    for all purposes, select auto generated code wisely and if nothing works, try using a different optimizer setting. I am at the point where I am compiling using a custom make script but setting up things is a bit of a waste.

    If I put a few graphics without taking measures, I hit a core memory limit very easy.

    But the out of box example has many graphics, high detail. And it runs. They put graphics in dedicated memory areas. I still have to learn that for this controller.

     

    Also I intend to pass this on to a customer who will have developers with 'simpler' minds so I need to package it such that they don't shoot themselves in the foot.

    Hire me image