The e² studio simple blinky project for Road test: Renesas Solution Starter Kit for RX23E-A. Can be used as a start project for new designs.
gcc toolchain
debug (E2 Lite) and release config
Starter Kit board selected
tested
precompile...
I Road Tested the Renesas' RX23E-A starter kit (Road test: Renesas Solution Starter Kit for RX23E-A). Now that the review is done, I can spend some time to go into the details. In this post, I'm checking how the firmware makes a preci...
Time for a first raw ADC test for Road test: Renesas Solution Starter Kit for RX23E-A. This is a first step to check (and learn) the analogue capacities of the RX23E-A.
On the starter kit, I'm using the default firmware and default setup. A...
I compared the results of Renesas' Thermocouple appnote's firmware for the Road test: Renesas Solution Starter Kit for RX23E-A. This is a first step to check (and learn) the analogue capacities of the RX23E-A.
All drawings and schemat...
The thermocouple appnote for Road test: Renesas Solution Starter Kit for RX23E-A comes with example firmware. In combination with the stater kit PC Tool, you get a temperature display. The firmware source is available as an e...
The kit for Road test: Renesas Solution Starter Kit for RX23E-A comes with a Thermocouple. You work with it via a PC application. By default, that application, and the oob firmware, are set up to directly test the delta sigma ADC....
I received the Renesas Solution Starter Kit for RX23E-A, for Road test: Renesas Solution Starter Kit for RX23E-A. In this post: how to get started with the kit and software .
The kit is is configured to work out of box with ...
Table of Contents
Introduction
Timer Modules
Configuring the Timer Peripheral
PWM Code
Example Output
Summary
Introduction
The Renesas RA series of ARM Cortex-M4 microcontrollers have a lot of excellent integrated peripherals. In a previous blog...
Table of Contents
Introduction
LCD Connections
LCD Code
Summary
Introduction
This is a very short blog that simply builds on earlier work: Using Segment LCD and ADC with Renesas RA Microcontrollers
I was interested in finding a large...
Introduction
This blog post discusses how to take segment LCD glass and attach it to ARM Cortex-M series microcontrollers known as the Renesas RA family.
Often projects might connect via I2C or SPI to displays that have on-board LCD controllers, how...
Table of Contents
Introduction
What is it? What can and can’t it do?
Exploring the Board
Connecting the Board
Running the supplied PC Application
Understanding Reports
Capturing and Decoding Reports using Python
Using an Arduino
Putting it a...
Devices, such as a laptop, have an instruction set architecture, and the RISC-V is becoming a new standard. (Image Credit: Enkin_Akyurt/pixabay)
Both the x86 and ARM ISAs (Instruction Set Articheture) are commonly found in varying devices. However, ...
Table of Contents
Introduction
Renesas RA4M1 Overview
Evaluation Board Overview
Pre-Loaded Demo
Software Installation
Building an Example Project
Uploading and Running Code
Setting up a Debug Configuration
Running a Debug Configuration
Creating ...
Do you have any informations or examples how to implement an OP TEE (Trusted Environment Execution) into the microcontroller AVNET Ultra96-v2?
I tried it to build the environment with Peta-Linux, but when I flashed this on the SD Card an booted the S...
(Image Credit: Samsung Display)
The best displays are usually based on their technical specifications and how effectively they can produce visuals. For instance, Samsung uses nanotech in displays to generate rich-filled, vibrant visuals. Samsung'...
Table of Contents
Introduction
Reusing a USB UART Board
Open Collector Outputs
Driver, Configuration Utility and SDK
GPIO Control Software
An Example Application: Pi Pico
Summary
Introduction
It can get really irritating having to press reset or...
Hello there,
I am trying to export my PCB design but the polygon is not visible on the DXF.
This is the altium design:
and here is the DXF export:
I don't understand why the circle is full and why the order is empty.
An illustration of two laser pulses zapping the world’s fastest logic gates. (Image Credit: University of Rochester illustration / Michael Osadciw)
Something new in good old logic gates? Researchers at the University of Rochester recently deve...
An artist's impression of a superconducting computer chip. (Image Credit: TU Delft)
For the first time, scientists at TU Delft developed a one-way superconductor that blocks current flow in one direction while providing zero resistance in the other....
The researchers combined this laser with a 50 gigahertz electro-optic modulator to develop a high-power transmitter. (Image Credit: Second Bay Studios/Harvard SEAS) Researchers at the Harvard John A. Paulson School of Engineering and Applied Scienc...
I used the TI, TMS320F38379D, dual core processor in the form of a low-cost launchpad board that's only about $40. This is part of TI's C2000 flagship Delfino series of MCUs (we used to call them DSPs). The Launchpad board has little more tha...