FPGA
  • Technologies
  • More
FPGA
Blog Arty S7 50 First Power Up and Hardware-Only Blinky
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join FPGA to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: javagoza
  • Date Created: 29 May 2022 6:19 AM Date Created
  • Views 9490 views
  • Likes 9 likes
  • Comments 3 comments
  • 7_ways_to_leave_your_spartan-6
  • 7 Ways to Leave Your Spartan-6
  • xilinx
  • fpga
  • vivado
  • digilent
  • fpga-project
  • spartan-7
  • verilog
  • Spartan_Migration
Related
Recommended

Arty S7 50 First Power Up and Hardware-Only Blinky

javagoza
javagoza
29 May 2022
Arty S7 50 First Power Up and Hardware-Only Blinky

I received the Digilent Arty S7 50  Board for the  7 Ways to Leave Your Spartan-6 FPGA program. In this blog I describe what the first power up of the board is like and then a small tutorial on how to create your first Hardware-Only design.

"7 Ways to Leave Your Spartan-6" related posts
1 Arty S7 50 First Power Up and Hardware-Only Blinky
2 Arty S7 50 First Baremetal Software Project
3 Arty S7 50 Rapid Prototyping - Environmental Monitor
4 Arty S7 50 ArtyBot Pulse Width Modulation (PWM) for Motor Speed Control
5 Arty S7 50 ArtyBot Custom AXI4 Lite IP Peripheral for Sensing Motor Rotational Speed
6 Arty S7 50 ArtyBot How to Store MicroBlaze Program in the Quad-SPI Flash from Vivado
7 Arty S7 50 ArtyBot - Bot Application Framework
8 Arty S7 50 ArtyBot becomes Emubot, an educational robot for young children
9 Arty S7 50 ArtyBot - Color sensing and line follower
10 Arty S7 50 The Spartan-6 Migration Path Game. Learning the Differences Between Spartan-6 and Spartan-7 FPGAs
11 Arty S7 50 ArtyBot ToF Sensor for Obstacle Avoidance. Vivado Hierarchical Blocks
12 "7 Ways to Leave Your Spartan-6 FPGA" program. My summary
13 Arty S7 50 VGA Thermal Imaging Camera

First Power Up

For more info about the board refer to Arty S7 - Digilent Reference

As soon as you plug in the board, a pre-installed bitstream runs. My board has a problem and it only works with usb power, there must be some component damaged and the AD2384 voltage regulator has burned out, see discussion: Arty S7 rev B vs Arty S7 rev E? Somewhat confused. - Forum - FPGA - element14 Community

image

On the back of the board you can see which board revision it is, necessary to be able to check the updated schematic. My board is Revision B

https://digilent.com/reference/_media/reference/programmable-logic/arty-s7/arty_s7_sch-rev_b.pdf

image

The board comes with a bitstream preloaded. You can play with the switches and buttons.

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image


Hardware-Only Blinky Counter Tutorial

This tutorial is based on Getting Started with Vivado for Hardware-Only Designs - Digilent Reference

Install Vivado. I'm using Vivado ML Editions 2021.1 for this demo. I have a very slow ADSL Internet connection and I had Vivado previously installed with that version.

Open Vivado and Create Project

image

Create project

image

Select default part

image

Review Project Summary

image

From Arty S7 - Digilent Reference go to Master XDC Files Repository

image

Download Master XDC files as zip or go to digilent-xdc/Arty-S7-50-Master.xdc at master · Digilent/digilent-xdc · GitHub and copy the lines you need.

image

From Vivado Sources right click over constraints and click on add sources

image

image

You can add the Arty-S7-50-Master.xdc file downloaded from github, then uncomment the lines corresponding to used pins and rename the used ports (in each line, after get_ports) according to the top level signal names in the project or create a new constraints file and edit your configuration.

For clarity I created a new file artys7_50.xdc

image

Edit the new file and copy and rename the ports

image

Configure one clock signal as clk, one switch button as sw and four leds led[0..3]

## Clock Signals
set_property -dict { PACKAGE_PIN F14   IOSTANDARD LVCMOS33 } [get_ports { clk }]; #IO_L13P_T2_MRCC_15 Sch=uclk
create_clock -add -name sys_clk_pin -period 83.333 -waveform {0 41.667} [get_ports { clk }];

## Switches
set_property -dict { PACKAGE_PIN H14   IOSTANDARD LVCMOS33 } [get_ports { sw }]; #IO_L20N_T3_A19_15 Sch=sw[0]

## LEDs
set_property -dict { PACKAGE_PIN E18   IOSTANDARD LVCMOS33 } [get_ports { led[0] }]; #IO_L16N_T2_A27_15 Sch=led[2]
set_property -dict { PACKAGE_PIN F13   IOSTANDARD LVCMOS33 } [get_ports { led[1] }]; #IO_L17P_T2_A26_15 Sch=led[3]
set_property -dict { PACKAGE_PIN E13   IOSTANDARD LVCMOS33 } [get_ports { led[2] }]; #IO_L17N_T2_A25_15 Sch=led[4]
set_property -dict { PACKAGE_PIN H15   IOSTANDARD LVCMOS33 } [get_ports { led[3] }]; #IO_L18P_T2_A24_15 Sch=led[5]


##Configuration options, can be used for all designs
set_property BITSTREAM.CONFIG.CONFIGRATE 50 [current_design]
set_property CONFIG_VOLTAGE 3.3 [current_design]
set_property CFGBVS VCCO [current_design]
set_property BITSTREAM.CONFIG.SPI_BUSWIDTH 4 [current_design]
set_property CONFIG_MODE SPIx4 [current_design]

# SW3 is assigned to a pin M5 in the 1.35v bank. This pin can also be used as
# the VREF for BANK 34. To be able to use this pin as an ordinary I/O the
# following property must be set to enable an internal VREF for BANK 34.
# Since a 1.35v supply is being used the internal reference is set to half that
# value (i.e. 0.675v).
#
set_property INTERNAL_VREF 0.675 [get_iobanks 34]

set_property BITSTREAM.GENERAL.COMPRESS TRUE [current_design]

Create a design source. Again right click over Design Sources and Add Sources, now Add or create design sources

image

Create Source File. Select your preferred Hardware Design Language, HDL. I selected Verilog

And name your file. File location is ok by default.

image

Press ok and finish adding sources

After clicking finish you are asked to define the new Module

Use the same name ports as in your constraints file: clk, sw and led. led is a bus with 4 lines 

image

  • Port Name: This field defines the name of the port and needs to match one of the names you used in your XDC file.
  • Direction: This drop-down menu can be set to input, output, or inout, defining the direction that signals propagate through this port, with respect to your module. Outputs are the signals that your module will be controlling.
  • Bus: This can be checked or not, when checked, this port consists of multiple single bit signals, grouped into a single bus.
  • MSB: The index of the most significant bit of the port, if it is a bus. This option is grayed out for single-bit ports.
  • LSB: The index of the least significant bit of the port, if it is a bus. This option is grayed out for single-bit ports.

Click OK and now you can edit blinky4.v module

image

`timescale 1ns / 1ps

module blinky4(
    input clk,
    output [0:3] led,
    input sw
    );
// reg for counter    
reg [24:0] count = 0;
 
assign led[0] = count[21];
assign led[1] = count[22];
assign led[2] = count[23];
assign led[3] = count[24];
 
always @ (posedge(clk)) count <= count + 1;    
endmodule

Save and run synthesis

After synthesis is completed you'll get a dialog

image

Click OK for running Implementation

When Implementation is completed you're asked again for the next action. Now we select Generate Bitstream

image

Connect your Arty S7 50 board to your PC

Open Hardware Manager

image

or

image

image

Then program device uploading the new bitstream

image

image

You're done. Your blinky counter running:

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

"7 Ways to Leave Your Spartan-6" related posts
1 Arty S7 50 First Power Up and Hardware-Only Blinky
2 Arty S7 50 First Baremetal Software Project
3 Arty S7 50 Rapid Prototyping - Environmental Monitor
4 Arty S7 50 ArtyBot Pulse Width Modulation (PWM) for Motor Speed Control
5 Arty S7 50 ArtyBot Custom AXI4 Lite IP Peripheral for Sensing Motor Rotational Speed
6 Arty S7 50 ArtyBot How to Store MicroBlaze Program in the Quad-SPI Flash from Vivado
7 Arty S7 50 ArtyBot - Bot Application Framework
8 Arty S7 50 ArtyBot becomes Emubot, an educational robot for young children
9 Arty S7 50 ArtyBot - Color sensing and line follower
10 Arty S7 50 The Spartan-6 Migration Path Game. Learning the Differences Between Spartan-6 and Spartan-7 FPGAs
11 Arty S7 50 ArtyBot ToF Sensor for Obstacle Avoidance. Vivado Hierarchical Blocks
12 "7 Ways to Leave Your Spartan-6 FPGA" program. My summary
13 Arty S7 50 VGA Thermal Imaging Camera
  • Sign in to reply
Parents
  • Jan Cumps
    Jan Cumps over 4 years ago

    Your version B of the board needs a jumper to change between USB / external power:

    image

    (also P11 of the PDF you linked.

    On the photo you showed, I couldn't see very well where the jumper J13 is positioned.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • javagoza
    javagoza over 4 years ago in reply to Jan Cumps

    Thanks,  Jan Cumps  

    Yes, I have changed the jumper for external power, but as soon as I connect a battery or a power supply it turns on but it starts to smell burnt and I quickly disconnect it, I think there must be something damaged I'll look at it more calmly. For now: does it work? Yes? don't touch it Smiley

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • javagoza
    javagoza over 4 years ago in reply to Jan Cumps

    Thanks,  Jan Cumps  

    Yes, I have changed the jumper for external power, but as soon as I connect a battery or a power supply it turns on but it starts to smell burnt and I quickly disconnect it, I think there must be something damaged I'll look at it more calmly. For now: does it work? Yes? don't touch it Smiley