FPGA
  • Technologies
  • More
FPGA
Blog Mini Elevator Arty S7 #1 - Introduction
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join FPGA to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: guillengap
  • Date Created: 7 Jun 2022 10:43 PM Date Created
  • Views 2644 views
  • Likes 9 likes
  • Comments 4 comments
  • arty-s7
  • RTL migration
  • MicroBlaze migration
  • xilinx
  • fpga
  • vivado
  • spartan-7
  • Spartan_Migration
Related
Recommended

Mini Elevator Arty S7 #1 - Introduction

guillengap
guillengap
7 Jun 2022

Table of Contents

  • Introduction
  • Getting Started
  • Build and Wiring
  • Programming with Vivado Design Suite
  • Adding the PIR Motion Sensor
  • Experimenting with Automatic Sliding Door
  • Summary

**********************************************************************************************************************

In this project I am going to develop a mini elevator prototype with the Arty S7 board. When I think about this project, I am thinking of people with disabilities because an elevator should not only be useful in an smart building, but also in houses with 2, 3 or 4 floors. In addition, a prototype helps us to carry out several experiments and quickly correct the possible errors that we find, avoiding serious problems in the future and seeing if we are on the right way or not. This will be 3-story mini elevator, and It will be 1 feet tall approx. Here’s how it will works!

image

Approach

The hardest part of figuring this out will the motor and floor detection technique. A real elevator probably uses a huge A/C motor with sensors at each floor location. We certainly could use this approach with a smaller-scale but putting sensors at each floor is a lot of wiring, and we would have concerns about sensitivity and alignment, etc. On the other hand, a stepper motor can be positioned precisel, but we would have to know exactly where we are and how far we have to go to do that.

Fortunately, I know how to use stepper motors and more interestingly, to save their positions in non-volatile memory (EEPROM). So we’ll use the same approach here. This way I will need a PIR Motion Sensor just to enable the elevator movement in the desired position.

The other design concern will be with the elevator call buttons. They need to be lit momentary contact switches, but the lights need to be controllable independently from the button. I will find any suitable solution using the push buttons and LEDS of the Arty S7 board to move up and down the elevator.

My idea is that when the user is inside the elevator cabin, he/she uses a switch to go up or down and when the one passes the hand over the PIR motion sensor the movement starts. When user reaches the destination the elevator will stop automatically. Also, the PIR motion sensor must be placed in a strategic place, for example inside a box or a cylinder, and where only the user can activate it with the hand.

Finally, I will experiment with an automatic sliding door that I will add to the Arty S7 mini elevator. I will explore several solutions to control this sliding door, including adding the CMOD S7 25 board that the sponsor gave me in another challenge.

image

Hardware

  • ARTY S7 50 board,
  • CMOD S7 25 board,
  • Stepper motor 5V,
  • DC motor 5V,
  • L298N driver,
  • L293B driver,
  • PIR Motion Sensor,
  • Battery 5V (2), and
  • Wire.

image

Software

  • VIVADO HLx Editions 2019.1

image

  • Sign in to reply

Top Comments

  • dang74
    dang74 over 4 years ago +1
    Sounds interesting. I look forward to the next blogs.
  • beacon_dave
    beacon_dave over 4 years ago +1
    This project reminds me of one of the elevator models from a Fischertechnik industrial programme back in the 1970's. Pictures of it used to be included in the smaller educational constructor kits for children…
Parents
  • beacon_dave
    beacon_dave over 4 years ago

    This project reminds me of one of the elevator models from a Fischertechnik industrial programme back in the 1970's. Pictures of it used to be included in the smaller educational constructor kits for children to aspire to. Unfortunately the pocket money never went that far... 

    After a bit of searching, I've managed to find some photos:
    https://www.ftcommunity.de/bilderpool/modelle/mechanische-modelle/aufzuge/aufzug-4-etagen/31875/

    Unfortunately there isn't a good photo of the control logic, but you can just make out some of the logic control blocks lower left and you can see some hidden at each floor.

    This YouTuber appears to have made a pretty good attempt at recreating it though and using some of the original logic control blocks of the time:
    https://www.youtube.com/watch?v=vs89aPbv9xM

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • guillengap
    guillengap over 4 years ago in reply to beacon_dave

    Thiat is a very elaborate project with many wires... I think that my project is a toy for children, in fact in my childhood I was a child very creative and curious ... regards

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • guillengap
    guillengap over 4 years ago in reply to beacon_dave

    Thiat is a very elaborate project with many wires... I think that my project is a toy for children, in fact in my childhood I was a child very creative and curious ... regards