FPGA
  • Technologies
  • More
FPGA
Blog XuLA2 FPGA - PWM with Dead Band in VHDL
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join FPGA to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: Jan Cumps
  • Date Created: 3 Feb 2017 2:39 PM Date Created
  • Views 4375 views
  • Likes 6 likes
  • Comments 8 comments
  • pwm
  • fpga
  • xula2
  • vhdl
  • dead_time
  • jcxula2
Related
Recommended

XuLA2 FPGA - PWM with Dead Band in VHDL

Jan Cumps
Jan Cumps
3 Feb 2017

A PWM module for FPGAs that supports dead band.

image

A VHDL project that generates two opposite PWM signals with a dead band. You can change the duty cycle with a rotary encoder.


When you drive half-bridge designs, you need a control signal for both transistors in the circuit.

These signals need to be each other's opposite, because you close one transistor when you drive the other.

At the switching time, you introduce a tiny bit of dead time, to allow one transistor to properly shut before the other opens.

If you don't allow for this stabilisation period, your transistors will get hot and the magic smoke will eventually (sooner rather than later) escape.

 

I've made a VHDL module that generates these complementary signals, including a configurable deadband.

You decide in your design what the frequency and deadband is.

You can then freely change the duty cycle. The FPGA takes care that the dead time is guaranteed.

 

PWM VHDL module

 

My design is 100% based on the Xess XuLA2 PWM library. I've added the complementary signal and introduced that delay for rising edges of both outputs.

 

entity PwmDeadBand is
  port (
    clk_i  : in  std_logic;             -- Input clock.
    duty_i : in  std_logic_vector;      -- Duty-cycle input.
    band_i : in  natural;               -- number of clock-ticks to keep both signals low before rising edge
    pwmA_o  : out std_logic;            -- PWM output.
    pwmB_o  : out std_logic             -- PWM output inverse.
    );
end entity;

 

duty_i is a register that holds the desired duty cycle. It's configurable - I've set it to 8 bits.

 

Your clock speed is dependent on the size of this register.

The clock that you present on the clk_i input of the module will be divided by 2^(number of bits). In this case, 2^8 -> 256.

For the standard 12 MHz clock of the XuLA2, the PWM module will beat at 47 kHz.

There are ways to increase the clock frequency in the FPGA and the XuLA2 libs have support for that.

 

The dead band, in clock ticks, is passed via the band_i pin. The two complementary signals appear on pwmA_o and pwmB_o.

In the constraint file of your project, you assign that to physical Spartan-6 pins:

 

# PM1 connections for the pwm outputs
net pwmA_o      loc=m16;
net pwmB_o      loc=k16;

 

If you use a StickIt! motherboard, you get the signals at PM1, pin D4 and D6.

image

If you tap them from the XuLA2 directly, they are chan4 and chan6 on the expansion header.

image

 

The implementation is just an extension of what the original Xess library does.

We introduce an additional channel that's HI when the other is LO,, and vice versa.

And we hold off driving any of these channels high until we've waited duty_i clock ticks.

 

architecture arch of PwmDeadBand is
  constant MAX_DUTY_C : std_logic_vector(duty_i'range) := (duty_i'range => ONE);
  signal timer_r      : natural range 0 to 2**duty_i'length-1;

begin

  process(clk_i)
  begin
    if rising_edge(clk_i) then
    
      pwmA_o   <= LO;

      timer_r <= timer_r + 1;
      if timer_r >= band_i + TO_INTEGER(unsigned(duty_i)) then
  pwmB_o <= HI;
  end if;

      if timer_r < TO_INTEGER(unsigned(duty_i)) then
        pwmB_o <= LO;
        if timer_r >= band_i  then
  pwmA_o <= HI;
   end if;
      end if;
    end if;
  end process;
  
end architecture;

 

That's really all for the PWM module. (afterthought in 2021: the line 02 may not be needed. MAX_DUTY_C is not used and the timer naturally iterates from 0 to maximum in this design)

 

Rotary Encoder module

 

This section is very short: read the previous blog post.

 

Patching it together

 

Also easy. We just have to wire the register that holds the value of the Rotary Encoder to the one that's driving the PWM module.

I just use the same register. That's the simplest way to do this.

 

 

entity Rotary_Pwm is
    Port ( clk_i : in  STD_LOGIC;
           rotEncA_i   : in  std_logic;        -- Rotary encoder phase 1 output.
           rotEncB_i   : in  std_logic;        -- Rotary encoder phase 2 output.
           pwmA_o      : out  STD_LOGIC;
           pwmB_o      : out  STD_LOGIC  
   );
end Rotary_Pwm;

architecture Behavioral of Rotary_Pwm is

  signal accumulator_s : std_logic_vector(7 downto 0) := "01111111"; -- 50%

begin

  u0 : PwmDeadBand
    port map (
      clk_i => clk_i,
  duty_i => accumulator_s,
  band_i => 16,
      pwmA_o => pwmA_o,
      pwmB_o => pwmB_o
      );

  u1 : RotaryEncoderWithCounter
    generic map (ALLOW_ROLLOVER_G => true, INITIAL_CNT_G => 127)
    port map (
      clk_i => clk_i,
      a_i   => rotEncA_i,
      b_i   => rotEncB_i,
      cnt_o => accumulator_s
      );

end Behavioral;

 

So the handover point is the 8-bit register accumulator_s. When you turn the encoder, it changes the value of the register to reflect your action.

In real-time, the duty cycle of the PWM module adapts. There's not a single clock tick between event and action.

 

Connections

 

image

I've used PM1 on the StickIt! motherboard, and used these pins:

 

 

PM1 pin
XuLA2 pin
Spartan-6 pinpin namedirectionfunction
6 - +3V3+3.3V+3.3Voutpull-up power for encoder
5 - GNDGNDGNDoutground for PWM and Rotary Encoder
4 - D6CHAN6K16pwmB_ooutPWM complementary signal B
3 - D4CHAN4M16pwmA_ooutPWM complementary signal A
2 - D2CHAN2R16rotEncB_iinRotary Encoder pin B
1 - D0CHAN0R7rotEncA_iinRotary Encoder pin A

 

If you want to wire the encoder inputs or pwm outputs to other pins, you only have to change the constraint file.

 

 

image

 

The project is attached, together with the PWM library.

I'm going to use this to drive my GaN experiment board. You?

 

XuLA2 FPGA - First Impressions of the Development Tools
XuLA2 FPGA - SD Card Read and Write
XuLA2 FPGA - Rotary Encoder and VHDL
XuLA2 FPGA - PWM with Dead Band in VHDL
XuLA2 FPGA - Up the Clock
XuLA2 FPGA - Utility to Generate Pin Assignments
XuLA2 FPGA - Test the VGA StickIt! Module: Image Preparation
Attachments:
Rotary_Pwm.zip
  • Sign in to reply

Top Comments

  • michaelkellett
    michaelkellett over 9 years ago in reply to clem57 +2
    If you want a quick and dirty metric to compare FPGAs the best one is probably to compare the number of look up tables. This is because most FPGAs use logic cells where the core thing that does the work…
  • clem57
    clem57 over 9 years ago +1
    Just wondering can this be handled by an Arduino since the duty cycle time is 47 KHz and you use a PLC of 12 Mhz?
  • clem57
    clem57 over 9 years ago in reply to clem57 +1
    Unfortunately, there is no clear answer to your question. A Logic Cell consists of a look-up tables and a flip-flop. A flip=flop with clear is worth about 6 or 7 gates in the ASIC world. A look-up table…
Parents
  • clem57
    clem57 over 9 years ago

    Just wondering can this be handled by an Arduino since the  duty cycle time is 47 KHz and you use a PLC of 12 Mhz?

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • Jan Cumps
    Jan Cumps over 9 years ago in reply to clem57

    An arduino can handle the 47 kHz requirement, Clem. (the 47 kHz is not a real requirement. It happens to be the frequency you get when the clock is 12 MHz and you have an 8-bit duty cycle control - 12000000/2^8)

    But not the 1 MHz PWM frequency requirement with granularity of 4ns for deadband and 256 duty cycle steps that I need for a design I'm working on (see XuLA2 FPGA - Up the Clock).

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • Jan Cumps
    Jan Cumps over 9 years ago in reply to clem57

    An arduino can handle the 47 kHz requirement, Clem. (the 47 kHz is not a real requirement. It happens to be the frequency you get when the clock is 12 MHz and you have an 8-bit duty cycle control - 12000000/2^8)

    But not the 1 MHz PWM frequency requirement with granularity of 4ns for deadband and 256 duty cycle steps that I need for a design I'm working on (see XuLA2 FPGA - Up the Clock).