FPGA
  • Technologies
  • More
FPGA
Blog XuLA2 FPGA - PWM with Dead Band in VHDL
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join FPGA to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: Jan Cumps
  • Date Created: 3 Feb 2017 2:39 PM Date Created
  • Views 4366 views
  • Likes 6 likes
  • Comments 8 comments
  • pwm
  • fpga
  • xula2
  • vhdl
  • dead_time
  • jcxula2
Related
Recommended

XuLA2 FPGA - PWM with Dead Band in VHDL

Jan Cumps
Jan Cumps
3 Feb 2017

A PWM module for FPGAs that supports dead band.

image

A VHDL project that generates two opposite PWM signals with a dead band. You can change the duty cycle with a rotary encoder.


When you drive half-bridge designs, you need a control signal for both transistors in the circuit.

These signals need to be each other's opposite, because you close one transistor when you drive the other.

At the switching time, you introduce a tiny bit of dead time, to allow one transistor to properly shut before the other opens.

If you don't allow for this stabilisation period, your transistors will get hot and the magic smoke will eventually (sooner rather than later) escape.

 

I've made a VHDL module that generates these complementary signals, including a configurable deadband.

You decide in your design what the frequency and deadband is.

You can then freely change the duty cycle. The FPGA takes care that the dead time is guaranteed.

 

PWM VHDL module

 

My design is 100% based on the Xess XuLA2 PWM library. I've added the complementary signal and introduced that delay for rising edges of both outputs.

 

entity PwmDeadBand is
  port (
    clk_i  : in  std_logic;             -- Input clock.
    duty_i : in  std_logic_vector;      -- Duty-cycle input.
    band_i : in  natural;               -- number of clock-ticks to keep both signals low before rising edge
    pwmA_o  : out std_logic;            -- PWM output.
    pwmB_o  : out std_logic             -- PWM output inverse.
    );
end entity;

 

duty_i is a register that holds the desired duty cycle. It's configurable - I've set it to 8 bits.

 

Your clock speed is dependent on the size of this register.

The clock that you present on the clk_i input of the module will be divided by 2^(number of bits). In this case, 2^8 -> 256.

For the standard 12 MHz clock of the XuLA2, the PWM module will beat at 47 kHz.

There are ways to increase the clock frequency in the FPGA and the XuLA2 libs have support for that.

 

The dead band, in clock ticks, is passed via the band_i pin. The two complementary signals appear on pwmA_o and pwmB_o.

In the constraint file of your project, you assign that to physical Spartan-6 pins:

 

# PM1 connections for the pwm outputs
net pwmA_o      loc=m16;
net pwmB_o      loc=k16;

 

If you use a StickIt! motherboard, you get the signals at PM1, pin D4 and D6.

image

If you tap them from the XuLA2 directly, they are chan4 and chan6 on the expansion header.

image

 

The implementation is just an extension of what the original Xess library does.

We introduce an additional channel that's HI when the other is LO,, and vice versa.

And we hold off driving any of these channels high until we've waited duty_i clock ticks.

 

architecture arch of PwmDeadBand is
  constant MAX_DUTY_C : std_logic_vector(duty_i'range) := (duty_i'range => ONE);
  signal timer_r      : natural range 0 to 2**duty_i'length-1;

begin

  process(clk_i)
  begin
    if rising_edge(clk_i) then
    
      pwmA_o   <= LO;

      timer_r <= timer_r + 1;
      if timer_r >= band_i + TO_INTEGER(unsigned(duty_i)) then
  pwmB_o <= HI;
  end if;

      if timer_r < TO_INTEGER(unsigned(duty_i)) then
        pwmB_o <= LO;
        if timer_r >= band_i  then
  pwmA_o <= HI;
   end if;
      end if;
    end if;
  end process;
  
end architecture;

 

That's really all for the PWM module. (afterthought in 2021: the line 02 may not be needed. MAX_DUTY_C is not used and the timer naturally iterates from 0 to maximum in this design)

 

Rotary Encoder module

 

This section is very short: read the previous blog post.

 

Patching it together

 

Also easy. We just have to wire the register that holds the value of the Rotary Encoder to the one that's driving the PWM module.

I just use the same register. That's the simplest way to do this.

 

 

entity Rotary_Pwm is
    Port ( clk_i : in  STD_LOGIC;
           rotEncA_i   : in  std_logic;        -- Rotary encoder phase 1 output.
           rotEncB_i   : in  std_logic;        -- Rotary encoder phase 2 output.
           pwmA_o      : out  STD_LOGIC;
           pwmB_o      : out  STD_LOGIC  
   );
end Rotary_Pwm;

architecture Behavioral of Rotary_Pwm is

  signal accumulator_s : std_logic_vector(7 downto 0) := "01111111"; -- 50%

begin

  u0 : PwmDeadBand
    port map (
      clk_i => clk_i,
  duty_i => accumulator_s,
  band_i => 16,
      pwmA_o => pwmA_o,
      pwmB_o => pwmB_o
      );

  u1 : RotaryEncoderWithCounter
    generic map (ALLOW_ROLLOVER_G => true, INITIAL_CNT_G => 127)
    port map (
      clk_i => clk_i,
      a_i   => rotEncA_i,
      b_i   => rotEncB_i,
      cnt_o => accumulator_s
      );

end Behavioral;

 

So the handover point is the 8-bit register accumulator_s. When you turn the encoder, it changes the value of the register to reflect your action.

In real-time, the duty cycle of the PWM module adapts. There's not a single clock tick between event and action.

 

Connections

 

image

I've used PM1 on the StickIt! motherboard, and used these pins:

 

 

PM1 pin
XuLA2 pin
Spartan-6 pinpin namedirectionfunction
6 - +3V3+3.3V+3.3Voutpull-up power for encoder
5 - GNDGNDGNDoutground for PWM and Rotary Encoder
4 - D6CHAN6K16pwmB_ooutPWM complementary signal B
3 - D4CHAN4M16pwmA_ooutPWM complementary signal A
2 - D2CHAN2R16rotEncB_iinRotary Encoder pin B
1 - D0CHAN0R7rotEncA_iinRotary Encoder pin A

 

If you want to wire the encoder inputs or pwm outputs to other pins, you only have to change the constraint file.

 

 

image

 

The project is attached, together with the PWM library.

I'm going to use this to drive my GaN experiment board. You?

 

XuLA2 FPGA - First Impressions of the Development Tools
XuLA2 FPGA - SD Card Read and Write
XuLA2 FPGA - Rotary Encoder and VHDL
XuLA2 FPGA - PWM with Dead Band in VHDL
XuLA2 FPGA - Up the Clock
XuLA2 FPGA - Utility to Generate Pin Assignments
XuLA2 FPGA - Test the VGA StickIt! Module: Image Preparation
Attachments:
Rotary_Pwm.zip
  • Sign in to reply

Top Comments

  • michaelkellett
    michaelkellett over 9 years ago in reply to clem57 +2
    If you want a quick and dirty metric to compare FPGAs the best one is probably to compare the number of look up tables. This is because most FPGAs use logic cells where the core thing that does the work…
  • clem57
    clem57 over 9 years ago +1
    Just wondering can this be handled by an Arduino since the duty cycle time is 47 KHz and you use a PLC of 12 Mhz?
  • clem57
    clem57 over 9 years ago in reply to clem57 +1
    Unfortunately, there is no clear answer to your question. A Logic Cell consists of a look-up tables and a flip-flop. A flip=flop with clear is worth about 6 or 7 gates in the ASIC world. A look-up table…
  • Jan Cumps
    Jan Cumps over 5 years ago

    The same code as above, on the Pynq-Z2. Rotary replaced by values coming out of the Zynq ARM cores.

    The VHDL design and bitstream build is done in Vivado

    image

    4: the ARM cores

    3: the PWM design of XESS, with the same modifications as in the blog above to get complimentary outputs and dead time generation.

    the 125 MHz clock is directly sent to the PWM. Output frequency is dependent on the precision (bit length) of duty_i.

     

    1: a slice to take 8 bits for duty_i out of the ARM 64 bit output bus

    2: a slice to take 4 bits for band_i out of the ARM 64 bit output bus

     

    The adapted VHDL (check here for original):

    --**********************************************************************
    -- Copyright (c) 2011-2014 by XESS Corp <http://www.xess.com>.
    -- All rights reserved.
    --
    -- This library is free software; you can redistribute it and/or
    -- modify it under the terms of the GNU Lesser General Public
    -- License as published by the Free Software Foundation; either
    -- version 3.0 of the License, or (at your option) any later version.
    -- 
    -- This library is distributed in the hope that it will be useful,
    -- but WITHOUT ANY WARRANTY; without even the implied warranty of
    -- MERCHANTABILITY or FITNESS FOR A PARTICULAR PURPOSE.  See the GNU
    -- Lesser General Public License for more details.
    -- 
    -- You should have received a copy of the GNU Lesser General Public
    -- License along with this library.  If not, see 
    -- <http://www.gnu.org/licenses/>.
    --**********************************************************************
    
    --*********************************************************************
    -- Modules for generating repetitive or single pulses.
    --*********************************************************************
    library IEEE;
    use IEEE.std_logic_1164.all;
    
    package PulsePckg is
    
      constant HI   : std_logic := '1';
      constant LO   : std_logic := '0';
      constant ONE  : std_logic := '1';
    
    --*********************************************************************
    -- PWM module.
    --*********************************************************************
      component Pwm is
        port (
          clk_i  : in  std_logic;           -- Input clock.
          duty_i : in  std_logic_vector;    -- Duty-cycle input.
          band_i : in  std_logic_vector;    -- number of clock-ticks to keep both signals low before rising edge
          pwmA_o  : out std_logic;          -- PWM output.
          pwmB_o  : out std_logic           -- PWM output inverse.
          );
      end component;
    
    end package;
    
    
    --*********************************************************************
    -- PWM module.
    --*********************************************************************
    
    library IEEE, UNISIM;
    use IEEE.MATH_REAL.all;
    use IEEE.std_logic_1164.all;
    use IEEE.numeric_std.all;
    use UNISIM.vcomponents.all;
    use WORK.PulsePckg.all;
    
    entity Pwm is
      port (
        clk_i  : in  std_logic;             -- Input clock.
        duty_i : in  std_logic_vector (7 downto 0);      -- Duty-cycle input.
        band_i : in  std_logic_vector (3 downto 0);      -- number of clock-ticks to keep both signals low before rising edge
        pwmA_o  : out std_logic;            -- PWM output.
        pwmB_o  : out std_logic             -- PWM output inverse.
        );
    end entity;
    
    architecture arch of Pwm is
      constant MAX_DUTY_C : std_logic_vector(duty_i'range) := (duty_i'range => ONE);
      signal timer_r      : natural range 0 to 2**duty_i'length-1;
    begin
    
      process(clk_i)
      begin
        if rising_edge(clk_i) then
    
          pwmA_o   <= LO;
    
          timer_r <= timer_r + 1;
          if timer_r >= unsigned(band_i) + unsigned(duty_i) then
    pwmB_o <= HI;
    end if;
    
          if timer_r < unsigned(duty_i) then
            pwmB_o <= LO;
            if timer_r >= unsigned(band_i)  then
    pwmA_o <= HI;
      end if;
          end if;
        end if;
      end process;
      
    end architecture;

     

    The Jupyter book, loading the bitstream and preparing the bits for duty_i and band_i:

    image

     

    Setting the values for 50% duty, 7 clock ticks dead time:

    image

    Result:

    image

     

    Customer action photo:

    image

     

    Detailed post: Learning Xilinx Zynq: port a Spartan 6 PWM example to Pynq

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • michaelkellett
    michaelkellett over 9 years ago in reply to clem57

    If you want a quick and dirty metric to compare FPGAs the best one is probably to compare the number of look up tables. This is because most FPGAs use logic cells where the core thing that does the work is a look up table bound up with a flip flop. Each logic cell may contain one or more such pairs as well as some other stuff. This sort of works, but not very well between different families of parts,because, for example, Lattice FPGAs use 4 input LUTs but Xilinx use 6. Lattice logic cells can't do the clever tricks Peter Alfke describes for the X parts.

     

    Then there are a whole load of other things like DSP blocks (multipliers and adders) some FPGAs have none, or three, or 800 ! If you do no multiplication they make no difference at all - but if you do .........

     

    If you look up X's MicroBlaze and A's Nios soft processors you can see how much of an FPGA they will use - this might give you a better idea of the capability of the FPGA.

     

    If you want to build a computer (for real) you don't do it with NAND gates - pick a higher level of abstraction like VHDL (or Verilog if you must but you'll never get what the hardware is doing if you do !!image) - a VHDL design could be synthesised to run on an FPGA or an ASIC (although in real life you need to know where it will run to make it anything like optimum).

     

    Currently I'm working on a design using a Lattice iCE5LP4k part with 3.5k LUts, at a glance you can tell it's just a baby compared with my other current project using a Xilinx Artix XC7S100 with 102k logic cells.

     

    The Xlinx logic cell is way more complex than the  iCE. X have  a nice long document to describe it: 

    http://www.xilinx.com/support/documentation/user_guides/ug474_7Series_CLB.pdf

     

    So I reckon when you take speed and other stuff into account the 100k Artix is probably 1000x more capable - and it probably uses 1000x the power as well !

     

     

     

    MK

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • clem57
    clem57 over 9 years ago in reply to clem57

    Unfortunately, there is no clear answer to your question.

    A Logic Cell consists of a look-up tables and a flip-flop.

     

    A flip=flop with clear is worth about 6 or 7 gates in the ASIC world.

    A look-up table may be used to be an inverter ( barely 1 gate) or it can implement a complicated function, like a parity checker, in which (extreme) case it would be worth over 20 gates (in ASIC terminology).

    The LUT might also form a 64-bit RAM, which means 64 latches plus address decoder, which adds up to well over 100 gates, or it could be used as a 32-bit shift register (4 gates per register bit) which equals 128 gates.

    We also normalize the Logic cell count, by assigning each 6-input LUT plus flip-flop the equivalence of 1.6 logic cells...

    You see, your simple question has a very convoluted answer, and we really like to sidestep this question.

    Gate count is a ASIC metric, Logic Cells are FPGA metrics, either method is meaningful only in its world.

    There is no translation table.

    Peter Alfke, Xilinx Applications

    I think I found the answer -> no clear answer               Image131.png

     

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • Jan Cumps
    Jan Cumps over 9 years ago in reply to clem57

    C-3PO (Clem) wrote:

     

    A little off subject: How many NAND gates can I implement on this FPGA (approximate if large).

    ...

    According to the Xess product page, the Xilinx Spartan-6 XC6SLX25  that's used has  24051 logic cells.

    I'm so not versed into this that I'm going to pull in johnbeetem and michaelkellett - the expert team.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • clem57
    clem57 over 9 years ago

    A little off subject: How many NAND gates can I implement on this FPGA (approximate if large). Currently I am taking course online and we are studying how to build a computer.

    Clem

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
>