Test & Tools
  • Technologies
  • More
Test & Tools
Blog SCPI on a Linux Board - Letter of Intent
  • Blog
  • Forum
  • Documents
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Test & Tools to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: Jan Cumps
  • Date Created: 27 Apr 2018 5:41 PM Date Created
  • Views 5948 views
  • Likes 14 likes
  • Comments 21 comments
  • pi
  • bbb
  • BeagleBone
  • raspberrypi
  • scpi
Related
Recommended

SCPI on a Linux Board - Letter of Intent

Jan Cumps
Jan Cumps
27 Apr 2018

I'm trying to build a SCPI shell for Linux.

I'd like to have it working over TCP/IP on a Raspberry Pi and a BeagleBone.

 

tl;dr It works. The rest of the blog series explains how to build a lab automation device that controls 8 outputs (2 of them relays), and read 8 inputs. With a Raspberry Pi and a PiFace Digital (2).

image

 

 

Here on element14, we've been playing with SCPI and microcontrollers. We have several instruments working on MSP432, Arduino and Hercules devices.

This time I'd like to get a Linux instrument up. To get some device independence, I'll try to make the source work on two different boards with different distros.

The program is expected to run as a background process.

 

I have a head start. My favourite SCPI library has a LwIP SCPI server example.

A relative head start, that is, because I have to find out how to get all the dependencies - I want to develop on a Windows PC image.

If this project fails, it'll be because of my develop for Linux skills.

 

related blog
SCPI on a Linux Board - Letter of Intent

SCPI on a Linux Board - Part 1: Proof of Concept

SCPI on a Linux Board - Part 2a: PiFace Digital C programming

SCPI on a Linux Board - Part 2b: PiFace Digital C++ programming
SCPI on a Linux Board - Part 3: TCP/IP Socket C++ programming
SCPI on a Linux Board - Part 4: TCP/IP SCPI and Instrument Service
SCPI on a Linux Board - Part 4b: TCP/IP SCPI and Instrument Service 100% Working
SCPI on a Linux Board - Part 4c: TCP/IP SCPI and Instrument Service - Run as a Daemon
SCPI on a Linux Board - Part 5a: LabVIEW Driver for LAB Switch: Open, Close and Switch functions
  • Sign in to reply

Top Comments

  • Jan Cumps
    Jan Cumps over 8 years ago in reply to Jan Cumps +4
    Yay! It works. Above is the capture of a LabVIEW back and forth communication - with the Raspberry Pi as a VISA TCP/IP device. *IDN? command sent, and the reply from the Pi arrived at LabVIEW.
  • DAB
    DAB over 8 years ago +3
    Good luck Jan. DAB
  • Jan Cumps
    Jan Cumps over 8 years ago in reply to Jan Cumps +3
    what's not working ok: even though I get a reply, the Visa Read block in LabVIEW throws a timeout error. when I close a connection (regardless of telnet, LabVIEW), the service on the Raspberry Pi goes…
Parents
  • Jan Cumps
    Jan Cumps over 8 years ago

    TCP/IP basics work on Raspberry Pi.

    Compiled and debugged in Eclipse on a Windows 10 PC, compiled program executed on the Pi:

    image

     

    Inspiration: http://www.cs.rpi.edu/~moorthy/Courses/os98/Pgms/server.c

     

    This may not look spectacular, but I think it's cool that you can compile a C executable on a windows machine, transfer it to the Pi and step through the code in the debugger on that same windows machine - with 1 click on some button

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • Jan Cumps
    Jan Cumps over 8 years ago

    TCP/IP basics work on Raspberry Pi.

    Compiled and debugged in Eclipse on a Windows 10 PC, compiled program executed on the Pi:

    image

     

    Inspiration: http://www.cs.rpi.edu/~moorthy/Courses/os98/Pgms/server.c

     

    This may not look spectacular, but I think it's cool that you can compile a C executable on a windows machine, transfer it to the Pi and step through the code in the debugger on that same windows machine - with 1 click on some button

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
Children
  • Jan Cumps
    Jan Cumps over 8 years ago in reply to Jan Cumps

    for the geeks (i.e.: me):

     

    image

     

    from a raw telnet console on a linux pc in the network, the payload 'test' is sent to the Pi on port 2222.

    In Eclipse debugger on Windows, this is captured and logged ("Here is the message: test" ).

    On the telnet that sent the message, a confirmation is received ("I got your message").

     

    That's all I need to get a SCPI communication shell. Now over to getting it executed as a daemon ...