Test & Tools
  • Technologies
  • More
Test & Tools
Blog SCPI on a Linux Board - Letter of Intent
  • Blog
  • Forum
  • Documents
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Test & Tools to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: Jan Cumps
  • Date Created: 27 Apr 2018 5:41 PM Date Created
  • Views 5937 views
  • Likes 14 likes
  • Comments 21 comments
  • pi
  • bbb
  • BeagleBone
  • raspberrypi
  • scpi
Related
Recommended

SCPI on a Linux Board - Letter of Intent

Jan Cumps
Jan Cumps
27 Apr 2018

I'm trying to build a SCPI shell for Linux.

I'd like to have it working over TCP/IP on a Raspberry Pi and a BeagleBone.

 

tl;dr It works. The rest of the blog series explains how to build a lab automation device that controls 8 outputs (2 of them relays), and read 8 inputs. With a Raspberry Pi and a PiFace Digital (2).

image

 

 

Here on element14, we've been playing with SCPI and microcontrollers. We have several instruments working on MSP432, Arduino and Hercules devices.

This time I'd like to get a Linux instrument up. To get some device independence, I'll try to make the source work on two different boards with different distros.

The program is expected to run as a background process.

 

I have a head start. My favourite SCPI library has a LwIP SCPI server example.

A relative head start, that is, because I have to find out how to get all the dependencies - I want to develop on a Windows PC image.

If this project fails, it'll be because of my develop for Linux skills.

 

related blog
SCPI on a Linux Board - Letter of Intent

SCPI on a Linux Board - Part 1: Proof of Concept

SCPI on a Linux Board - Part 2a: PiFace Digital C programming

SCPI on a Linux Board - Part 2b: PiFace Digital C++ programming
SCPI on a Linux Board - Part 3: TCP/IP Socket C++ programming
SCPI on a Linux Board - Part 4: TCP/IP SCPI and Instrument Service
SCPI on a Linux Board - Part 4b: TCP/IP SCPI and Instrument Service 100% Working
SCPI on a Linux Board - Part 4c: TCP/IP SCPI and Instrument Service - Run as a Daemon
SCPI on a Linux Board - Part 5a: LabVIEW Driver for LAB Switch: Open, Close and Switch functions
  • Sign in to reply

Top Comments

  • Jan Cumps
    Jan Cumps over 8 years ago in reply to Jan Cumps +4
    Yay! It works. Above is the capture of a LabVIEW back and forth communication - with the Raspberry Pi as a VISA TCP/IP device. *IDN? command sent, and the reply from the Pi arrived at LabVIEW.
  • DAB
    DAB over 8 years ago +3
    Good luck Jan. DAB
  • Jan Cumps
    Jan Cumps over 8 years ago in reply to Jan Cumps +3
    what's not working ok: even though I get a reply, the Visa Read block in LabVIEW throws a timeout error. when I close a connection (regardless of telnet, LabVIEW), the service on the Raspberry Pi goes…
Parents
  • Jan Cumps
    Jan Cumps over 8 years ago

    Some more progress: first contact from LabVIEW

     

    image

    I don't have the reply working in the LabVIEW flow yet - it works different than serial/usb. But things look good.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • Jan Cumps
    Jan Cumps over 8 years ago in reply to Jan Cumps

    Yay!

     

    image

     

     

     

    It works. Above is the capture of a LabVIEW back and forth communication - with the Raspberry Pi as a VISA TCP/IP device.

    *IDN? command sent, and the reply from the Pi arrived at LabVIEW.

    • Cancel
    • Vote Up +4 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • shabaz
    shabaz over 8 years ago in reply to Jan Cumps

    Hi Jan,

     

    It's a while since I looked at the POSIX socket API, so I'm not sure either, but it might be worth also testing that newsockfd does not equal 0 before trying the read operation, e.g.

     

    if (newsockfd) {
      n=read(newsockfd, buffer, 255);
    }

     

    From memory I think using 'select' API is a good method to handle acting as a TCP server, but I need to read up on it. I'll try to dig up some useful links. There are some good patterns to handling socket reads, I just need to find them.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • Jan Cumps
    Jan Cumps over 8 years ago in reply to shabaz

    You may be on to something. I only call newsockfd() once at the start and assign it to a global variable (blush). So it will never be 0, but it may very well be invalid.

     

    I'll check if I have to reallocate each time, or if I have to check that handle's validity ...

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • shabaz
    shabaz over 8 years ago in reply to Jan Cumps

    Hi Jan,

     

    This is using select, so not the same, but nevertheless they are handling the read slightly differently.

    The code tests for zero, and if it is zero, then the socket needs to be closed.

     

    Unfortunately that means you mean need a loop to open a new socket after that, i.e. to re-execute from your line 117 in your code I think.

    The photo is from 'Unix Network Programming' and it is old, so some things could have changed.

    image

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • Jan Cumps
    Jan Cumps over 8 years ago in reply to shabaz

    I'm slowly getting there.

     

    This example keeps alive even if I close on the LabVIEW site. That's a step forward.

     

    #include<stdio.h>
    #include<string.h>    //strlen
    #include<sys/socket.h>
    #include<arpa/inet.h> //inet_addr
    #include<unistd.h>    //write
    
    
    int main(int argc , char *argv[])
    {
    int socket_desc , client_sock , c , read_size;
    struct sockaddr_in server , client;
    char client_message[2000];
    
    
    //Create socket
    socket_desc = socket(AF_INET , SOCK_STREAM , 0);
    if (socket_desc == -1)
    {
    printf("Could not create socket");
    }
    puts("Socket created");
    
    
    //Prepare the sockaddr_in structure
    server.sin_family = AF_INET;
    server.sin_addr.s_addr = INADDR_ANY;
    server.sin_port = htons( 2222 );
    
    
    //Bind
    if( bind(socket_desc,(struct sockaddr *)&server , sizeof(server)) < 0)
    {
    //print the error message
    perror("bind failed. Error");
    return 1;
    }
    puts("bind done");
    while (1) {
    
    
    //Listen
    listen(socket_desc , 3);
    
    
    //Accept and incoming connection
    puts("Waiting for incoming connections...");
    c = sizeof(struct sockaddr_in);
    
    
    //accept connection from an incoming client
    client_sock = accept(socket_desc, (struct sockaddr *)&client, (socklen_t*)&c);
    if (client_sock < 0)
    {
    perror("accept failed");
    return 1;
    }
    puts("Connection accepted");
    
    
    //Receive a message from client
    while( (read_size = recv(client_sock , client_message , 2000 , 0)) > 0 )
    {
    //Send the message back to client
    write(client_sock , client_message , strlen(client_message));
    }
    
    
    if(read_size == 0)
    {
    puts("Client disconnected");
    fflush(stdout);
    }
    else if(read_size == -1)
    {
    perror("recv failed");
    }
    }
    
    
    return 0;
    }

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • Jan Cumps
    Jan Cumps over 8 years ago in reply to Jan Cumps

    image

    I had a read on the timeout. It happens when the expected numbers of characters haven't arrived after the given timeout.

    Because TCP/IP in VISA doesn't support querying the number of characters waiting to be read (I've tried and I get Not Supported by this instrument), I have made this decision:

    After reading from the TCP/IP pipe, throw away that particular timeout error, because it is expected. Comment f you would do this differently.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • Jan Cumps
    Jan Cumps over 8 years ago in reply to Jan Cumps

    image

    I had a read on the timeout. It happens when the expected numbers of characters haven't arrived after the given timeout.

    Because TCP/IP in VISA doesn't support querying the number of characters waiting to be read (I've tried and I get Not Supported by this instrument), I have made this decision:

    After reading from the TCP/IP pipe, throw away that particular timeout error, because it is expected. Comment f you would do this differently.