Test & Tools
  • Technologies
  • More
Test & Tools
Blog
  • Blog
  • Forum
  • Documents
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Test & Tools to participate - click to join for free!

Blog

  • Tags
  • Subscribe by email
  • More
  • Cancel
  • Programmable Electronic Load - UART

    Jan Cumps
    Jan Cumps
    This blog documents focuses on the UART approach for the electronic load that peteroakes, jc2048 and jancumps designed.UART combined with SCPI are the programming interface for the instruments. UART Info: initial design used UART1 as 2nd op...
    • 10 Oct 2020
  • Programmable Electronic Load - RTOS Config

    Jan Cumps
    Jan Cumps
    This blog documents focuses on the RTOS approach for the electronic load that peteroakes, jc2048 and jancumps designed. CCS 8 with MSP432 compiler TI v 16.12.0.STS or >TI-RTOS for MSP43X, any SimpleLink version  RTOS Tasks overview&...
    • 10 Oct 2020
  • Programmable Electronic Load - SCPI interface and Error Handling

    Jan Cumps
    Jan Cumps
    This blog documents focuses on the SCPI functionality of the electronic load that peteroakes, jc2048 and jancumps designed.The interface works with software that can do serial communications on a COM port.This project comes with a LABView driver and ...
    • 10 Oct 2020
  • WirePulser: A DIY Wire Locating Tool

    shabaz
    shabaz
    Introduction How is it Used? How does it Work? Is it Legal? Circuit Details Trying it out Summary  IntroductionI needed to upgrade a spare room at home to convert it into an office. The ceiling has some low-voltage halogen lights fit...
    • 3 Oct 2020
  • Researchers develop a chemical sensor capable of detecting toxic gases at parts-per-billion level

    Catwell
    Catwell
    Researchers have developed a new 2D system by depositing platinum atoms on the carbon buffer layer's surface. This chemical sensor can be used to detect toxic gases such as benzene. (Image Credit: Chalmers University of Technology) Researche...
    • 24 Sep 2020
  • Building a Measurement Amplifier

    shabaz
    shabaz
    Introduction What is a Measurement Amplifier? Amplifier Circuit Building It Amplifier Noise Frequency Response Building Revision 2.0 Summary   Note: This blog post is now historical, there is a more improved version of the M...
    • 21 Sep 2020
  • Artificial skin can react to pain like human skin

    Catwell
    Catwell
    This new artificial skin can sense changes in pressure, heat, and cold. This artificial skin could lead to more advanced prosthetics and robots. (Image credit: RMIT University) Though it’s unpleasant, pain is necessary because it helps keep us s...
    • 15 Sep 2020
  • Researchers demonstrate spin-galvanic effect graphene with topological topping

    Catwell
    Catwell
    To achieve the effect, researchers created a unique Hall-bar-like device of graphene-topological insulator heterostructures. Researchers believe this discovery could be used for applications in spintronic and quantum technologies. (Image credit: CC0 ...
    • 14 Sep 2020
  • Researchers create a true holographic movie

    Catwell
    Catwell
    Are we one step closer to the holographic technology found in a galaxy far, far away? (Image credit: Tokyo University) Remember the scene from Star Wars: A New Hope when Princess Leia used holographic technology to ask Obi-Wan Kenobi for help? T...
    • 11 Sep 2020
  • Engineers develop tiny tweezers that can manipulate biomolecules and proteins

    Catwell
    Catwell
    The nano=scaled tweezers could be used to detect pathogens and early stages of diseases such as Alzheimer's. (Image Credit: Justus Ndukaife, Vanderbilt University) Today's optical tweezers, which use a highly focused laser beam to trap a...
    • 10 Sep 2020
  • Elon Musk Demonstrates Neuralink Brain Implant Working in a Pig

    Catwell
    Catwell
    Source: screenshot from neuralink.  In a live-stream broadcast via YouTube on August 28, Elon Musk demonstrated his startup Neuralink’s technology, which had been surgically implanted into the skull of a pig named Gertrude. The aim of this impla...
    • 31 Aug 2020
  • Hayabusa2 spacecraft received approval to land in Australia

    Catwell
    Catwell
    Hayabusa2 deployed three rovers and a lander on the Ryugu asteroid, which collected samples of the asteroid's surface. The return mission has been officially approved to land in Australia on December 6th. (Image Credit: JAXA/Akihiro Ikeshita)&nbs...
    • 28 Aug 2020
  • Omega’s TI-125 Digital Thermal Camera Capable of More than R&D and Industrial Applications

    Catwell
    Catwell
    The TI-125 is designed for measurement, detection, and sampling tasks for R&D and industrial functions, but can also be utilized for COVID-19 applications as well. (Image credit: Omega) Omega designed its T-120 Series of thermal imaging came...
    • 21 Aug 2020
  • 'Quantum negativity' may lead to more precise measurements

    Catwell
    Catwell
    'This physical property can be used to make more precise measurements, which in turn can lead to advance technology like quantum computers. Quantum laser light shines on to a chemical molecule that needs to be measured. The light then passes thro...
    • 18 Aug 2020
  • Wi-Fi system uses lasers to bring stable internet connection underwater

    Catwell
    Catwell
    The new system would be ideal for underwater data centers that need to connect with surface networks. The system uses various off-the-shelf components and a Raspberry Pi to act as a modem. (Image credit: KAUST) With Wi-Fi readily available in ou...
    • 17 Aug 2020
  • Scientists can now Track Space Debris 24-Hours a Day

    Catwell
    Catwell
    The new method of tracking space junk involves using high-powered lasers that detect diffused reflections bouncing back from the debris orbiting up to 36,000 kilometers away. (Image credit: NASA)  There’s a good chance that no matter where you a...
    • 10 Aug 2020
  • Global lockdown leads to 50% reduction of human-linked vibrations

    Catwell
    Catwell
    Citizen-owned seismometers showed significant reductions of noise around schools and universities in places like Cornwall, UK and Boston, U.S.  (Image Credit: Imperial College London) Seismometers measure seismic waves from earthquakes, vol...
    • 7 Aug 2020
  • Using the INA210-214 for Current Measurement for IoT Devices

    shabaz
    shabaz
    IntroductionThis short blog post documents a simple project to measure current in devices that may have low power operation for periods, but possibly have periods of high current draw.I recently needed to monitor the current of a few wireless devices...
    • 28 Jul 2020
  • Measure the Low Power Mode currents of a ST Micro Nucleo microcontroller

    Jan Cumps
    Jan Cumps
    I have a ST Micro Nucleo board with a low power microcontroller. The STM32F030R8I'm going to measure its power consumption, to see how well it would do in low power designs.ST has a good power measurement example; called PWR_CurrentConsumption. I...
    • 25 Jul 2020
  • Mutekimaru, a fish in Japan is unknowingly playing Pokemon Ruby

    Catwell
    Catwell
    Mutekimaru has already logged over 780 hours of Pokemon Ruby. (Image Credit: Mutekimaure Channel)  I’ve been a huge fan of fish ever since my “Project Goldie" internet controlled fishtank build here on element14. This is a pretty fun way of inte...
    • 21 Jul 2020
  • Researchers examine fractional quantum hall states in 2D semiconductors

    Catwell
    Catwell
    This image shows a monolayer WSe2 housing "composite fermions," a quasi-particle created from the interaction between electrons. It's also responsible for the sequence of fractional quantum Hall states. (Image Credit: Cory Dean/Columbia...
    • 15 Jul 2020
  • i2c Debugging with a RIGOL DS1054Z Oscilloscope: Trigger and Decode

    Jan Cumps
    Jan Cumps
    This real world example shows how to trigger a RIGOL DS1054Z oscilloscope at a specific point in an i2c communication, and then check signal + data.The DS1054Z comes with i2c functionality. In the past they were options you bought separately. Since 2...
    • 10 Jul 2020
  • The first ever video call was made 50 years ago using Picturephone Mod II

    Catwell
    Catwell
    The very first video call took place fifty years ago, which involved using the Picturephone Mod II device. (Image Credit: Chris Harrison/Carnegie Mellon University) Fifty years ago, the first-ever video call took place using AT&T’s Pictureph...
    • 9 Jul 2020
  • Wearable gloves can translate sign language into written and spoken words

    Catwell
    Catwell
    A new prototype from UCLA can translate sign language using a smartphone with 98.63% accuracy. Unlike previous devices, this one is lightweight and inexpensive. (Image credit:  UCLA) American Sign Language (ASL) is a difficult language to l...
    • 6 Jul 2020
  • Researchers discover a new phenomenon that could lead to quantum devices

    Catwell
    Catwell
    The diagram shows the conditions that cause the Kohn anomaly to rise in convenient metals (left) and a material is known as a Weyl semimetal (right).  (Image Credit: MIT) Researchers at MIT and elsewhere have discovered an exotic physical p...
    • 26 Jun 2020
<>